i.mx8m-mini w/ 4G/DDR3L with ISSI dual rank 1x16Gb

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx8m-mini w/ 4G/DDR3L with ISSI dual rank 1x16Gb

461 Views
jbtalley
Contributor III

Custom board using i.mx8m-mini

Using MX8M-Mini-DDR3l_RPA-v9

2 x 1Gx16 ISSI Memory (https://www.issi.com/WW/pdf/43-46TR16K01S2A-AL.pdf) installed (4GB total, 32Gb)

MScale v3.30

The DDR3 has 2 CS lines.  CS0 on each die are tied together (DRAM_CS0_N).  CS1 of each die are tied together (DRAM_CS1_N).  

The RPA line 20 says DRAM density per chip (Gb).  The DDRL has 2 ranks - so, my only option is to *assume* this means per rank, and not per physical die on the board.  So, I choose 8.  However, using that same logic fails on DRAM Bus Width per chip.  I feel like the right answer would be 16 - but I don't understand why that value isn't available in the RPA (values stem from cell C124?)

I'm looking for help in selecting the right values in the RPA tool.  There aren't _THAT_ many combinations, and I feel like I've tried them all - and none of them will pass calibration.  I've had limited success with some in uboot, but stability is non-existent.

I hesitate to share any successes configurations because they all feel like dumb luck.  At one point, I was able to calibrate 3 boards, but then when I moved the code to u-boot (2020) it failed, and I was unable to reproduce the calibration from the mscale tool.  Ironically, when these successes did occur, the total density detected on the board was 2048MB - which is 1/2 of what is actually present.

 

 

 

 

 

Labels (1)
0 Kudos
Reply
0 Replies