i.mx6ull dram test via jtag lauterbach

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx6ull dram test via jtag lauterbach

322件の閲覧回数
designteam
Contributor I

can someby point me at a simple way to attach and run some ddr test on a i.m6ull based board, i have having issues with using usb to load uboot so need to narrow down what the issue is

0 件の賞賛
1 返信

315件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi designteam

 

one can refer to AN5229 Arm® DS-5 Development Studio Debug i.MX6UL-EVK

and try to reause /apps/..ddr_test.c from i.MX6Q baremetal sdk (1.1.0_iMX6_Platform_SDK.zip)

from link

https://community.nxp.com/t5/i-MX-Processors/SMP-Enable-in-IMX6/m-p/542111

 

Best regards
igor

0 件の賞賛