i.mx6ul的.dtsi中interrupts=<3>,中间参数的意义是什么?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx6ul的.dtsi中interrupts=<3>,中间参数的意义是什么?

1,184 Views
rooftree
Contributor II

interrupts = <GIC_SPI 14 IRQ_TYPE_LEVEL_HIGH>;

中间的数字是什么意义?我看linux的documentation/devicetree/bindings/interrupt-controller的interrupt.txt,只说明了2个参数的情况,并没有3个参数的说明。

Labels (1)
0 Kudos
Reply
1 Reply

592 Views
igorpadykov
NXP Employee
NXP Employee

Hi

for description of interrupt property please look at

p.8 AN5125 Introduction to Device Trees

http://cache.nxp.com/files/32bit/doc/app_note/AN5125.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply