i.mx6q sabresd and DirectFB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx6q sabresd and DirectFB

ソリューションへジャンプ
2,114件の閲覧回数
alexanderz
Contributor I

Hi!

DirectFB reports:

DirectFB/Graphics: Vivante unknown chip model 1.0 (Vivante)

1) I'm having problem ATM to use hw acceleration for displaying/scaling preallocated I420 surfaces. At first, I've got alignment warnings like these:

(!!!)  *** WARNING [Prealloc address is not aligned!                                                                           
] *** [gc_dfb_pool.c:322 in galAllocateBuffer()]                                                                                

(!!!)  *** WARNING [Failed to do blit. status: -20 

After I align preallocated buffer by 64 bytes I started getting the following warning:


*** [gc_dfb_raster.c:1463 in galBlit()]                                                                                       

(!!!)  *** WARNING [Failed to do blit. status: -20 ]

If I disable hw acceleration (e.g. either by  by removing libdirectfb_gal.so from gfxdrivers directory or by setting "no-hardware" option in directfbrc) I can create I420 surface and scale it if needed(using StretchBlit()) without any problems.

Original source code for blitting/stretch blitting:

idsc.flags = DSDESC_HEIGHT | DSDESC_WIDTH | DSDESC_PREALLOCATED | DSDESC_PIXELFORMAT;

idsc.caps = DSCAPS_NONE;

idsc.pixelformat = DSPF_I420;

idsc.preallocated[0].data = (uint8_t *)ptr; /* 64 byte aligned */

idsc.preallocated[0].pitch = idsc.width;

idsc.preallocated[1].data = NULL;

idsc.preallocated[1].pitch = 0;

DFBCHECK(dfb->CreateSurface(dfb, &idsc, &yuvsf));

DFBCHECK(primary->Blit(primary, yuvsf, NULL, x, y));

DFBCHECK(yuvsf->Release(yuvsf));

primary's format is RGB32.

2) I'm also having problems when trying to Blit RGB24 preallocated surface to RGB32 primary surface. Errors:

] *** [gc_dfb_utils.c:239 in gal_get_native_format()]

(!?!)  *** BUG [unexpected pixelformat.

TIA.

Best regards.

Alex.

ラベル(4)
1 解決策
1,180件の閲覧回数
Martin1z
Contributor III

Yes, I already did this using fbset.

After some additional investigation I resolved the problem. I think it was related to the pixel format that I compiled into QT. By default QT used ARGB pixel format where the alpha bits remain on the most significant bits. I suppose that these bits where responsible for the wrong pixel offset.

So after recompiling QT without 32bit ARGB support the problem is gone for me.

元の投稿で解決策を見る

7 返答(返信)
1,180件の閲覧回数
PrabhuSundarara
NXP Employee
NXP Employee

Do you see any problems with the surface which are not preallocated?

0 件の賞賛
1,180件の閲覧回数
Martin1z
Contributor III

I have detected that there is an option to adjust alignment in direcftb. But unfortunatly this feature wasn't available in directfb 1.4.0.

git.directfb.org Git - core/DirectFB.git/commit

0 件の賞賛
1,180件の閲覧回数
Martin1z
Contributor III

Meanwhile I have added this patch to my directfb-1.4.0 version manually, but unfortunatly it does not resolve the situation. The surfaces allocated by qt are all at a 64 byte offset. Therefore I think it is a problem surface pool handling inside gfxdriver?!

0 件の賞賛
1,180件の閲覧回数
ChucoChe
NXP Employee
NXP Employee

Have you tried to increase the size of the frame buffer virtual size?

Vivantes directfb implementation takes the size of the surfaces from the frame buffer.

Michel

0 件の賞賛
1,181件の閲覧回数
Martin1z
Contributor III

Yes, I already did this using fbset.

After some additional investigation I resolved the problem. I think it was related to the pixel format that I compiled into QT. By default QT used ARGB pixel format where the alpha bits remain on the most significant bits. I suppose that these bits where responsible for the wrong pixel offset.

So after recompiling QT without 32bit ARGB support the problem is gone for me.

1,180件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

no response.

0 件の賞賛
1,180件の閲覧回数
Martin1z
Contributor III

I have the same problem here (using a QT based application), but I did not yet take a deeper look into this problem.

And yes, I do see a lot of display errors.

BTW: Will the source code of the gfxdriver be available in future?

0 件の賞賛