[i.mx6d]CPU load is 160% when play 1080P video with gstreamer tee element

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[i.mx6d]CPU load is 160% when play 1080P video with gstreamer tee element

920 Views
andyyang
Contributor II

Hi everyone

I have a question about Gstreamer tee element when playing 10@80P video.

when i play 1080P video with gstreamer tee element,CPU load is 160%.

Detail of my project requirement and software design as below:

[Project requirement]

Playback 1080P video and output videostream to two different display(DISP1:UI + Video,DISP2:Video)

[software design]

1.Design videoplayer based on playbin of gstreamer

2.Add tee element to the playbin in order to output videostream to two imxv4l2sink

[tee element reference code]

m_videoSink2 = gst_element_factory_make("imxv4l2sink", NULL);

g_object_set(G_OBJECT(m_videoSink2), "device", "/dev/video18", NULL);

......

gst_object_ref(GST_OBJECT(m_videoSink2));

//creat tee element

tee = gst_element_factory_make ("tee",NULL);

g_object_set(G_OBJECT(tee), "allow-not-linked", true, NULL);

queues[0] =gst_element_factory_make("queue",NULL);

queues[1] =gst_element_factory_make("queue",NULL);

qsrc_pad = gst_element_get_static_pad(queues[0],"src");

gst_bin_add_many(GST_BIN(m_videoOutputBin),m_videoIdentity, tee,queues[0],m_videoSink1,queues[1],m_videoSink2,NULL);

gst_element_link(queues[0],m_videoSink1);

gst_element_link(queues[1],m_videoSink2);

for (i = 0; i < NUM_SUBSTREAMS; ++i) {

tee_srcpads[i] = gst_element_get_request_pad (tee, "src_%u");

qsinkpads[i]= gst_element_get_static_pad (queues[i], "sink");

gst_pad_link (tee_srcpads[i],qsinkpads[i]);

}

gst_element_link(m_videoIdentity, tee);

[Test Result]

1.Play 1080P video to one display,CPU Load:8%(Compute based on IPU/VPU)

1.Play 1080P video to two display with above software design,CPU Load:160%(Compute based on IPU/VPU and CPU??)

So i think the reason of cpu overload is about tee element,maybe tee element copy the videostream data to two imxv4l2sink based on CPU.

Could anyone give me some advice about how to solve  this issue?

Appreciate any help in advance.

Thank you

Andy

Labels (1)
0 Kudos
Reply
2 Replies

636 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please refer to “i.MX_Linux_User's_Guide.pdf”.

“Video playback to multiple displays can be supported by a video sink plugin.

To configure the video sink plugin for multidisplay mode, see Overlaysink usage

later in this document.”

  It makes sense to use the recent BSP.

i.MX 6 Series Software and Development Tool|NXP

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

636 Views
andyyang
Contributor II

HI Yuri

Thank you for your reply.

According to your advice,i use overlaysink to display the same video on two different monitor.

On the monitor1,i want to display:Background graphic for UI,Frontground graphic for Video.

But when i use overlaysink,video graphic of frontground consist of video content and black sreen.

So i can not see the UI graphic of background.

I do not want to display black sreen of the video graphic(FG).

I change  overlay-top/overlay-left of overlaysink property,but it seems not work.

Is there any method on how to do not display black sreen of the video graphic(FG).

Thank you

Andy

0 Kudos
Reply