i.mx6 with LPDDR2 having 2 channel mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx6 with LPDDR2 having 2 channel mode

491件の閲覧回数
prev
Contributor II

Hi,

I am planning to use i.mx6 with 16G bits DDR2 Mobile RAM(LPDDR2)

Organization

— 32M words × 32 bits × 8 banks × 2 ranks

Data's of 32 bits connected with i.mx6 processor  out of 64 bit data.

The renaming 32 bits are floated. My query is that can we connect like this or i.mx6 support only 64 bit 2channel LPDDR2.?

pastedImage_1.png

Thanks

Prev Ravanth

タグ(2)
0 件の賞賛
1 返信

335件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Prev

such connection also may be used.

MMDC supports LPDDR2 two channel x16/x32 memory types.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛