i.mx6 can't connect with USB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.mx6 can't connect with USB

393 次查看
yun1405007
Contributor I

    Hi everybody:   According to the official manual,we design circuit again about  I.MX6 processor,now,we tested the board yestoday,But,

the board can't be recognised in USB.VDDCORE and VDDSOC is 1.4V, VDD_HIGH_IN and NSNVS are 3.0V.All supply voltages

are in line with  the official manual.There are nothing wrong in multiplexing I / O ports and power-up sequence,However,we alway can't connect with USB.To our strange,when VDDCORE and VDDSOC voltage at around 1.2V ,USB can be connected,but Loading image fails .

thanks

0 项奖励
1 回复

325 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi,

You could refer to section 3.11 “USB recommendations” of the “Hardware Development Guide for i.MX 6Quad, 6Dual, 6DualLite, 6Solo Families of Applications Processo...” document and to section 3.4.1.2 “USB” of the application note AN3951 “i.MX Layout Recommendations”.

Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励