i.mx285 hardware design issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx285 hardware design issue

ソリューションへジャンプ
848件の閲覧回数
liyingchun
Contributor I

Hi experts

I plan to use i.mx285 to design a gateway product. I want to know that how many layers of the pcb is Suitable for my design?(especially how many signal layers?)

The peripheral which I will use is that: 1 i2c, 2 spi, 3 uart, 1 sdio, 1 audio interface, 2 can, 2 usb, flash + DDR2, no ethernet and no graphic interface(LCD)

and the area of the pcb is rich.

There is a reference design:

Home Health Hub Reference Platform|Freescale

how many layer of the pcb it use?

Thanks very much!

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
780件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

Please refer to app note AN4215 (i.MX28 Layout and Design Guidelines).

http://cache.freescale.com/files/32bit/doc/app_note/AN4215.pdf 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
781件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

Please refer to app note AN4215 (i.MX28 Layout and Design Guidelines).

http://cache.freescale.com/files/32bit/doc/app_note/AN4215.pdf 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------