i.MXRT evaluation board with parallel camera port?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MXRT evaluation board with parallel camera port?

1,185件の閲覧回数
Mc2023
Contributor IV

Hi @kerryzhou , All,

Is there an i.MXRT evaluation board with parallel camera port?

Best regards,

 

ラベル(1)
タグ(3)
0 件の賞賛
返信
7 返答(返信)

1,113件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Mc2023 ,

    Thanks for your trust.

     Yes, of course, our MIMXRT1060-EVK board is the parallel cameral port:

kerryzhou_0-1691388782956.png

 

https://www.nxp.com/design/development-boards/i-mx-evaluation-and-development-boards/i-mx-rt1060-eva...

 

Wish it helps you!

If you still have a question about it, please kindly let me know.

Best Regards,

kerry

0 件の賞賛
返信

1,108件の閲覧回数
Mc2023
Contributor IV

Hi @kerryzhou ,

Thanks for your feedback!

In the meantime, I have also noticed that MIMXRT1060-EVK has a CSI interface. There is also the 1050-EVK.

I have forgotten to mention, I am looking for an EVK composed of a dual core i.MXRT and a csi port. Do you have that? 

Best regards

0 件の賞賛
返信

1,100件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

You mean RT11XX board, right?

Until now, our EVK for RT11XX are all MIPI interface, no parallel interface.

Maybe you can check the schematic, check the related parallel pins, whether you can use wire connect out or not.

 

Best Regards,

kerry

0 件の賞賛
返信

1,097件の閲覧回数
Mc2023
Contributor IV

hi @kerryzhou ,

Thanks for your feedback!

Any EVK with an i.MXRT dual processor and parallel interface.

Best regards

 

0 件の賞賛
返信

1,068件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Mc2023 ,

   As I know, our EVK with dual core are all the MIPI interface, not the parallel interface.

  But, our RT11XX with dual core can support the parallel interface, just not fan out it to the elcd RGB interface, the parallel interface is the same as the MIMXRT1060-EVK, MIMXRT1050-EVKB board.

  So, if you have the RT1060, RT1050 board, you also can use that board test it, then to the dual board, you can design your own board.

 

Wish it helps you!

Best Regards,

Kerry

0 件の賞賛
返信

1,054件の閲覧回数
Mc2023
Contributor IV

Hi @kerryzhou,

Thanks for your feedback!

It looks that we are going to switch to a microcontroller from ST Microelectronics.

Best regards,

 

0 件の賞賛
返信

1,043件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Sorry for the inconvenience we bring you.

Maybe you also can select the MIPI interface RGB LCD, just like the RT1170-EVK associated with the 

https://www.nxp.com/design/development-boards/i-mx-evaluation-and-development-boards/i-mx-rt1170-eva...

 

Wish it helps you!

Best Regards,

Kerry

0 件の賞賛
返信