i.MX8dx Ethernet (cdc_ether) dev_watchdog warning

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8dx Ethernet (cdc_ether) dev_watchdog warning

501 Views
liu_y10
Contributor I

version: imx8dx imx-yocto-bsp4.14.98_2.3.0
We use pinctrl_usbotg3 to connect quectel's device
Every time we connect, the watch_dog timeout exception log will appear after pulling up our usb device for more than 10 seconds.
And when we use the module to transfer and decompress the upgraded package to imx8dx using nfs through this usb, this log will also appear occasionally. After appearing, the usb l is disconnected
The specific log is as follows:

---------------------------------------------------------------------------------------------------------------------------------------

U-Boot SPL 2018.03 (Apr 17 2022 - 18:41:34 +0800)
Normal Boot
Trying to boot from MMC1
Load image from MMC/SD 0x53000
U

U-Boot 2018.03 (Apr 17 2022 - 18:41:34 +0800)

CPU: Freescale i.MX8QXP revC A35 at 1200 MHz at 37C
Model: Freescale i.MX8DX MEK
Board: iMX8DX MEK
Boot: MMC0
DRAM: 994 MiB
gpio@5d090000: dir_output: error: gpio GPIO1_7 not reserved
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... *** Warning - bad CRC, using default environment

Failed (-5)
TX PLL is not locked.
In: serial
Out: serial
Err: serial

BuildInfo:
- SCFW b929edfe, SECO-FW 268f2c02, IMX-MKIMAGE d7f9440d, ATF bb209a0
- U-Boot 2018.03

switch to partitions #0, OK
mmc0(part 0) is current device
flash target is MMC:0
Net: No ethernet found.
Fastboot: Normal

MMC read: dev # 0, block # 4642816, count 1 ... 1 blocks read: OK
update complete
update start

MMC write: dev # 0, block # 0, count 1 ... 1 blocks written: OK
start_partition_choose===>start from main
Normal Boot
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0(part 0) is current device
** Unable to read file boot.scr **
26908672 bytes read in 120 ms (213.9 MiB/s)
Booting from mmc ...
Authenticate OS container at 0x98000000
## Flattened Device Tree blob at 83000000
Booting using the fdt blob at 0x83000000
Using Device Tree in place at 0000000083000000, end 0000000083014083
Disable gpt0@5d140000, resource id 207 not owned
Disable dsp@596e8000, resource id 512 not owned
/dma-controller@591F0000, 54008
/dma-controller@599F0000, 54972
/dma-controller@5a1f0000, 53056
/dma-controller@5a1f0000, 53056

Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.14.98 (jenkins@cnninvmjnkns01) (gcc version 7.3.0 (GCC)) #1 SMP PREEMPT Fri Apr 29 19:28:48 CST 2022
[ 0.000000] Boot CPU: AArch64 Processor [410fd042]
[ 0.000000] Machine model: Freescale i.MX8DX MEK - NIO
[ 0.000000] OF: reserved mem: OVERLAP DETECTED!
[ 0.000000] ramoops@0xbfc00000 (0x00000000bfc00000--0x00000000bfd00000) overlaps with nouse@0xbfc00000 (0x00000000bfc00000--0x00000000c0000000)
[ 0.000000] OF: reserved mem: OVERLAP DETECTED!
[ 0.000000] nouse@0xbfc00000 (0x00000000bfc00000--0x00000000c0000000) overlaps with optee_shm@0xbfc00000 (0x00000000bfc00000--0x00000000c0000000)
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000096000000, size 320 MiB
[ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x0000000090400000, size 28 MiB
[ 0.000000] OF: reserved mem: initialized node rpmsg_dma@0x90400000, compatible id shared-dma-pool
[ 0.000000] NUMA: No NUMA configuration found
[ 0.000000] NUMA: Faking a node at [mem 0x0000000000000000-0x00000000bdffffff]
[ 0.000000] NUMA: NODE_DATA [mem 0xbdf8c480-0xbdf8e27f]
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000080200000-0x00000000bdffffff]
[ 0.000000] Normal empty
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000080200000-0x0000000083ffffff]
[ 0.000000] node 0: [mem 0x0000000086200000-0x000000008fffffff]
[ 0.000000] node 0: [mem 0x0000000094c00000-0x00000000bdffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000080200000-0x00000000bdffffff]
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: Trusted OS migration not required
[ 0.000000] psci: SMC Calling Convention v1.1
[ 0.000000] percpu: Embedded 22 pages/cpu @ffff80003df5b000 s49304 r8192 d32616 u90112
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] Speculative Store Bypass Disable mitigation not required
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 221760
[ 0.000000] Policy zone: DMA
[ 0.000000] Kernel command line: console=ttyLP0,115200 earlycon=,115200 bootflag=main u-bootversion=SAN.01.00.2154.16
[ 0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes)
[ 0.000000] Memory: 398528K/901120K available (12094K kernel code, 984K rwdata, 4300K rodata, 8768K init, 463K bss, 174912K reserved, 327680K cma-reserved)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] modules : 0xffff000000000000 - 0xffff000008000000 ( 128 MB)
[ 0.000000] vmalloc : 0xffff000008000000 - 0xffff7dffbfff0000 (129022 GB)
[ 0.000000] .text : 0xffff000008080000 - 0xffff000008c50000 ( 12096 KB)
[ 0.000000] .rodata : 0xffff000008c50000 - 0xffff000009090000 ( 4352 KB)
[ 0.000000] .init : 0xffff000009090000 - 0xffff000009920000 ( 8768 KB)
[ 0.000000] .data : 0xffff000009920000 - 0xffff000009a16008 ( 985 KB)
[ 0.000000] .bss : 0xffff000009a16008 - 0xffff000009a89e48 ( 464 KB)
[ 0.000000] fixed : 0xffff7dfffe7fb000 - 0xffff7dfffec00000 ( 4116 KB)
[ 0.000000] PCI I/O : 0xffff7dfffee00000 - 0xffff7dffffe00000 ( 16 MB)
[ 0.000000] vmemmap : 0xffff7e0000000000 - 0xffff800000000000 ( 2048 GB maximum)
[ 0.000000] 0xffff7e0000008000 - 0xffff7e0000f80000 ( 15 MB actual)
[ 0.000000] memory : 0xffff800000200000 - 0xffff80003e000000 ( 990 MB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] RCU restricting CPUs from NR_CPUS=64 to nr_cpu_ids=2.
[ 0.000000] Tasks RCU enabled.
[ 0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: no VLPI support, no direct LPI support
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000051b00000
[ 0.000000] arch_timer: cp15 timer(s) running at 8.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1d854df40, max_idle_ns: 440795202120 ns
[ 0.000005] sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199023255500ns
[ 0.002589] Console: colour dummy device 80x25
[ 0.002650] Calibrating delay loop (skipped), value calculated using timer frequency.. 16.00 BogoMIPS (lpj=32000)
[ 0.002663] pid_max: default: 32768 minimum: 301
[ 0.002747] Security Framework initialized
[ 0.003110] Dentry cache hash table entries: 131072 (order: 8, 1048576 bytes)
[ 0.003284] Inode-cache hash table entries: 65536 (order: 7, 524288 bytes)
[ 0.003306] Mount-cache hash table entries: 2048 (order: 2, 16384 bytes)
[ 0.003324] Mountpoint-cache hash table entries: 2048 (order: 2, 16384 bytes)
[ 0.019921] ASID allocator initialised with 32768 entries
[ 0.027918] Hierarchical SRCU implementation.
[ 0.037007] *****Initialized MU
[ 0.037036] ***** imx8_init_pm_domains *****
[ 0.038204] CPU identified as i.MX8QXP, silicon rev 1.2
[ 0.043982] smp: Bringing up secondary CPUs ...
[ 0.072440] Detected VIPT I-cache on CPU1
[ 0.072472] GICv3: CPU1: found redistributor 1 region 0:0x0000000051b20000
[ 0.072505] CPU1: Booted secondary processor [410fd042]
[ 0.072592] smp: Brought up 1 node, 2 CPUs
[ 0.072608] SMP: Total of 2 processors activated.
[ 0.072618] CPU features: detected feature: GIC system register CPU interface
[ 0.072627] CPU features: detected feature: 32-bit EL0 Support
[ 0.072636] CPU features: detected feature: Kernel page table isolation (KPTI)
[ 0.076442] CPU: All CPU(s) started at EL2
[ 0.076458] alternatives: patching kernel code
[ 0.077017] devtmpfs: initialized
[ 0.088828] random: get_random_u32 called from bucket_table_alloc+0x108/0x260 with crng_init=0
[ 0.089446] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.089482] futex hash table entries: 512 (order: 4, 65536 bytes)
[ 0.098738] pinctrl core: initialized pinctrl subsystem
[ 0.100224] NET: Registered protocol family 16
[ 0.102100] cpuidle: using governor menu
[ 0.102267] NET: Registered protocol family 42
[ 0.103521] vdso: 2 pages (1 code @ ffff000008c56000, 1 data @ ffff000009924000)
[ 0.103538] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.110575] DMA: preallocated 256 KiB pool for atomic allocations
[ 0.111089] imx rpmsg driver is registered.
[ 0.116841] pstore: using zlib compression
[ 0.117286] console [pstore-1] enabled
[ 0.117293] pstore: Registered ramoops as persistent store backend
[ 0.117305] ramoops: attached 0x100000@0xbfc00000, ecc: 0/0
[ 0.118856] MU and Power domains initialized
[ 0.118872] ***** imx8qxp_clocks_init *****
[ 0.124889] random: fast init done
[ 0.197886] imx8qxp-pinctrl iomuxc: initialized IMX pinctrl driver
[ 0.208777] mxs_phy 5b100000.usbphy: 5b100000.usbphy supply phy-3p0 not found, using dummy regulator
[ 0.249897] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.266891] ACPI: Interpreter disabled.
[ 0.278043] vgaarb: loaded
[ 0.278488] SCSI subsystem initialized
[ 0.278922] usbcore: registered new interface driver usbfs
[ 0.278978] usbcore: registered new interface driver hub
[ 0.279030] usbcore: registered new device driver usb
[ 0.279732] usb_phy_generic usbphynop1: usbphynop1 supply vcc not found, using dummy regulator
[ 0.280015] media: Linux media interface: v0.10
[ 0.280050] Linux video capture interface: v2.00
[ 0.280154] pps_core: LinuxPPS API ver. 1 registered
[ 0.280165] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.280188] PTP clock support registered
[ 0.281516] EDAC MC: Ver: 3.0.0
[ 0.282855] clocksource: mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns
[ 0.289485] clocksource: Switched to clocksource arch_sys_counter
[ 0.289652] VFS: Disk quotas dquot_6.6.0
[ 0.289713] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.289853] pnp: PnP ACPI: disabled
[ 0.296997] NET: Registered protocol family 2
[ 0.297693] TCP established hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.297810] TCP bind hash table entries: 8192 (order: 5, 131072 bytes)
[ 0.297942] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.298052] UDP hash table entries: 512 (order: 2, 16384 bytes)
[ 0.298085] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
[ 0.298222] NET: Registered protocol family 1
[ 0.298601] RPC: Registered named UNIX socket transport module.
[ 0.298612] RPC: Registered udp transport module.
[ 0.298621] RPC: Registered tcp transport module.
[ 0.298630] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.724021] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
[ 0.724428] kvm [1]: 8-bit VMID
[ 0.725219] kvm [1]: GICv3: no GICV resource entry
[ 0.725230] kvm [1]: disabling GICv2 emulation
[ 0.725256] kvm [1]: GIC system register CPU interface enabled
[ 0.725303] kvm [1]: vgic interrupt IRQ1
[ 0.725367] kvm [1]: Hyp mode initialized successfully
[ 0.726737] audit: initializing netlink subsys (disabled)
[ 0.726848] audit: type=2000 audit(0.724:1): state=initialized audit_enabled=0 res=1
[ 0.727265] workingset: timestamp_bits=44 max_order=18 bucket_order=0
[ 0.734376] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.735035] NFS: Registering the id_resolver key type
[ 0.735065] Key type id_resolver registered
[ 0.735073] Key type id_legacy registered
[ 0.735088] Installing knfsd (copyright (C) 1996 okir@monad.swb.de).
[ 0.735746] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
[ 0.740250] NET: Registered protocol family 38
[ 0.740364] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 246)
[ 0.740377] io scheduler noop registered
[ 0.740527] io scheduler cfq registered (default)
[ 0.740537] io scheduler mq-deadline registered
[ 0.740545] io scheduler kyber registered
[ 0.746768] mxs-dma 5b810000.dma-apbh: initialized
=0 fsgid=0 tty=(none) ses=4294967295 comm="swapper/0" exe=(null)
[ 0.755172] 5a060000.serial: ttyLP0 at MMIO 0x5a060010 (irq = 32, base_baud = 5000000) is a FSL_LPUART
[ 1.728875] console [ttyLP0] enabled
[ 1.732708] fsl-lpuart 5a060000.serial: NO DMA tx channel, run at cpu mode
[ 1.739610] fsl-lpuart 5a060000.serial: NO DMA rx channel, run at cpu mode
[ 1.757189] loop: module loaded
[ 1.780448] libphy: Fixed MDIO Bus: probed
[ 1.784831] tun: Universal TUN/TAP device driver, 1.6
[ 1.790399] CAN device driver interface
[ 1.795419] e1000e: Intel(R) PRO/1000 Network Driver - 3.2.6-k
[ 1.801308] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[ 1.807410] sky2: driver version 1.30
[ 1.811462] usbcore: registered new interface driver cdc_ether
[ 1.817359] usbcore: registered new interface driver rndis_host
[ 1.829250] Can't support > 32 bit dma.
[ 1.833157] xhci-cdns3: xHCI Host Controller
[ 1.837547] xhci-cdns3: new USB bus registered, assigned bus number 1
[ 1.880012] xhci-cdns3: hcc params 0x200073c8 hci version 0x100 quirks 0xffffffffa0018010
[ 1.888519] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 1.895339] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 1.902592] usb usb1: Product: xHCI Host Controller
[ 1.907487] usb usb1: Manufacturer: Linux 4.14.98 xhci-hcd
[ 1.912987] usb usb1: SerialNumber: xhci-cdns3
[ 1.918059] hub 1-0:1.0: USB hub found
[ 1.921849] hub 1-0:1.0: 1 port detected
[ 1.926078] xhci-cdns3: xHCI Host Controller
[ 1.930458] xhci-cdns3: new USB bus registered, assigned bus number 2
[ 1.937010] xhci-cdns3: Host supports USB 3.0 SuperSpeed
[ 1.942555] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[ 1.950758] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003
[ 1.957566] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 1.964811] usb usb2: Product: xHCI Host Controller
[ 1.969701] usb usb2: Manufacturer: Linux 4.14.98 xhci-hcd
[ 1.975200] usb usb2: SerialNumber: xhci-cdns3
[ 1.980039] hub 2-0:1.0: USB hub found
[ 1.983837] hub 2-0:1.0: 1 port detected
[ 1.988371] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 1.994928] ehci-pci: EHCI PCI platform driver
[ 1.999473] ehci-platform: EHCI generic platform driver
[ 2.004976] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
[ 2.011186] ohci-pci: OHCI PCI platform driver
[ 2.015711] ohci-platform: OHCI generic platform driver
[ 2.021573] usbcore: registered new interface driver usb-storage
[ 2.027700] usbcore: registered new interface driver usbserial
[ 2.033699] usbcore: registered new interface driver usbserial_generic
[ 2.040268] usbserial: USB Serial support registered for generic
[ 2.046331] usbcore: registered new interface driver option
[ 2.051943] usbserial: USB Serial support registered for GSM modem (1-port)
[ 2.059045] usbcore: registered new interface driver usb_ehset_test
[ 2.066589] usbmisc_imx 5b0d0200.usbmisc: 5b0d0200.usbmisc supply vbus-wakeup not found, using dummy regulator
[ 2.088388] using random self ethernet address
[ 2.092870] using random host ethernet address
[ 2.097885] usb0: HOST MAC 32:13:56:b5:db:ee
[ 2.102298] usb0: MAC fa:b0:93:78:01:81
[ 2.106174] using random self ethernet address
[ 2.110636] using random host ethernet address
[ 2.115143] g_ether gadget: Ethernet Gadget, version: Memorial Day 2008
[ 2.121781] g_ether gadget: g_ether ready
[ 2.129564] input: sc-powerkey as /devices/platform/sc-powerkey/input/input0
[ 2.140141] mxc-jpeg 58400000.jpegdec: decoder device registered as /dev/video0 (81,0)
[ 2.149146] mxc-jpeg 58450000.jpegenc: encoder device registered as /dev/video1 (81,1)
[ 2.158250] pps pps0: new PPS source pps.-1
[ 2.162541] pps pps0: Registered IRQ 98 as PPS source
[ 2.169194] device-mapper: uevent: version 1.0.3
[ 2.174129] device-mapper: ioctl: 4.37.0-ioctl (2017-09-20) initialised: dm-devel@redhat.com
[ 2.182808] device-mapper: multipath round-robin: version 1.2.0 loaded
[ 2.190138] sdhci: Secure Digital Host Controller Interface driver
[ 2.196430] sdhci: Copyright(c) Pierre Ossman
[ 2.200884] sdhci-pltfm: SDHCI platform and OF driver helper
[ 2.253534] mmc0: SDHCI controller on 5b010000.usdhc [5b010000.usdhc] using ADMA
[ 2.269239] usbcore: registered new interface driver usbhid
[ 2.274957] usbhid: USB HID core driver
[ 2.281273] optee: probing for conduit method from DT.
[ 2.286790] optee: initialized driver
[ 2.290976] usbcore: registered new interface driver qcom_usb_qrtr
[ 2.298768] usbcore: registered new interface driver rmnet_usb
[ 2.308953] usbcore: registered new interface driver usb_bridge
[ 2.319725] diag: failed to find diag_dload imem node
[ 2.324954] usbcore: registered new interface driver diag_bridge
[ 2.331122] usbcore: registered new interface driver ks_bridge
[ 2.337222] usbcore: registered new interface driver mdm_data_bridge
[ 2.343789] NET: Registered protocol family 26
[ 2.349287] Netfilter messages via NETLINK v0.30.
[ 2.354035] nfnl_acct: registering with nfnetlink.
[ 2.359054] nf_conntrack version 0.5.0 (6144 buckets, 24576 max)
[ 2.365283] nf_tables: (c) 2007-2009 Patrick McHardy <kaber@trash.net>
[ 2.372034] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 2.380216] NET: Registered protocol family 10
[ 2.387537] Segment Routing with IPv6
[ 2.391294] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 2.398112] NET: Registered protocol family 17
[ 2.402624] can: controller area network core (rev 20170425 abi 9)
[ 2.408901] NET: Registered protocol family 29
[ 2.413378] can: raw protocol (rev 20170425)
[ 2.417680] can: broadcast manager protocol (rev 20170425 t)
[ 2.423373] can: netlink gateway (rev 20170425) max_hops=1
[ 2.429133] 8021q: 802.1Q VLAN Support v1.8
[ 2.433363] lib80211: common routines for IEEE802.11 drivers
[ 2.439087] 9pnet: Installing 9P2000 support
[ 2.443501] Key type dns_resolver registered
[ 2.447815] mmc0: new HS400 Enhanced strobe MMC card at address 0001
[ 2.455467] mmcblk0: mmc0:0001 8GUF4R 7.28 GiB
[ 2.460897] mmcblk0boot0: mmc0:0001 8GUF4R partition 1 31.9 MiB
[ 2.465340] imx8_cpufreq_init: cluster 0 running at freq 1200 MHz, suspend freq 1200 MHz
[ 2.467480] mmcblk0boot1: mmc0:0001 8GUF4R partition 2 31.9 MiB
[ 2.481924] mmcblk0rpmb: mmc0:0001 8GUF4R partition 3 4.00 MiB
[ 2.485754] SD1_SPWR: disabling
[ 2.490963] usb_otg_vbus: disabling
[ 2.494629] Warning: unable to open an initial console.
[ 2.501443] mmcblk0: p1 p2 p3 p4 < p5 p6 p7 p8 p9 p10 p11 p12 p13 >
[ 2.503328] Freeing unused kernel memory: 8768K
[ 2.548207] EXT4-fs (mmcblk0p10): mounted filesystem with ordered data mode. Opts: errors=remount-ro
[ 2.598466] EXT4-fs (dm-0): mounted filesystem with ordered data mode. Opts: errors=remount-ro
[ 2.672436] EXT4-fs (mmcblk0p6): mounted filesystem with ordered data mode. Opts: errors=remount-ro
[ 2.927745] systemd[1]: System time before build time, advancing clock.
CCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid)
[ 2.977790] systemd[1]: Detected architecture arm64.

Welcome to NXP i.MX Release Distro 4.14-sumo (sumo)!

[ 2.997960] systemd[1]: Set hostname to <imx8dxmek>.
[ 3.009618] random: systemd: uninitialized urandom read (16 bytes read)
[ 3.016297] systemd[1]: Initializing machine ID from random generator.
[ 3.022992] systemd[1]: Installed transient /etc/machine-id file.
roup based firewalling.
[ 3.135969] systemd[1]: Proceeding WITHOUT firewalling in effect! (This warning is only shown for the first loaded unit using IP firewalling.)
[ 3.174819] systemd[1]: /lib/systemd/system/store_kernelpanic.service:1: Assignment outside of section. Ignoring.
[ 3.185172] systemd[1]: /lib/systemd/system/store_kernelpanic.service:2: Assignment outside of section. Ignoring.
[ 3.195497] systemd[1]: /lib/systemd/system/store_kernelpanic.service:3: Assignment outside of section. Ignoring.
[ 3.306365] random: systemd: uninitialized urandom read (16 bytes read)
[ OK ] Reached target Swap.
[ 3.325899] random: systemd: uninitialized urandom read (16 bytes read)
[ OK ] Created slice System Slice.
[ OK ] Created slice system-serial\x2dgetty.slice.
[ OK ] Listening on Journal Audit Socket.
[ OK ] Listening on Journal Socket (/dev/log).
[ OK ] Created slice system-getty.slice.
[ OK ] Reached target Remote File Systems.
[ OK ] Listening on Journal Socket.
Mounting POSIX Message Queue File System...
Starting /var/psis mount...
Mounting Huge Pages File System...
Starting Load Kernel Modules...
Starting /var/ota mount...
[ 3.495074] cryptodev: loading out-of-tree module taints kernel.
Starting /var/reserve mount...
[ 3.508147] cryptodev: driver 1.12 loaded.
[ OK ] Listening on udev Control Socket.
[ OK ] Listening on udev Kernel Socket.
Starting udev Coldplug all Devices...
[ OK ] Created slice User and Session Slice.
[ OK ] Reached target Slices.
[ OK ] Started Dispatch Password Requests to Console Directory Watch.
Mounting Temporary Directory (/tmp)...
Mounting Kernel Debug File System...
[ OK ] Listening on /dev/initctl Compatibility Named Pipe.
[ OK ] Listening on Syslog Socket.
Starting Journal Service...
[ OK ] Started Forward Password Requests to Wall Directory Watch.
[ OK ] Reached target Paths.
Starting Remount Root and Kernel File Systems...
[ OK ] Listening on Network Service Netlink Socket.
Starting Create list of required st…ce nodes for the current kernel...
[ OK ] Started Journal Service.
[ OK ] Mounted POSIX Message Queue File System.
[ OK ] Mounted Huge Pages File System.
[ 3.785389] EXT4-fs (mmcblk0p7): mounted filesystem with ordered data mode. Opts: errors=remount-ro
[ OK ] Started Load Kernel Modules.
[ OK ] Mounted Temporary Directory (/tmp).
[ OK ] Mounted Kernel Debug File System.
[ 3.859099] EXT4-fs (mmcblk0p12): mounted filesystem with ordered data mode. Opts: errors=remount-ro
[ OK [ 3.870958] EXT4-fs (mmcblk0p13): mounted filesystem with ordered data mode. Opts: errors=remount-ro
] Started Remount Root and Kernel File Systems.
[ OK ] Started Create list of required sta…vice nodes for the current kernel.
[ OK ] Started /var/psis mount.
[ OK ] Started /var/ota mount.
[ OK ] Started /var/reserve mount.
Starting Create Static Device Nodes in /dev...
Mounting NFSD configuration filesystem...
Mounting Kernel Configuration File System...
Starting Apply Kernel Variables...
Starting Flush Journal to Persistent Storage...
[ OK ] Started udev Coldplug all Devices.
[ OK ] Started Create Static Device Nodes in /dev.
[ OK ] Mounted NFSD configuration filesystem.
[ OK ] Mounted Kernel Configuration File System.
[ OK ] Started Apply Kernel Variables.
Starting udev Kernel Device Manager...
[ OK ] Reached target Local File Systems (Pre).
[ OK ] Reached target Containers.
Mounting /var/volatile...
[ OK ] Mounted /var/volatile.
[ OK ] Started udev Kernel Device Manager.
[ 4.252147] systemd-journald[1663]: Received request to flush runtime journal from PID 1
Starting Network Service...
Starting Load/Save Random Seed...
[ OK ] Reached target Local File Systems.
Starting Rebuild Journal Catalog...
[ OK ] Started Flush Journal to Persistent Storage.
[ OK ] Started Load/Save Random Seed.
[ OK ] Started Network Service.
Starting Create Volatile Files and Directories...
[ OK ] Started Rebuild Journal Catalog.
Starting Update is Completed...
[ OK ] Started Update is Completed.
[ OK ] Started Create Volatile Files and Directories.
Starting Network Time Synchronization...
Starting Update UTMP about System Boot/Shutdown...
Starting Network Name Resolution...
[ OK ] Started Update UTMP about System Boot/Shutdown.
[ OK ] Started Network Time Synchronization.
[ OK ] Reached target System Initialization.
[ OK ] Listening on RPCbind Server Activation Socket.
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[ OK ] Listening on D-Bus System Message Bus Socket.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target Timers.
Starting sshd.socket.
[ OK ] Reached target System Time Synchronized.
[ OK ] Started Network Name Resolution.
[ OK ] Found device /dev/ttyLP0.
[ OK ] Listening on sshd.socket.
[ OK ] Reached target Sockets.
[ OK ] Reached target Basic System.
[ OK ] Started TEE Supplicant.
Starting Telephony service...
[ OK ] Started JPCC fdbus host service.
[ 4.974842] IPv6: ADDRCONF(NETDEV_UP): usb0: link is not ready
Starting Avahi mDNS/DNS-SD Stack...
[ OK ] Started Kernel Logging Service.
[ OK ] Started System Logging Service.
Starting store_kernelpanic.service...
Starting RPC Bind Service...
Starting GENIVI DLT logging daemon...
[ OK ] Started D-Bus System Message Bus.
[ OK ] Started JPCC fdbus name service.
Starting JPCC fdbus service...
Starting Login Service...
[ OK ] Reached target Host and Network Name Lookups.
[ OK ] Reached target Network.
Starting Permit User Sessions...
[ OK ] Started store_kernelpanic.service.
[ OK ] Started RPC Bind Service.
[ OK ] Started GENIVI DLT logging daemon.
[ OK ] Started Permit User Sessions.
[ OK ] Started Avahi mDNS/DNS-SD Stack.
[ OK ] Started Telephony service.
[ OK ] Started Login Service.
[ OK ] Started Getty on tty1.
[ OK ] Started Serial Getty on ttyLP0.
[ OK ] Reached target Login Prompts.
[ OK ] Reached target Multi-User System.
Starting Update UTMP about System Runlevel Changes...
[ OK ] Started NFS status monitor for NFSv2/3 locking..
[ OK ] Started NFS Mount Daemon.
Starting NFS server and services...
[ OK ] Started Update UTMP about System Runlevel Changes.
[ 6.155574] NFSD: Using /var/lib/nfs/v4recovery as the NFSv4 state recovery directory
[ 6.163832] NFSD: starting 30-second grace period (net ffff0000099e8100)
[ OK ] Started NFS server and services.
[ 7.846747] audit: type=1325 audit(1598953332.916:3): table=nat family=2 entries=5
5 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=4294967295 comm="iptables" exe="/usr/sbin/iptables" key=(null)
[ 7.881328] audit: type=1327 audit(1598953332.916:3): proctitle=69707461626C6573002D74006E6174002D46
[ 8.005597] audit: type=1325 audit(1598953332.916:4): table=nat family=2 entries=5
5 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=4294967295 comm="iptables" exe="/usr/sbin/iptables" key=(null)
415351554552414445002D6F0075736231
[ OK ] Started JPCC fdbus service.
[ OK ] Started JPCC network service.
[ OK ] Started JPCC system service.
[ OK ] Started JPCC power service.
[ OK ] Started JPCC upgrade service.
[ OK ] Started JPCC v2x service.

NXP i.MX Release Distro 4.14-sumo imx8dxmek ttyLP0

imx8dxmek login: [ 16.745529] usb 1-1: new high-speed USB device number 2 using cdns-usb3
[ 16.901440] usb 1-1: config 1 has an invalid interface number: 7 but max is 6
[ 16.908638] usb 1-1: config 1 has an invalid interface number: 8 but max is 6
[ 16.915824] usb 1-1: config 1 has no interface number 3
[ 16.921100] usb 1-1: config 1 has no interface number 6
[ 16.927484] usb 1-1: New USB device found, idVendor=2c7c, idProduct=0455
[ 16.934223] usb 1-1: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[ 16.941387] usb 1-1: Product: LTE-A Module
[ 16.945513] usb 1-1: Manufacturer: Quectel
[ 16.949640] usb 1-1: SerialNumber: e56eb956
[ 16.986624] option 1-1:1.0: GSM modem (1-port) converter detected
[ 16.993230] usb 1-1: GSM modem (1-port) converter now attached to ttyUSB0
[ 17.004944] rmnet_usb 1-1:1.2 rmnet_usb1: register 'rmnet_usb' at usb-xhci-cdns3-1, RmNET device 1, f6:4a:77:19:56:8a
[ 17.031907] cdc_ether 1-1:1.4 usb1: register 'cdc_ether' at usb-xhci-cdns3-1, CDC Ethernet Device, 0e:29:34:12:74:d4
[ 17.045186] option 1-1:1.7: GSM modem (1-port) converter detected
[ 17.051660] usb 1-1: GSM modem (1-port) converter now attached to ttyUSB1
[ 17.058943] option 1-1:1.8: GSM modem (1-port) converter detected
[ 17.065513] usb 1-1: GSM modem (1-port) converter now attached to ttyUSB2
[ 27.869501] NETDEV WATCHDOG: usb1 (cdc_ether): transmit queue 0 timed out 4294897608
[ 27.877430] ------------[ cut here ]------------
[ 27.882070] WARNING: CPU: 1 PID: 0 at net/sched/sch_generic.c:319 dev_watchdog+0x2cc/0x2d8
[ 27.890338] Modules linked in: cryptodev(O)
[ 27.894540] CPU: 1 PID: 0 Comm: swapper/1 Tainted: G O 4.14.98 #1
[ 27.901762] Hardware name: Freescale i.MX8DX MEK - NIO (DT)
[ 27.907341] task: ffff80003a218c80 task.stack: ffff000009ab8000
[ 27.913267] PC is at dev_watchdog+0x2cc/0x2d8
[ 27.917630] LR is at dev_watchdog+0x2cc/0x2d8
[ 27.921987] pc : [<ffff000008a7003c>] lr : [<ffff000008a7003c>] pstate: 20000145
[ 27.929388] sp : ffff00000800bd90
[ 27.932707] x29: ffff00000800bd90 x28: 0000000000000020
[ 27.938023] x27: ffff000009925180 x26: ffff80003a218c80
[ 27.943340] x25: 00000000ffffffff x24: ffff000009926000
[ 27.948657] x23: 00000000fffeefc8 x22: ffff8000369bd41c
[ 27.953973] x21: 0000000000000000 x20: ffff8000369bd000
[ 27.959290] x19: ffff800036a3a600 x18: 0000000000000010
[ 27.964607] x17: 0000ffffb1352fc0 x16: 0000000000000000
[ 27.969924] x15: ffffffffffffffff x14: 32342074756f2064
[ 27.975240] x13: 656d697420302065 x12: ffff000009929e78
[ 27.980557] x11: ffff0000083b3e80 x10: 72656874655f6364
[ 27.985874] x9 : 0000000000000015 x8 : 3a474f4448435441
[ 27.991191] x7 : 572056454454454e x6 : 000000000000014c
[ 27.996507] x5 : 0000000000000002 x4 : 0000000000000002
[ 28.001824] x3 : 0000000000000000 x2 : 0000000000000040
[ 28.007141] x1 : ffff80003a218c80 x0 : 0000000000000049
[ 28.012458] Call trace:
[ 28.014911] Exception stack(0xffff00000800bc50 to 0xffff00000800bd90)
[ 28.021357] bc40: 0000000000000049 ffff80003a218c80
[ 28.029195] bc60: 0000000000000040 0000000000000000 0000000000000002 0000000000000002
[ 28.037030] bc80: 000000000000014c 572056454454454e 3a474f4448435441 0000000000000015
[ 28.044866] bca0: 72656874655f6364 ffff0000083b3e80 ffff000009929e78 656d697420302065
[ 28.052702] bcc0: 32342074756f2064 ffffffffffffffff 0000000000000000 0000ffffb1352fc0
[ 28.060538] bce0: 0000000000000010 ffff800036a3a600 ffff8000369bd000 0000000000000000
[ 28.068376] bd00: ffff8000369bd41c 00000000fffeefc8 ffff000009926000 00000000ffffffff
[ 28.076211] bd20: ffff80003a218c80 ffff000009925180 0000000000000020 ffff00000800bd90
[ 28.084049] bd40: ffff000008a7003c ffff00000800bd90 ffff000008a7003c 0000000020000145
[ 28.091883] bd60: ffff000008f9ed58 0000000000000000 0000ffffffffffff 00000000000000c0
[ 28.099717] bd80: ffff00000800bd90 ffff000008a7003c
[ 28.104602] [<ffff000008a7003c>] dev_watchdog+0x2cc/0x2d8
[ 28.110007] [<ffff000008125ba4>] call_timer_fn.isra.5+0x24/0x80
[ 28.115929] [<ffff000008125ca4>] expire_timers+0xa4/0xb0
[ 28.121245] [<ffff000008125d64>] run_timer_softirq+0xb4/0x170
[ 28.126999] [<ffff000008081204>] __do_softirq+0x124/0x218
[ 28.132402] [<ffff0000080cb648>] irq_exit+0xd0/0xf0
[ 28.137285] [<ffff00000810f278>] __handle_domain_irq+0x60/0xb8
[ 28.143121] [<ffff000008080fe0>] gic_handle_irq+0x78/0x174
[ 28.148609] Exception stack(0xffff000009abbe20 to 0xffff000009abbf60)
[ 28.155060] be20: 0000000000000000 0000000000000000 0000000000000001 0000000000000000
[ 28.162894] be40: ffff000009916108 ffff000009abbf50 000080003465f000 0000000000000000
[ 28.170730] be60: 0000000000000002 ffff000009abbee0 0000000000000870 0000000000000000
[ 28.178566] be80: 0000000000000000 0000000000000000 0000000000000000 00003712a2000000
[ 28.186403] bea0: ffff000008217408 0000ffffb1352fc0 0000000000000221 ffff000009912018
[ 28.194241] bec0: ffff000009929000 ffff000009929000 ffff00000991bc38 ffff000009929f18
[ 28.202075] bee0: 0000000000000000 0000000000000000 ffff80003a218c80 0000000000000000
[ 28.209913] bf00: 0000000000000000 ffff000009abbf60 ffff000008084e94 ffff000009abbf60
[ 28.217747] bf20: ffff000008084e98 0000000000000145 0000000000000000 0000000000000000
[ 28.225584] bf40: ffffffffffffffff ffff000008135f74 ffff000009abbf60 ffff000008084e98
[ 28.233427] [<ffff000008082a30>] el1_irq+0xb0/0x124
[ 28.238311] [<ffff000008084e98>] arch_cpu_idle+0x10/0x18
[ 28.243629] [<ffff0000081012a0>] do_idle+0x120/0x1e0
[ 28.248597] [<ffff0000081014f8>] cpu_startup_entry+0x20/0x28
[ 28.254262] [<ffff00000808f0f8>] secondary_start_kernel+0x110/0x120
[ 28.260531] ---[ end trace 59261fbdb6422a3d ]---
[ 96.545607] random: crng init done
[ 96.549033] random: 7 urandom warning(s) missed due to ratelimiting
[ 194.054727] sh (3106): drop_caches: 3
[ 276.197672] EXT4-fs (mmcblk0p5): mounted filesystem with ordered data mode. Opts: (null)

0 Kudos
Reply
0 Replies