Hello,
When I use SPI on i.MX8QM,booting log shows below error:
[ 3.657052] fsl_lpspi 5a000000.spi: spi_register_controller error.
[ 5.728282] fsl_lpspi 5a000000.spi: dma setup error -19, use pio
and spidev system point cannot open by application,what is the problem?
how to fixed it?
Hi,
My dts config like this:
Hi,
Also reproduce it on QM mek with LF_v5.10.72-2.2.0_images_IMX8QMMEK
Full log:
U-Boot 2021.04-lf_v2021.04+g263b27e076 (Nov 22 2021 - 01:39:23 +0000)
CPU: NXP i.MX8QM RevB A53 at 1200 MHz at 23C
Model: NXP i.MX8QM MEK
Board: iMX8QM MEK
Boot: MMC0
DRAM: 6 GiB
TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C0 0x51]
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... *** Warning - bad CRC, using default environment
[*]-Video Link 0it6263_i2c_reg_read, read err 3
faill to read from it6263 revision, ret 3
(1280 x 720)
[0] dpu@56180000, video
[1] lvds-channel@0, display
[2] lvds-to-hdmi-bridge@4c, video_bridge
In: serial
Out: serial
Err: serial
BuildInfo:
- SCFW 549b1e18, SECO-FW 2f7f6f59, IMX-MKIMAGE 7a277c8a, ATF 5782363
- U-Boot 2021.04-lf_v2021.04+g263b27e076
switch to partitions #0, OK
mmc0(part 0) is current device
flash target is MMC:0
Net: eth0: ethernet@5b040000 [PRIME], eth1: ethernet@5b050000
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0(part 0) is current device
Failed to load 'boot.scr'
30118400 bytes read in 124 ms (231.6 MiB/s)
Booting from mmc ...
106496 bytes read in 2 ms (50.8 MiB/s)
Loading hdp firmware from 0x000000009c000000 offset 0x0000000000002000
Loading hdp firmware Complete
135847 bytes read in 2 ms (64.8 MiB/s)
Moving Image from 0x80280000 to 0x80400000, end=82150000
## Flattened Device Tree blob at 83000000
Booting using the fdt blob at 0x83000000
ERROR: reserving fdt memory region failed (addr=901ff000 size=1000)
Using Device Tree in place at 0000000083000000, end 00000000830242a6
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[ 0.000000] Linux version 5.10.72-lts-5.10.y+ga68e31b63f86 (oe-user@oe-host) (aarch64-poky-linux-gcc (GCC) 10.2.0, GNU ld (GNU Binutils) 2.36.1.20210209) #1 SMP PREEMPT Tue Nov 23 06:02:20 UTC 2021
[ 0.000000] Machine model: Freescale i.MX8QM MEK
[ 0.000000] efi: UEFI not found.
[ 0.000000] OF: fdt: Reserved memory: failed to reserve memory for node 'm4@0x88000000': base 0x0000000088000000, size 128 MiB
[ 0.000000] Reserved memory: created CMA memory pool at 0x00000000c0000000, size 960 MiB
[ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x0000000090400000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vdevbuffer, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x0000000094300000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vdev0buffer@94300000, compatible id shared-dma-pool
[ 0.000000] NUMA: No NUMA configuration found
[ 0.000000] NUMA: Faking a node at [mem 0x0000000080200000-0x000000097fffffff]
[ 0.000000] NUMA: NODE_DATA [mem 0x97f408700-0x97f40afff]
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000080200000-0x00000000ffffffff]
[ 0.000000] DMA32 empty
[ 0.000000] Normal [mem 0x0000000100000000-0x000000097fffffff]
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000080200000-0x0000000083ffffff]
[ 0.000000] node 0: [mem 0x0000000084000000-0x00000000863fffff]
[ 0.000000] node 0: [mem 0x0000000086400000-0x000000008fffffff]
[ 0.000000] node 0: [mem 0x0000000090000000-0x000000009001ffff]
[ 0.000000] node 0: [mem 0x0000000090020000-0x00000000900fefff]
[ 0.000000] node 0: [mem 0x00000000900ff000-0x000000009011ffff]
[ 0.000000] node 0: [mem 0x0000000090120000-0x00000000901fefff]
[ 0.000000] node 0: [mem 0x00000000901ff000-0x00000000901fffff]
[ 0.000000] node 0: [mem 0x0000000090200000-0x00000000903fffff]
[ 0.000000] node 0: [mem 0x0000000090400000-0x00000000904fffff]
[ 0.000000] node 0: [mem 0x0000000090500000-0x0000000091ffffff]
[ 0.000000] node 0: [mem 0x0000000092000000-0x0000000094bfffff]
[ 0.000000] node 0: [mem 0x0000000094c00000-0x00000000ffffffff]
[ 0.000000] node 0: [mem 0x0000000880000000-0x000000088fffffff]
[ 0.000000] node 0: [mem 0x0000000890000000-0x000000097fffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000080200000-0x000000097fffffff]
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: MIGRATE_INFO_TYPE not supported.
[ 0.000000] psci: SMC Calling Convention v1.2
[ 0.000000] percpu: Embedded 23 pages/cpu s56280 r8192 d29736 u94208
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] CPU features: detected: ARM erratum 845719
[ 0.000000] CPU features: detected: GIC system register CPU interface
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 1547784
[ 0.000000] Policy zone: Normal
[ 0.000000] Kernel command line: console=ttyLP0,115200 earlycon root=/dev/mmcblk0p2 rootwait rw cpufreq.default_governor=SCHEDUTIL
[ 0.000000] Dentry cache hash table entries: 1048576 (order: 11, 8388608 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 524288 (order: 10, 4194304 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] software IO TLB: mapped [mem 0x00000000bc000000-0x00000000c0000000] (64MB)
[ 0.000000] Memory: 4610468K/6289408K available (17920K kernel code, 1508K rwdata, 6928K rodata, 2944K init, 552K bss, 695900K reserved, 983040K cma-reserved)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=6, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU event tracing is enabled.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=6.
[ 0.000000] Trampoline variant of Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=6
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: 512 SPIs implemented
[ 0.000000] GICv3: 0 Extended SPIs implemented
[ 0.000000] GICv3: Distributor has no Range Selector support
[ 0.000000] GICv3: 16 PPIs implemented
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000051b00000
[ 0.000000] ITS: No ITS available, not enabling LPIs
[ 0.000000] random: get_random_bytes called from start_kernel+0x320/0x4e4 with crng_init=0
[ 0.000000] arch_timer: cp15 timer(s) running at 8.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1d854df40, max_idle_ns: 440795202120 ns
[ 0.000004] sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199023255500ns
[ 0.000818] Console: colour dummy device 80x25
[ 0.000903] Calibrating delay loop (skipped), value calculated using timer frequency.. 16.00 BogoMIPS (lpj=32000)
[ 0.000916] pid_max: default: 32768 minimum: 301
[ 0.000990] LSM: Security Framework initializing
[ 0.001072] Mount-cache hash table entries: 16384 (order: 5, 131072 bytes, linear)
[ 0.001104] Mountpoint-cache hash table entries: 16384 (order: 5, 131072 bytes, linear)
[ 0.002611] rcu: Hierarchical SRCU implementation.
[ 0.004847] EFI services will not be available.
[ 0.005092] smp: Bringing up secondary CPUs ...
[ 0.005849] Detected VIPT I-cache on CPU1
[ 0.005879] GICv3: CPU1: found redistributor 1 region 0:0x0000000051b20000
[ 0.005925] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[ 0.006708] Detected VIPT I-cache on CPU2
[ 0.006726] GICv3: CPU2: found redistributor 2 region 0:0x0000000051b40000
[ 0.006749] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
[ 0.007491] Detected VIPT I-cache on CPU3
[ 0.007507] GICv3: CPU3: found redistributor 3 region 0:0x0000000051b60000
[ 0.007529] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
[ 0.009097] CPU features: detected: EL2 vector hardening
[ 0.009105] CPU features: detected: Spectre-v2
[ 0.009109] CPU features: detected: ARM errata 1165522, 1319367, or 1530923
[ 0.009113] Detected PIPT I-cache on CPU4
[ 0.009130] GICv3: CPU4: found redistributor 100 region 0:0x0000000051b80000
[ 0.009154] CPU4: Booted secondary processor 0x0000000100 [0x410fd082]
[ 0.009921] Detected PIPT I-cache on CPU5
[ 0.009933] GICv3: CPU5: found redistributor 101 region 0:0x0000000051ba0000
[ 0.009950] CPU5: Booted secondary processor 0x0000000101 [0x410fd082]
[ 0.010012] smp: Brought up 1 node, 6 CPUs
[ 0.010050] SMP: Total of 6 processors activated.
[ 0.010057] CPU features: detected: 32-bit EL0 Support
[ 0.010063] CPU features: detected: CRC32 instructions
[ 0.010069] CPU features: detected: 32-bit EL1 Support
[ 0.024707] CPU: All CPU(s) started at EL2
[ 0.024742] alternatives: patching kernel code
[ 0.025807] devtmpfs: initialized
[ 0.042651] KASLR disabled due to lack of seed
[ 0.042820] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.042838] futex hash table entries: 2048 (order: 5, 131072 bytes, linear)
[ 0.075004] pinctrl core: initialized pinctrl subsystem
[ 0.075635] DMI not present or invalid.
[ 0.076078] NET: Registered protocol family 16
[ 0.080441] DMA: preallocated 1024 KiB GFP_KERNEL pool for atomic allocations
[ 0.081087] DMA: preallocated 1024 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[ 0.081833] DMA: preallocated 1024 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[ 0.081886] audit: initializing netlink subsys (disabled)
[ 0.082068] audit: type=2000 audit(0.080:1): state=initialized audit_enabled=0 res=1
[ 0.082379] thermal_sys: Registered thermal governor 'step_wise'
[ 0.082382] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.082837] cpuidle: using governor menu
[ 0.083003] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.083118] ASID allocator initialised with 65536 entries
[ 0.085264] Serial: AMBA PL011 UART driver
[ 0.085330] imx mu driver is registered.
[ 0.085351] imx rpmsg driver is registered.
[ 0.186389] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.186401] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.186408] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.186414] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
[ 0.187358] cryptd: max_cpu_qlen set to 1000
[ 0.191966] ACPI: Interpreter disabled.
[ 0.194227] iommu: Default domain type: Translated
[ 0.194377] vgaarb: loaded
[ 0.194686] SCSI subsystem initialized
[ 0.195015] usbcore: registered new interface driver usbfs
[ 0.195056] usbcore: registered new interface driver hub
[ 0.195085] usbcore: registered new device driver usb
[ 0.197276] mc: Linux media interface: v0.10
[ 0.197309] videodev: Linux video capture interface: v2.00
[ 0.197375] pps_core: LinuxPPS API ver. 1 registered
[ 0.197382] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.197396] PTP clock support registered
[ 0.197774] EDAC MC: Ver: 3.0.0
[ 0.199799] FPGA manager framework
[ 0.199882] Advanced Linux Sound Architecture Driver Initialized.
[ 0.200782] Bluetooth: Core ver 2.22
[ 0.200808] NET: Registered protocol family 31
[ 0.200814] Bluetooth: HCI device and connection manager initialized
[ 0.200825] Bluetooth: HCI socket layer initialized
[ 0.200833] Bluetooth: L2CAP socket layer initialized
[ 0.200852] Bluetooth: SCO socket layer initialized
[ 0.202363] imx-scu scu: NXP i.MX SCU Initialized
[ 0.241054] random: fast init done
[ 0.321480] imx8qm-pinctrl scu:pinctrl: Invalid fsl,pins or pins property in node /scu/pinctrl/wifi_initgrp
[ 0.321505] imx8qm-pinctrl scu:pinctrl: initialized IMX pinctrl driver
[ 0.325875] clocksource: Switched to clocksource arch_sys_counter
[ 0.326150] VFS: Disk quotas dquot_6.6.0
[ 0.326220] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.326402] pnp: PnP ACPI: disabled
[ 0.366693] NET: Registered protocol family 2
[ 0.367064] IP idents hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[ 0.369109] tcp_listen_portaddr_hash hash table entries: 4096 (order: 4, 65536 bytes, linear)
[ 0.369191] TCP established hash table entries: 65536 (order: 7, 524288 bytes, linear)
[ 0.369454] TCP bind hash table entries: 65536 (order: 8, 1048576 bytes, linear)
[ 0.369991] TCP: Hash tables configured (established 65536 bind 65536)
[ 0.370114] UDP hash table entries: 4096 (order: 5, 131072 bytes, linear)
[ 0.370216] UDP-Lite hash table entries: 4096 (order: 5, 131072 bytes, linear)
[ 0.370408] NET: Registered protocol family 1
[ 0.370782] RPC: Registered named UNIX socket transport module.
[ 0.370793] RPC: Registered udp transport module.
[ 0.370798] RPC: Registered tcp transport module.
[ 0.370803] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.371518] PCI: CLS 0 bytes, default 64
[ 0.372259] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
[ 0.374402] kvm [1]: IPA Size Limit: 40 bits
[ 0.375486] kvm [1]: vgic-v2@52020000
[ 0.375517] kvm [1]: GIC system register CPU interface enabled
[ 0.375642] kvm [1]: vgic interrupt IRQ9
[ 0.375798] kvm [1]: Hyp mode initialized successfully
[ 0.379388] Initialise system trusted keyrings
[ 0.379498] workingset: timestamp_bits=42 max_order=21 bucket_order=0
[ 0.384804] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.385339] NFS: Registering the id_resolver key type
[ 0.385359] Key type id_resolver registered
[ 0.385364] Key type id_legacy registered
[ 0.385438] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 0.385446] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[ 0.385472] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
[ 0.385839] 9p: Installing v9fs 9p2000 file system support
[ 0.421892] Key type asymmetric registered
[ 0.421899] Asymmetric key parser 'x509' registered
[ 0.421932] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 241)
[ 0.421940] io scheduler mq-deadline registered
[ 0.421946] io scheduler kyber registered
[ 0.442429] imx6q-pcie 5f010000.pcie: supply epdev_on not found, using dummy regulator
[ 0.446442] pwm-backlight lvds_backlight@0: supply power not found, using dummy regulator
[ 0.446808] pwm-backlight lvds_backlight@1: supply power not found, using dummy regulator
[ 0.447888] EINJ: ACPI disabled.
[ 0.590298] mxs-dma 5b810000.dma-apbh: initialized
[ 0.596343] Bus freq driver module loaded
[ 0.603808] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 0.608418] 5a060000.serial: ttyLP0 at MMIO 0x5a060010 (irq = 61, base_baud = 5000000) is a FSL_LPUART
[ 1.804368] printk: console [ttyLP0] enabled
[ 1.809415] 5a070000.serial: ttyLP1 at MMIO 0x5a070010 (irq = 62, base_baud = 5000000) is a FSL_LPUART
[ 1.820365] arm-smmu 51400000.iommu: probing hardware configuration...
[ 1.826915] arm-smmu 51400000.iommu: SMMUv2 with:
[ 1.831622] arm-smmu 51400000.iommu: stage 1 translation
[ 1.837031] arm-smmu 51400000.iommu: stage 2 translation
[ 1.842431] arm-smmu 51400000.iommu: nested translation
[ 1.847749] arm-smmu 51400000.iommu: stream matching with 32 register groups
[ 1.854894] arm-smmu 51400000.iommu: 32 context banks (0 stage-2 only)
[ 1.861509] arm-smmu 51400000.iommu: Supported page sizes: 0x61311000
[ 1.868042] arm-smmu 51400000.iommu: Stage-1: 48-bit VA -> 48-bit IPA
[ 1.874578] arm-smmu 51400000.iommu: Stage-2: 48-bit IPA -> 48-bit PA
[ 1.959214] nwl-dsi 56228000.dsi_host: [drm:nwl_dsi_probe] *ERROR* Failed to get device IRQ: -517
[ 1.968450] nwl-dsi 57228000.dsi_host: [drm:nwl_dsi_probe] *ERROR* Failed to get device IRQ: -517
[ 1.983585] loop: module loaded
[ 1.988343] megasas: 07.714.04.00-rc1
[ 1.994255] ahci-imx 5f020000.sata: Adding to iommu group 0
[ 2.000042] ahci-imx 5f020000.sata: phy impedance ratio is not specified.
[ 2.006888] ahci-imx 5f020000.sata: No cache used with register defaults set!
[ 2.014619] imx ahci driver is registered.
[ 2.023301] fsl_lpspi 5a020000.spi: spi_register_controller error.
[ 2.032571] spi-nor spi0.0: mt35xu512aba (65536 Kbytes)
[ 2.044009] libphy: Fixed MDIO Bus: probed
[ 2.049274] tun: Universal TUN/TAP device driver, 1.6
[ 2.055552] thunder_xcv, ver 1.0
[ 2.058813] thunder_bgx, ver 1.0
[ 2.062061] nicpf, ver 1.0
[ 2.065541] fec 5b040000.ethernet: Adding to iommu group 1
[ 2.072218] pps pps0: new PPS source ptp0
[ 2.077646] libphy: fec_enet_mii_bus: probed
[ 2.082815] mdio_bus 5b040000.ethernet-1: MDIO device at address 1 is missing.
[ 2.090372] fec 5b040000.ethernet eth0: registered PHC device 0
[ 2.097019] fec 5b050000.ethernet: Adding to iommu group 1
[ 2.107399] hclge is initializing
[ 2.110742] hns3: Hisilicon Ethernet Network Driver for Hip08 Family - version
[ 2.117972] hns3: Copyright (c) 2017 Huawei Corporation.
[ 2.123330] e1000: Intel(R) PRO/1000 Network Driver
[ 2.128227] e1000: Copyright (c) 1999-2006 Intel Corporation.
[ 2.134020] e1000e: Intel(R) PRO/1000 Network Driver
[ 2.138987] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[ 2.144936] igb: Intel(R) Gigabit Ethernet Network Driver
[ 2.150340] igb: Copyright (c) 2007-2014 Intel Corporation.
[ 2.155932] igbvf: Intel(R) Gigabit Virtual Function Network Driver
[ 2.162210] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 2.168556] sky2: driver version 1.30
[ 2.173446] usbcore: registered new interface driver r8152
[ 2.178965] usbcore: registered new interface driver asix
[ 2.184409] usbcore: registered new interface driver ax88179_178a
[ 2.190519] usbcore: registered new interface driver cdc_ether
[ 2.196378] usbcore: registered new interface driver net1080
[ 2.202057] usbcore: registered new interface driver cdc_subset
[ 2.207995] usbcore: registered new interface driver zaurus
[ 2.213593] usbcore: registered new interface driver cdc_ncm
[ 2.219443] VFIO - User Level meta-driver version: 0.3
[ 2.228267] cdns3-imx 5b110000.usb: Adding to iommu group 2
[ 2.234965] cdns-usb3 5b130000.usb: Adding to iommu group 2
[ 2.241286] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 2.247821] ehci-pci: EHCI PCI platform driver
[ 2.252313] ehci-platform: EHCI generic platform driver
[ 2.258079] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
[ 2.264278] ohci-pci: OHCI PCI platform driver
[ 2.268757] ohci-platform: OHCI generic platform driver
[ 2.275306] usbcore: registered new interface driver uas
[ 2.280653] usbcore: registered new interface driver usb-storage
[ 2.286711] usbcore: registered new interface driver usbserial_generic
[ 2.293250] usbserial: USB Serial support registered for generic
[ 2.299311] usbcore: registered new interface driver ftdi_sio
[ 2.305077] usbserial: USB Serial support registered for FTDI USB Serial Device
[ 2.312402] usbcore: registered new interface driver usb_serial_simple
[ 2.318943] usbserial: USB Serial support registered for carelink
[ 2.325044] usbserial: USB Serial support registered for zio
[ 2.330721] usbserial: USB Serial support registered for funsoft
[ 2.336741] usbserial: USB Serial support registered for flashloader
[ 2.343110] usbserial: USB Serial support registered for google
[ 2.349040] usbserial: USB Serial support registered for libtransistor
[ 2.355582] usbserial: USB Serial support registered for vivopay
[ 2.361603] usbserial: USB Serial support registered for moto_modem
[ 2.367886] usbserial: USB Serial support registered for motorola_tetra
[ 2.374515] usbserial: USB Serial support registered for novatel_gps
[ 2.380887] usbserial: USB Serial support registered for hp4x
[ 2.386642] usbserial: USB Serial support registered for suunto
[ 2.392576] usbserial: USB Serial support registered for siemens_mpi
[ 2.398953] usbcore: registered new interface driver usb_ehset_test
[ 2.411020] input: sc-powerkey as /devices/platform/sc-powerkey/input/input0
[ 2.421258] imx-sc-rtc scu:rtc: registered as rtc0
[ 2.426398] imx-sc-rtc scu:rtc: setting system clock to 1970-01-01T04:17:51 UTC (15471)
[ 2.435161] i2c /dev entries driver
[ 2.446354] Bluetooth: HCI UART driver ver 2.3
[ 2.450816] Bluetooth: HCI UART protocol H4 registered
[ 2.455962] Bluetooth: HCI UART protocol BCSP registered
[ 2.461289] Bluetooth: HCI UART protocol LL registered
[ 2.466426] Bluetooth: HCI UART protocol ATH3K registered
[ 2.471839] Bluetooth: HCI UART protocol Three-wire (H5) registered
[ 2.478318] Bluetooth: HCI UART protocol Broadcom registered
[ 2.483996] Bluetooth: HCI UART protocol QCA registered
[ 2.493300] sdhci: Secure Digital Host Controller Interface driver
[ 2.499540] sdhci: Copyright(c) Pierre Ossman
[ 2.504783] Synopsys Designware Multimedia Card Interface Driver
[ 2.512208] sdhci-pltfm: SDHCI platform and OF driver helper
[ 2.519584] sdhci-esdhc-imx 5b020000.mmc: Adding to iommu group 3
[ 2.519741] sdhci-esdhc-imx 5b010000.mmc: Adding to iommu group 3
[ 2.532027] ledtrig-cpu: registered to indicate activity on CPUs
[ 2.532259] sdhci-esdhc-imx 5b020000.mmc: voltage-ranges unspecified
[ 2.532617] sdhci-esdhc-imx 5b010000.mmc: voltage-ranges unspecified
[ 2.540003] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[ 2.557523] usbcore: registered new interface driver usbhid
[ 2.563109] usbhid: USB HID core driver
[ 2.564194] mmc0: SDHCI controller on 5b010000.mmc [5b010000.mmc] using ADMA
[ 2.585882] mxc-mipi-csi2 58227000.csi: lanes: 4, name: mxc-mipi-csi2.0
[ 2.609873] mxc-mipi-csi2 58247000.csi: lanes: 4, name: mxc-mipi-csi2.1
[ 2.618523] mxc-isi 58100000.isi: mxc_isi.0 registered successfully
[ 2.625842] mxc-isi 58110000.isi: mxc_isi.1 registered successfully
[ 2.632942] mxc-isi 58120000.isi: mxc_isi.2 registered successfully
[ 2.640215] mxc-isi 58130000.isi: mxc_isi.3 registered successfully
[ 2.647171] mxc-isi 58140000.isi: mxc_isi.4 registered successfully
[ 2.654149] mxc-isi 58150000.isi: mxc_isi.5 registered successfully
[ 2.661087] mxc-isi 58160000.isi: mxc_isi.6 registered successfully
[ 2.663774] mmc0: new HS400 MMC card at address 0001
[ 2.668058] mxc-isi 58170000.isi: mxc_isi.7 registered successfully
[ 2.673171] mmcblk0: mmc0:0001 R1J57L 29.1 GiB
[ 2.683482] mmcblk0boot0: mmc0:0001 R1J57L partition 1 8.00 MiB
[ 2.683793] remoteproc remoteproc0: releasing imx-rproc
[ 2.689690] mmcblk0boot1: mmc0:0001 R1J57L partition 2 8.00 MiB
[ 2.694744] remoteproc remoteproc0: releasing imx-rproc
[ 2.700824] mmcblk0rpmb: mmc0:0001 R1J57L partition 3 4.00 MiB, chardev (511:0)
[ 2.706699] remoteproc remoteproc0: imx-dsp-rproc is available
[ 2.714601] mmcblk0: p1 p2
[ 2.731812] Galcore version 6.4.3.p2.336687
[ 2.748966] [drm] Initialized vivante 1.0.0 20170808 for 80000000.imx8_gpu1_ss on minor 0
[ 2.758627] mxc_emvsim 5a0d0000.sim0: emvsim register success
[ 2.768280] [VPU Decoder] init rtx channel failed, ret: -517
[ 2.773956] [VPU Decoder] failed to request mailbox, ret = -517
[ 2.783480] [VPU Encoder] init rtx channel failed, ret: -517
[ 2.789257] [VPU Encoder] init rtx channel failed, ret: -517
[ 2.795049] [VPU Encoder] fail to request mailbox, ret = -517
[ 2.833360] fsl-audmix 59840000.amix: DAI FE name:HiFi-AUDMIX-FE-ai@59820000
[ 2.840468] fsl-audmix 59840000.amix: DAI FE name:HiFi-AUDMIX-FE-ai@59830000
[ 2.854646] NET: Registered protocol family 26
[ 2.859412] NET: Registered protocol family 10
[ 2.864405] Segment Routing with IPv6
[ 2.868106] NET: Registered protocol family 17
[ 2.872649] Bluetooth: RFCOMM TTY layer initialized
[ 2.877534] Bluetooth: RFCOMM socket layer initialized
[ 2.882693] Bluetooth: RFCOMM ver 1.11
[ 2.886460] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 2.891785] Bluetooth: BNEP filters: protocol multicast
[ 2.897018] Bluetooth: BNEP socket layer initialized
[ 2.901985] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 2.907910] Bluetooth: HIDP socket layer initialized
[ 2.912899] 8021q: 802.1Q VLAN Support v1.8
[ 2.917091] lib80211: common routines for IEEE802.11 drivers
[ 2.922829] 9pnet: Installing 9P2000 support
[ 2.927125] tsn generic netlink module v1 init...
[ 2.931870] Key type dns_resolver registered
[ 2.936305] registered taskstats version 1
[ 2.940418] Loading compiled-in X.509 certificates
[ 2.963870] mxs_phy 5b100000.usbphy: supply phy-3p0 not found, using dummy regulator
[ 2.983989] imx-lpi2c 3b230000.i2c: can't get the TX DMA channel, error -19!
[ 2.991062] imx-lpi2c 3b230000.i2c: error -ENODEV: dma setup error -19, use pio
[ 2.998636] pca953x 2-0020: using no AI
[ 3.018003] cs42xx8 2-0048: failed to get device ID, ret = -5
[ 3.023899] cs42xx8: probe of 2-0048 failed with error -5
[ 3.029339] i2c i2c-2: LPI2C adapter registered
[ 3.034771] imx-lpi2c 5a800000.i2c: can't get the TX DMA channel, error -19!
[ 3.041845] imx-lpi2c 5a800000.i2c: error -ENODEV: dma setup error -19, use pio
[ 3.049595] isl29023 3-0044: supply vdd not found, using dummy regulator
[ 3.062892] input: isl29023 light sensor as /devices/virtual/input/input1
[ 3.070191] isl29023 3-0044: driver version 1.0 enabled
[ 3.076162] input: fxos8700 as /devices/platform/bus@5a000000/5a800000.i2c/i2c-3/3-001e/input/input2
[ 3.087239] fxos8700 device driver probe successfully
[ 3.087858] input: fxas2100x as /devices/platform/bus@5a000000/5a800000.i2c/i2c-3/3-0020/input/input3
[ 3.102821] fxas2100x 3-0020: fxas2100x device driver probe successfully
[ 3.109730] max732x 3-0068: failed reading
[ 3.113836] max732x: probe of 3-0068 failed with error -5
[ 3.119800] read mpl3115 chip id 0xc4
[ 3.123515] input: mpl3115 as /devices/virtual/input/input4
[ 3.129770] mpl3115 device driver probe successfully
[ 3.131045] i2c i2c-3: LPI2C adapter registered
[ 3.141264] gpio-494 (scl): enforced open drain please flag it properly in DT/ACPI DSDT/board file
[ 3.150245] imx-lpi2c 5a810000.i2c: using scl,sda for recovery
[ 3.156089] imx-lpi2c 5a810000.i2c: can't get the TX DMA channel, error -19!
[ 3.163140] imx-lpi2c 5a810000.i2c: error -ENODEV: dma setup error -19, use pio
[ 3.176173] i2c i2c-4: LPI2C adapter registered
[ 3.181636] imx-lpi2c 58226000.i2c: can't get the TX DMA channel, error -19!
[ 3.188699] imx-lpi2c 58226000.i2c: error -ENODEV: dma setup error -19, use pio
[ 3.206025] max9286_mipi 5-006a: max9286_read_reg:read reg error: reg=1e
[ 3.212739] max9286 is not found, chip id reg 0x1e = 0x(ffffffff)
[ 3.218880] i2c i2c-5: LPI2C adapter registered
[ 3.224264] imx-lpi2c 58246000.i2c: can't get the TX DMA channel, error -19!
[ 3.231335] imx-lpi2c 58246000.i2c: error -ENODEV: dma setup error -19, use pio
[ 3.250063] max9286_mipi 6-006a: max9286_read_reg:read reg error: reg=1e
[ 3.256781] max9286 is not found, chip id reg 0x1e = 0x(ffffffff)
[ 3.262924] i2c i2c-6: LPI2C adapter registered
[ 3.274716] pwm-backlight lvds_backlight@0: supply power not found, using dummy regulator
[ 3.275164] imx6q-pcie 5f000000.pcie: No cache used with register defaults set!
[ 3.275400] imx6q-pcie 5f010000.pcie: No cache used with register defaults set!
[ 3.286011] pwm-backlight lvds_backlight@1: supply power not found, using dummy regulator
[ 3.301918] imx6q-pcie 5f010000.pcie: PCIe PLL locked after 0 us.
[ 3.312066] imx6q-pcie 5f010000.pcie: host bridge /bus@5f000000/pcie@0x5f010000 ranges:
[ 3.317933] imx6q-pcie 5f000000.pcie: PCIe PLL locked after 0 us.
[ 3.320179] imx6q-pcie 5f010000.pcie: IO 0x007ff80000..0x007ff8ffff -> 0x0000000000
[ 3.334437] imx6q-pcie 5f010000.pcie: MEM 0x0070000000..0x007fefffff -> 0x0070000000
[ 3.342905] imx6q-pcie 5f000000.pcie: host bridge /bus@5f000000/pcie@0x5f000000 ranges:
[ 3.351224] imx6q-pcie 5f000000.pcie: IO 0x006ff80000..0x006ff8ffff -> 0x0000000000
[ 3.359439] imx6q-pcie 5f000000.pcie: MEM 0x0060000000..0x006fefffff -> 0x0060000000
[ 3.360740] dpu-core 56180000.dpu: driver probed
[ 3.374471] dpu-core 57180000.dpu: driver probed
[ 3.380951] imx-drm display-subsystem: bound imx-drm-dpu-bliteng.2 (ops dpu_bliteng_ops)
[ 3.389169] imx-drm display-subsystem: bound imx-drm-dpu-bliteng.5 (ops dpu_bliteng_ops)
[ 3.397588] imx-drm display-subsystem: bound imx-dpu-crtc.0 (ops dpu_crtc_ops)
[ 3.405318] imx-drm display-subsystem: bound imx-dpu-crtc.1 (ops dpu_crtc_ops)
[ 3.412827] imx-drm display-subsystem: bound imx-dpu-crtc.3 (ops dpu_crtc_ops)
[ 3.420541] imx-drm display-subsystem: bound imx-dpu-crtc.4 (ops dpu_crtc_ops)
[ 3.429306] ahci-imx 5f020000.sata: phy impedance ratio is not specified.
[ 3.436164] ahci-imx 5f020000.sata: No cache used with register defaults set!
[ 3.443526] ahci-imx 5f020000.sata: supply ahci not found, using dummy regulator
[ 3.451020] ahci-imx 5f020000.sata: supply phy not found, using dummy regulator
[ 3.458360] ahci-imx 5f020000.sata: supply target not found, using dummy regulator
[ 3.466076] ahci-imx 5f020000.sata: external osc is used.
[ 3.473873] ahci-imx 5f020000.sata: no ahb clock.
[ 3.478636] ahci-imx 5f020000.sata: AHCI 0001.0301 32 slots 1 ports 6 Gbps 0x1 impl platform mode
[ 3.487517] ahci-imx 5f020000.sata: flags: 64bit ncq sntf pm clo only pmp fbs pio slum part ccc sadm sds apst
[ 3.498261] scsi host0: ahci-imx
[ 3.501636] ata1: SATA max UDMA/133 mmio [mem 0x5f020000-0x5f02ffff] port 0x100 irq 119
[ 3.510810] fsl_lpspi 5a020000.spi: dma setup error -19, use pio
[ 3.589842] imx-rproc imx8qm_cm4@0: mbox_request_channel_byname() could not locate channel named "txdb"
[ 3.592481] sdhci-esdhc-imx 5b020000.mmc: voltage-ranges unspecified
[ 3.599258] imx-rproc imx8qm_cm4@0: No txdb, ret -22
[ 3.610907] remoteproc remoteproc1: imx-rproc is available
[ 3.611152] sdhci-esdhc-imx 5b020000.mmc: Got CD GPIO
[ 3.621540] sdhci-esdhc-imx 5b020000.mmc: Got WP GPIO
[ 3.621566] imx-rproc imx8x_cm4@1: mbox_request_channel_byname() could not locate channel named "txdb"
[ 3.635939] imx-rproc imx8x_cm4@1: No txdb, ret -22
[ 3.641612] remoteproc remoteproc2: imx-rproc is available
[ 3.658727] mmc1: SDHCI controller on 5b020000.mmc [5b020000.mmc] using ADMA
[ 3.664762] debugfs: File 'Playback' in directory 'dapm' already present!
[ 3.672635] debugfs: File 'Capture' in directory 'dapm' already present!
[ 3.795535] can01-stby: supplied by can01-en
[ 3.800715] can2-stby: supplied by can2-en
[ 3.816950] imx-lpi2c 56247000.i2c: can't get the TX DMA channel, error -19!
[ 3.824052] imx-lpi2c 56247000.i2c: error -ENODEV: dma setup error -19, use pio
[ 3.824276] ata1: SATA link down (SStatus 0 SControl 300)
[ 3.832558] it6263 7-004c: Probe failed. Remote port 'lvds-channel@0' disabled
[ 3.844146] i2c i2c-7: LPI2C adapter registered
[ 3.849622] imx-lpi2c 57247000.i2c: can't get the TX DMA channel, error -19!
[ 3.856713] imx-lpi2c 57247000.i2c: error -ENODEV: dma setup error -19, use pio
[ 3.864793] it6263 8-004c: Probe failed. Remote port 'lvds-channel@0' disabled
[ 3.872094] i2c i2c-8: LPI2C adapter registered
[ 3.877481] imx-lpi2c 56226000.i2c: can't get the TX DMA channel, error -19!
[ 3.884555] imx-lpi2c 56226000.i2c: error -ENODEV: dma setup error -19, use pio
[ 3.892292] adv7511 9-003d: supply avdd not found, using dummy regulator
[ 3.899097] adv7511 9-003d: supply dvdd not found, using dummy regulator
[ 3.905854] adv7511 9-003d: supply pvdd not found, using dummy regulator
[ 3.912604] adv7511 9-003d: supply a2vdd not found, using dummy regulator
[ 3.919419] adv7511 9-003d: supply v3p3 not found, using dummy regulator
[ 3.926152] adv7511 9-003d: supply v1p2 not found, using dummy regulator
[ 3.933308] adv7511 9-003d: Probe failed. Remote port 'dsi_host@56228000' disabled
[ 3.940950] i2c i2c-9: LPI2C adapter registered
[ 3.946389] imx-lpi2c 57226000.i2c: can't get the TX DMA channel, error -19!
[ 3.953456] imx-lpi2c 57226000.i2c: error -ENODEV: dma setup error -19, use pio
[ 3.961134] adv7511 10-003d: supply avdd not found, using dummy regulator
[ 3.968020] adv7511 10-003d: supply dvdd not found, using dummy regulator
[ 3.974842] adv7511 10-003d: supply pvdd not found, using dummy regulator
[ 3.981657] adv7511 10-003d: supply a2vdd not found, using dummy regulator
[ 3.988565] adv7511 10-003d: supply v3p3 not found, using dummy regulator
[ 3.995389] adv7511 10-003d: supply v1p2 not found, using dummy regulator
[ 4.002664] adv7511 10-003d: Probe failed. Remote port 'dsi_host@57228000' disabled
[ 4.010398] i2c i2c-10: LPI2C adapter registered
[ 4.016836] imx-drm display-subsystem: bound imx-drm-dpu-bliteng.2 (ops dpu_bliteng_ops)
[ 4.025043] imx-drm display-subsystem: bound imx-drm-dpu-bliteng.5 (ops dpu_bliteng_ops)
[ 4.033384] imx-drm display-subsystem: bound imx-dpu-crtc.0 (ops dpu_crtc_ops)
[ 4.040775] imx-drm display-subsystem: bound imx-dpu-crtc.1 (ops dpu_crtc_ops)
[ 4.048272] imx-drm display-subsystem: bound imx-dpu-crtc.3 (ops dpu_crtc_ops)
[ 4.055691] imx-drm display-subsystem: bound imx-dpu-crtc.4 (ops dpu_crtc_ops)
[ 4.062953] imx-drm display-subsystem: bound 56228000.dsi_host (ops nwl_dsi_component_ops)
[ 4.071348] imx-drm display-subsystem: bound bus@56240000:ldb@562410e0 (ops imx8qm_ldb_ops)
[ 4.079725] imx-drm display-subsystem: bound 57228000.dsi_host (ops nwl_dsi_component_ops)
[ 4.088060] imx-drm display-subsystem: bound bus@57240000:ldb@572410e0 (ops imx8qm_ldb_ops)
[ 4.096675] [drm] Initialized imx-drm 1.0.0 20120507 for display-subsystem on minor 1
[ 4.109626] imx8qxp-lpcg-clk 5ac90000.clock-controller: deferred probe timeout, ignoring dependency
[ 4.118714] imx8qxp-lpcg-clk: probe of 5ac90000.clock-controller failed with error -110
[ 4.134682] isi-m2m 58100000.isi:m2m_device: Register m2m success for ISI.0
[ 4.142414] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[ 4.152329] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[ 4.159005] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
[ 4.167700] platform regulatory.0: Falling back to sysfs fallback for: regulatory.db
[ 4.193774] ALSA device list:
[ 4.197878] #0: imx-audmix
[ 4.200765] #1: bt-sco-audio
[ 4.203827] #2: wm8960-audio
[ 4.329905] imx6q-pcie 5f010000.pcie: Phy link never came up
[ 4.335878] imx6q-pcie 5f010000.pcie: failed to initialize host
[ 4.341821] imx6q-pcie 5f010000.pcie: unable to add pcie port.
[ 4.358510] imx6q-pcie 5f000000.pcie: Phy link never came up
[ 4.364271] imx6q-pcie 5f000000.pcie: failed to initialize host
[ 4.370221] imx6q-pcie 5f000000.pcie: unable to add pcie port.
[ 4.385443] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 4.393665] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 4.400085] devtmpfs: mounted
[ 4.404743] Freeing unused kernel memory: 2944K
[ 4.409533] Run /sbin/init as init process
[ 4.503144] systemd[1]: System time before build time, advancing clock.
[ 4.520128] systemd[1]: systemd 247.6+ running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR -SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -ZSTD -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid)
[ 4.542618] systemd[1]: Detected architecture arm64.
Welcome to NXP i.MX Release Distro 5.10-hardknott (hardknott)!
[ 4.578803] systemd[1]: Set hostname to <imx8qmmek>.
[ 4.587189] random: systemd: uninitialized urandom read (16 bytes read)
[ 4.594076] systemd[1]: Initializing machine ID from random generator.
[ 4.652756] systemd-sysv-generator[272]: SysV service '/etc/init.d/reboot' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 4.676871] systemd-sysv-generator[272]: SysV service '/etc/init.d/sendsigs' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 4.701009] systemd-sysv-generator[272]: SysV service '/etc/init.d/single' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 4.725320] systemd-sysv-generator[272]: SysV service '/etc/init.d/umountfs' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 4.749563] systemd-sysv-generator[272]: SysV service '/etc/init.d/save-rtc.sh' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 4.773959] systemd-sysv-generator[272]: SysV service '/etc/init.d/umountnfs.sh' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 4.798494] systemd-sysv-generator[272]: SysV service '/etc/init.d/halt' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 4.822341] systemd-sysv-generator[272]: SysV service '/etc/init.d/rc.local' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 5.018326] systemd[1]: /lib/systemd/system/docker.socket:6: ListenStream= references a path below legacy directory /var/run/, updating /var/run/docker.sock → /run/docker.sock; please update the unit file accordingly.
[ 5.145621] systemd[1]: Queued start job for default target Graphical Interface.
[ 5.154283] random: systemd: uninitialized urandom read (16 bytes read)
[ 5.243655] systemd[1]: Created slice system-getty.slice.
[ OK ] Created slice system-getty.slice.
[ 5.266044] random: systemd: uninitialized urandom read (16 bytes read)
[ 5.274441] systemd[1]: Created slice system-modprobe.slice.
[ OK ] Created slice system-modprobe.slice.
[ 5.295830] systemd[1]: Created slice system-serial\x2dgetty.slice.
[ OK ] Created slice system-serial\x2dgetty.slice.
[ 5.320084] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 5.342240] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Started Dispatch Password …ts to Console Directory Watch.
[ 5.366284] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ OK ] Started Forward Password R…uests to Wall Directory Watch.
[ 5.390445] systemd[1]: Reached target Host and Network Name Lookups.
[ OK ] Reached target Host and Network Name Lookups.
[ 5.414132] systemd[1]: Reached target Paths.
[ OK ] Reached target Paths.
[ 5.434092] systemd[1]: Reached target Remote File Systems.
[ OK ] Reached target Remote File Systems.
[ 5.454064] systemd[1]: Reached target Slices.
[ OK ] Reached target Slices.
[ 5.474122] systemd[1]: Reached target Swap.
[ OK ] Reached target Swap.
[ 5.499043] systemd[1]: Listening on RPCbind Server Activation Socket.
[ OK ] Listening on RPCbind Server Activation Socket.
[ 5.522118] systemd[1]: Reached target RPC Port Mapper.
[ OK ] Reached target RPC Port Mapper.
[ 5.542932] systemd[1]: Listening on Syslog Socket.
[ OK ] Listening on Syslog Socket.
[ 5.562333] systemd[1]: Listening on initctl Compatibility Named Pipe.
[ OK ] Listening on initctl Compatibility Named Pipe.
[ 5.586943] systemd[1]: Listening on Journal Audit Socket.
[ OK ] Listening on Journal Audit Socket.
[ 5.610527] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
[ 5.634663] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Journal Socket.
[ 5.654874] systemd[1]: Listening on Network Service Netlink Socket.
[ OK ] Listening on Network Service Netlink Socket.
[ 5.680285] systemd[1]: Listening on udev Control Socket.
[ OK ] Listening on udev Control Socket.
[ 5.702512] systemd[1]: Listening on udev Kernel Socket.
[ OK ] Listening on udev Kernel Socket.
[ 5.722500] systemd[1]: Listening on User Database Manager Socket.
[ OK ] Listening on User Database Manager Socket.
[ 5.752214] systemd[1]: Mounting Huge Pages File System...
Mounting Huge Pages File System...
[ 5.780129] systemd[1]: Mounting POSIX Message Queue File System...
Mounting POSIX Message Queue File System...
[ 5.808482] systemd[1]: Mounting Kernel Debug File System...
Mounting Kernel Debug File System...
[ 5.830691] systemd[1]: Condition check resulted in Kernel Trace File System being skipped.
[ 5.845654] random: crng init done
[ 5.846376] systemd[1]: Mounting Temporary Directory (/tmp)...
[ 5.849082] random: 7 urandom warning(s) missed due to ratelimiting
Mounting Temporary Directory (/tmp)...
[ 5.886266] systemd[1]: Starting Create list of static device nodes for the current kernel...
Starting Create list of st…odes for the current kernel...
[ 5.916058] systemd[1]: Starting Load Kernel Module configfs...
Starting Load Kernel Module configfs...
[ 5.943400] systemd[1]: Starting Load Kernel Module drm...
Starting Load Kernel Module drm...
[ 5.971323] systemd[1]: Starting Load Kernel Module fuse...
Starting Load Kernel Module fuse...
[ 5.984781] fuse: init (API version 7.32)
[ 6.001072] systemd[1]: Starting RPC Bind...
Starting RPC Bind...
[ 6.018280] systemd[1]: Condition check resulted in File System Check on Root Device being skipped.
[ 6.028160] systemd[1]: systemd-journald.service: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling.
[ 6.041129] systemd[1]: (This warning is only shown for the first unit using IP firewalling.)
[ 6.055996] systemd[1]: Starting Journal Service...
Starting Journal Service...
[ 6.075793] systemd[1]: Condition check resulted in Load Kernel Modules being skipped.
[ 6.088643] systemd[1]: Starting Remount Root and Kernel File Systems...
Starting Remount Root and Kernel File Systems...
[ 6.109278] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
[ 6.126996] systemd[1]: Starting Apply Kernel Variables...
Starting Apply Kernel Variables...
[ 6.150931] systemd[1]: Starting Coldplug All udev Devices...
Starting Coldplug All udev Devices...
[ 6.178973] systemd[1]: Starting Setup Virtual Console...
Starting Setup Virtual Console...
[ 6.205085] systemd[1]: Started RPC Bind.
[ OK ] Started RPC Bind.
[ 6.226543] systemd[1]: Started Journal Service.
[ OK ] Started Journal Service.
[ OK ] Mounted Huge Pages File System.
[ OK ] Mounted POSIX Message Queue File System.
[ OK ] Mounted Kernel Debug File System.
[ OK ] Mounted Temporary Directory (/tmp).
[ OK ] Finished Create list of st… nodes for the current kernel.
[ OK ] Finished Load Kernel Module configfs.
[ OK ] Finished Load Kernel Module drm.
[ OK ] Finished Load Kernel Module fuse.
[ OK ] Finished Remount Root and Kernel File Systems.
[ OK ] Finished Apply Kernel Variables.
[ OK ] Finished Setup Virtual Console.
Mounting FUSE Control File System...
Mounting Kernel Configuration File System...
Starting Flush Journal to Persistent Storage...
[ 6.522398] systemd-journald[290]: Received client request to flush runtime journal.
Starting Create System Users...
[ OK ] Mounted FUSE Control File System.
[ OK ] Mounted Kernel Configuration File System.
[ OK ] Finished Flush Journal to Persistent Storage.
[ OK ] Finished Create System Users.
Starting Create Static Device Nodes in /dev...
[ OK ] Finished Create Static Device Nodes in /dev.
[ OK ] Reached target Local File Systems (Pre).
Mounting /var/volatile...
Starting Rule-based Manage…for Device Events and Files...
[ OK ] Mounted /var/volatile.
Starting Load/Save Random Seed...
[ OK ] Reached target Local File Systems.
Starting Rebuild Dynamic Linker Cache...
Starting Create Volatile Files and Directories...
[ OK ] Started Rule-based Manager for Device Events and Files.
[ OK ] Finished Load/Save Random Seed.
[ OK ] Finished Create Volatile Files and Directories.
Starting Rebuild Journal Catalog...
Starting Network Time Synchronization...
Starting Update UTMP about System Boot/Shutdown...
[ OK ] Finished Rebuild Journal Catalog.
[ OK ] Finished Update UTMP about System Boot/Shutdown.
[ OK ] Started Network Time Synchronization.
[ OK ] Reached target System Time Set.
[ OK ] Reached target System Time Synchronized.
[ 7.170012] caam 31400000.crypto: device ID = 0x0a16040000000100 (Era 9)
[ 7.181672] caam 31400000.crypto: job rings = 2, qi = 0
[ 7.222809] [VPU Encoder] enable mu for core[0]
[ OK ] Finished Coldplug All udev Devices.
[ 7.235058] [VPU Encoder] vpu encoder core[0] firmware version is 1.3.1
Starting Start Psplash Boot Screen...
[ 7.261855] imx8_media_dev: module is from the staging directory, the quality is unknown, you have been warned.
[ 7.274527] mx8-img-md: Registered mxc_isi.0.capture as /dev/video1
[ OK ] Started Start Psplash Boot Screen 7.282453] mx8-img-md: Registered mxc_isi.1.capture as /dev/video2
m.
[ 7.299471] mx8-img-md: Registered mxc_isi.2.capture as /dev/video3
[ 7.313229] mx8-img-md: Registered mxc_isi.3.capture as /dev/video4
[ 7.320893] mx8-img-md: Registered mxc_isi.4.capture as /dev/video5
[ 7.329964] mx8-img-md: Registered mxc_isi.5.capture as /dev/video6
[ 7.336594] CAN device driver interface
[ 7.341049] mx8-img-md: Registered mxc_isi.6.capture as /dev/video7
[ 7.348130] mx8-img-md: Registered mxc_isi.7.capture as /dev/video8
[ 7.362155] unregister ISI channel: mxc_isi.0
[ OK ] Started Start psplash-syst…progres[ 7.367626] unregister ISI channel: mxc_isi.1
s communication helper.
[ 7.385204] unregister ISI channel: mxc_isi.2
[ 7.439200] unregister ISI channel: mxc_isi.3
[ 7.504233] unregister ISI channel: mxc_isi.4
[ OK ] Created slice system-systemd\x2dbacklight.slice.
[ OK ] Reached target Hardware activated USB gadget.
Starting Start Psplash Boot Screen...
[ 7.570397] unregister ISI channel: mxc_isi.5
Starting Load/Save Screen … backlight:lvds_backlight@0...
Starting Load/Save Screen … backlight:lvds_backlight@1...
[ 7.603188] unregister ISI channel: mxc_isi.6
[ OK ] Finished Rebuild Dynamic Linker Cach[ 7.616730] unregister ISI channel: mxc_isi.7
e.
[ OK ] Started Start Psplash Boot Screen.
[ OK ] Finished Load/Save Screen …of backlight:lvds_backlight@0.
[ 7.676063] mxc-jpeg 58400000.jpegdec: decoder device registered as /dev/video1 (81,3)
[ OK ] Finished Load/Save Screen …of backlight:lvds_backlight@1.
[ 7.699569] mxc-jpeg 58450000.jpegenc: encoder device registered as /dev/video2 (81,4)
[ 7.796108] caam algorithms registered in /proc/crypto
[ 7.809068] caam 31400000.crypto: caam pkc algorithms registered in /proc/crypto
[ 7.817167] caam 31400000.crypto: registering rng-caam
[ 7.823544] Device caam-keygen registered
Starting Start Psplash Boot Screen...
Starting Update is Completed...
[ OK ] Started Start Psplash Boot Screen.
[ OK ] Finished Update is Completed.
[ OK ] Reached target System Initialization.
[ OK ] Started Daily rotation of log files.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target Timers.
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[ OK ] Listening on D-Bus System Message Bus Socket.
Starting Docker Socket for the API.
[ OK ] Listening on dropbear.socket.
Starting Weston socket.
Starting Console System Startup Logging...
[ OK ] Started Start psplash-syst…progress communication helper.
[ OK ] Listening on Docker Socket for the API.
[ OK ] Listening on Weston socket.
[ OK ] Finished Console System Startup Logging.
[ OK ] Reached target Sockets.
[ OK ] Reached target Basic System.
Starting Save/Restore Sound Card State...
[ OK ] Started Job spooling tools.
[ OK ] Started Periodic Command Scheduler.
[ OK ] Started D-Bus System Message Bus.
[ OK ] Started Linux Firmware Loader Daemon.
[ OK ] Started Configuration for i.MX GPU (Former rc_gpu.S).
Starting IPv6 Packet Filtering Framework...
Starting IPv4 Packet Filtering Framework...
Starting Network Time Service (one-shot ntpdate mode)...
Starting Telephony service...
[ OK ] Started Updates psplash to basic.
[ OK ] Started System Logging Service.
Starting User Login Management...
[ OK ] Started TEE Supplicant.
[ OK ] Finished Save/Restore Sound Card State.
[ OK ] Finished IPv6 Packet Filtering Framework.
[ OK ] Finished IPv4 Packet Filtering Framework.
[ OK ] Finished Network Time Service (one-shot ntpdate mode).
[ OK ] Started User Login Management.
[ OK ] Started Telephony service.
[ OK ] Created slice system-systemd\x2dfsck.slice.
[ OK ] Reached target Network (Pre).
[ OK ] Reached target Sound Card.
Starting Connection service...
Starting File System Check on /dev/mmcblk0p1...
Starting Network Service...
[ OK ] Finished File System Check on /dev/mmcblk0p1.
[ OK ] Started Connection service.
[ OK ] Started Network Service.
Mounting /run/media/mmcblk0p1...
Starting Avahi mDNS/DNS-SD Stack...
Starting Hostname Service...
Starting WPA supplicant...
[ OK ] Mounted /run/media/mmcblk0p1.
[ OK ] Started Avahi mDNS/DNS-SD Stack.
[ OK ] Started WPA supplicant.
[ OK ] Started Hostname Service.
[ OK ] Reached target Network.
Starting containerd container runtime...
[ OK ] Started NFS status monitor for NFSv2/3 locking..
[ OK ] Started Respond to IPv6 Node Information Queries.
[ OK ] Started Update psplash to network.
Starting Terminate Psplash Boot Screen...
Starting /etc/rc.local Compatibility...
[ OK ] Started Network Router Discovery Daemon.
Starting Permit User Sessions...
[FAILED] Failed to start Terminate Psplash Boot Screen.
See 'systemctl status psplash-quit.service' for details.
[ OK ] Started /etc/rc.local Compatibility.
[ OK ] Finished Permit User Sessions.
[ OK ] Started Getty on tty1.
[ OK ] Started Serial Getty on ttyLP0.
[ OK ] Reached target Login Prompts.
Starting Weston, a Wayland…ositor, as a system service...
Starting User Database Manager...
[ OK ] Started User Database Manager.
[ OK ] Created slice User Slice of UID 0.
Starting User Runtime Directory /run/user/0...
[ OK ] Finished User Runtime Directory /run/user/0.
Starting User Manager for UID 0...
[ 9.801522] audit: type=1006 audit(1616581523.292:2): pid=698 uid=0 old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=1 res=1
[ OK ] Started containerd container runtime.
[ OK ] Reached target Multi-User System.
[ OK ] Started User Manager for UID 0.
[ OK ] Started Session c1 of user root.
[ 10.261588] audit: type=1006 audit(1616581523.752:3): pid=687 uid=0 old-auid=4294967295 auid=0 tty=tty7 old-ses=4294967295 ses=2 res=1
[FAILED] Failed to start Weston, a …mpositor, as a system service.
See 'systemctl status weston.service' for details.
[ OK ] Reached target Graphical Interface.
Starting Update UTMP about System Runlevel Changes...
[ OK ] Finished Update UTMP about System Runlevel Changes.
NXP i.MX Release Distro 5.10-hardknott imx8qmmek ttyLP0