i.MX8QM USB boot Fail

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8QM USB boot Fail

272 Views
st_hw
Contributor I

你好,

 

我用i.MX8QM制作了一个板子,默认boot模式为eMMC0 boot,可手动切换为USB Serial Download模式。

我出现的问题是:

在默认boot模式下,板子上电正常。外部稳压源给板子的供电电压为5V,实际输出电流为0.65A。在手动切换到USB Serial Download模式后,稳压源电压输出保持不变,但输出电流降低到0.44A。经测PMIC1和PMIC2的SW regulator输出电压,发现异常。比如:SW7应该输出3.3V,实测为3.0V。SW6应该输出1.1V,实测为0.8V。将boot模式切换为默认模式后,稳压源输出电流又恢复至0.65A,PMIC的输出电压又恢复正常。

因为切换到USB Serial Download模式后,PMIC输出电压异常,导致上位机无法识别i.MX8这个USB设备。

感谢你的关注,期待你的解答与帮助,谢谢!

0 Kudos
Reply
1 Reply

236 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

Could you please share the power, boot mode switches and USB sections? To discard any issue on hardware side.

Best regards.

0 Kudos
Reply