Hi,
I tried to toggle an LED from imx8QM MEK SCU FW (board.c function board_init()) using SCU_LED on SC_GPIO_02.
Can someone suggest what's the issue here ?
In board_init(), I call a test function (DEBUG_Toggle_GPIO) from the BOOT_PHASE_FINAL_INIT case. The DEBUG function gets called but no LED toggles :
void DEBUG_Toggle_GPIO(uint32_t secs)
{
pad_force_mux(SC_P_SCU_GPIO0_02, 0,SC_PAD_CONFIG_NORMAL, SC_PAD_ISO_OFF);
rgpio_pin_config_t config;
config.pinDirection = kRGPIO_DigitalOutput;
/* SCU_LED on SC_GPIO_02 */
config.outputLogic = 1U;
for (uint32_t i = 0; i<secs; i++)
{
FGPIO_PinInit(FGPIOA, 2U, &config);
SYSTICK_CycleDelay(SC_SYSTICK_NSEC_TO_TICKS(30U) + 1U);
if (i%2 == 0)
{
FGPIO_PinWrite(FGPIOA, 1U, 1U);
}
else
{
FGPIO_PinWrite(FGPIOA, 1U, 0U);
}
SystemTimeDelay(1000000U);
}
}
Thanks
已解决! 转到解答。
So, I found my typo in FGPIO_PinInit()....I needed to correct the Pin (1U):
FGPIO_PinInit(FGPIOA, 2U 1U, &config);
Now, I can see the LED toggle properly in my test, that's great.
Please ignore this question.
So, I found my typo in FGPIO_PinInit()....I needed to correct the Pin (1U):
FGPIO_PinInit(FGPIOA, 2U 1U, &config);
Now, I can see the LED toggle properly in my test, that's great.
Please ignore this question.