i.MX8QM ESD diode max current

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8QM ESD diode max current

1,754 Views
oferausterlitz
Senior Contributor II

Hi,

For the i.MX8QM, what is the max allowed current of the internal ESD protection diode

for a GPIO Type 1.8V IO single supply ball?

Thanks in advance.

0 Kudos
Reply
4 Replies

1,677 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ofer

unfortunately such parameter was not characterized and not described in datasheet.

One can consider 1 mA as safe as described in AN4731 Understanding Injection Current 

sect.3.2 Externally limiting injection current

https://www.nxp.com/docs/en/application-note/AN4731.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,677 Views
oferausterlitz
Senior Contributor II

Hi Igor,

Have you received any additional information regarding the above?

Thanks in advance.

0 Kudos
Reply

1,677 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ofer

 

>Have you received any additional information regarding the above?

not, sorry. This data is not characterized and not provided in datasheet.

Also there is no such data for other i.MX processors.

If you wish that such info was added to datasheet, suggest to apply to

local marketing office and provide solid reason for such additions.

Best regards
igor

0 Kudos
Reply

1,677 Views
oferausterlitz
Senior Contributor II

Hi,

Thank you for the reference.

Since it is not listed in the datasheet, Is it possible to have the ESD diode specs from the team familiar in specific with the i.MX8QM internals?

Thank you for your support!

0 Kudos
Reply