i.MX8MQ NVMe SSD device not detected

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8MQ NVMe SSD device not detected

1,664 Views
kinjalGediya
Contributor III

Hi NXP Team,

We are trying to connect the NVMe SSD device (WD SN720) on PCIe2 of the i.MX8MQ processor custom board on L5.4.3_1.0.0 version. Please find attached schematics of the same.

# lspci
0000:00:00.0 PCI bridge: Synopsys, Inc. DWC_usb3 (rev 01)
0000:01:00.0 Non-Volatile memory controller: Sandisk Corp WD Black 2018/PC SN720 NVMe SSD

# dmesg | grep pcie
[ 1.619930] imx6q-pcie 33c00000.pcie: 33c00000.pcie supply epdev_on not found, using dummy regulator
[ 1.629439] imx6q-pcie 33c00000.pcie: host bridge /soc@0/pcie@33c00000 ranges:
[ 1.636726] imx6q-pcie 33c00000.pcie: No bus range found for /soc@0/pcie@33c00000, using [bus 00-ff]
[ 1.646068] imx6q-pcie 33c00000.pcie: IO 0x27f80000..0x27f8ffff -> 0x00000000
[ 1.657523] imx6q-pcie 33c00000.pcie: MEM 0x20000000..0x27efffff -> 0x20000000
[ 1.873843] imx6q-pcie 33c00000.pcie: Link up
[ 1.901730] imx6q-pcie 33800000.pcie: 33800000.pcie supply epdev_on not found, using dummy regulator
[ 1.911086] imx6q-pcie 33800000.pcie: host bridge /soc@0/pcie@33800000 ranges:
[ 1.927280] imx6q-pcie 33800000.pcie: IO 0x1ff80000..0x1ff8ffff -> 0x00000000
[ 1.937649] imx6q-pcie 33800000.pcie: MEM 0x18000000..0x1fefffff -> 0x18000000
[ 1.973849] imx6q-pcie 33c00000.pcie: Link up
[ 1.978222] imx6q-pcie 33c00000.pcie: Link up, Gen2
[ 1.983196] imx6q-pcie 33c00000.pcie: PCI host bridge to bus 0000:00
[ 2.139805] pcieport 0000:00:00.0: PME: Signaling with IRQ 218
[ 2.145821] pcieport 0000:00:00.0: AER: enabled with IRQ 218
[ 2.157823] imx6q-pcie 33800000.pcie: Link up
[ 2.166136] imx6q-pcie 33800000.pcie: Link up
[ 2.175555] imx6q-pcie 33800000.pcie: Link up, Gen1
[ 2.185548] imx6q-pcie 33800000.pcie: PCI host bridge to bus 0001:00
[ 2.502174] pcieport 0001:00:00.0: PME: Signaling with IRQ 221
[ 2.511696] pcieport 0001:00:00.0: AER: enabled with IRQ 221

# dmesg | grep nvme
[ 2.261612] nvme nvme0: pci function 0000:01:00.0
[ 2.319528] nvme 0000:01:00.0: enabling device (0000 -> 0002)
[ 2.695517] nvme nvme0: Removing after probe failure status: -19

 


Observation:
Linux driver is initialized successfully. But when driver probed then we have received below errors:
"nvme nvme0: Removing after probe failure status: -19".

[ 2.626903] csts: 4294967295

We have checked in the driver and observed that nvme_pci_configure_admin_queue() called nvme_enable_ctrl() at that time NVME_REG_CSTS register will received the 4294967295 value.

Ideally it should be received zero.
when nvme_pci_configure_admin_queue() called nvme_disable_ctrl() at that time NVME_REG_CSTS register will received the 0 value.

[ 2.506076] csts success: 0


=========
drivers/nvme/host/core.c
==> nvme_wait_ready() is being called by nvme_enable_ctrl() and nvme_disable_ctrl().
while ((ret = ctrl->ops->reg_read32(ctrl, NVME_REG_CSTS, &csts)) == 0) {
if (csts == ~0) {
printk("csts: %u\n", csts);
printk("%s: %s: %d\n", __FILE__, __func__, __LINE__);
return -ENODEV;
}
printk("csts success: %u\n", csts);
========

 

0 Kudos
Reply
2 Replies

1,650 Views
igorpadykov
NXP Employee
NXP Employee

Hi kinjalGediya

 

seems this is WD SN720 specific driver issue and may be posted on wd community:

https://community.wd.com/t/linux-detect-my-sn750-as-sn720-and-the-read-speed-can-not-reach-its-claim...

 

Best regards
igor

0 Kudos
Reply

1,636 Views
kinjalGediya
Contributor III

Hi igor,

Thank you for quick reply,

I have checked that link shared by you.
But in our scenario we are not getting the /dev/nvme* node.

Let me know if you need any information.

0 Kudos
Reply