I have a serious problem with HAB on i.MX8MQ, I signed the u-boot and the kernel by following the NXP documentation, so it seems to me that u-boot is well signed, but I have a weird behavior when I try to authenticate the kernel.
The event doesn’t appear when I call hab_auth_img, but if I call hab_status two times, I have one event with wrong header and without sens.
my laodaddr is 0x40480000, the size of the kernel 0x1a06960
I load the Image, here is the prompt from u-boot :
u-boot=> run loadimage 27289952 bytes read in 643 ms (40.5 MiB/s) hab fuse not enabled Authenticate image from DDR location 0x40480000… Secure boot disabled HAB Configuration: 0x00, HAB State: 0x00 Secure boot disabled HAB Configuration: 0x00, HAB State: 0x00 Secure boot disabled HAB Configuration: 0x00, HAB State: 0x00 ——— HAB Event 1 —————– STS = HAB_SUCCESS (0xF0) u-boot=> |
For me an hab event should start by a Tag: 0xdb = Event, but here it starts with 0x00, secondly it shows a HAB_SUCCESS (0xF0).
I think that U-boot verification is well done because it is verified by ROM code and SPL, that means they are in EL3.
Nevertheless, U-BOOT is EL2, therefore it calls SMC to make a call for the ROM code through ARM Trusted firmware (BL31).
We think that the problem could come from the interface between u-boot and ATF.
For information, fuses are already programmed.
My question are :
已解决! 转到解答。
Thank you @utkarsh_gupta , for your answer but imx8 was not in FAB state. It was a problem of communication between ATF and U-boot proper. The SPL was showing me correct informations but not U-boot(After adding a patch to SPL so the SPL shows the HAB state).
To correct this problem, I simply added OP-TEE, I think it's more a problem of BSP of the board, than a problem related to HAB.
Thank you
Thank you @utkarsh_gupta , for your answer but imx8 was not in FAB state. It was a problem of communication between ATF and U-boot proper. The SPL was showing me correct informations but not U-boot(After adding a patch to SPL so the SPL shows the HAB state).
To correct this problem, I simply added OP-TEE, I think it's more a problem of BSP of the board, than a problem related to HAB.
Thank you