Hi
According to the i.MX8M datasheet section 13.6.9 MIPI DSI HOST DPI INTFC horizontal timing parameters are measured in bytes.
Looking in the linux driver nwl-dsi.c it seems as if the parameters are given in pixels, as all other places in the DRM subsystem.
Anyone out there who can clarify this?
Thanks in advance
Steen
One pixel is 3 bytes, so if you ned 20 pixels for Hsync and write 20 into the
MIPI_DSI_HOST_DPI_INTFC_DSI_HOST_CFG_DPI_HSA register then you only get a Hsync pulse of 20/3 pixels, as far as I can see.
Or am I totally wrong?