i.MX8MP Linux 5.10.35_2.0.0 BSP Patch

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX8MP Linux 5.10.35_2.0.0 BSP Patch

3,195 次查看
Rebecca_Arm
Contributor II

Arm is working with several partners that are looking to achieve SystemReady certification on i.MX8M+ based platforms.  The i.MX8M+ has a different uboot configuration that is not addressed in the June 2021 release of the BSP (Linux 5.10.35_2.0.0).  We have a tight deadline to enable these partners and need to offer a workaround ahead of the Q3 release of the BSP.  Would it be possible to provide an interim binary of the BSP to address this gap?

Thanks,

Rebecca_Arm

标签 (1)
0 项奖励
13 回复数

2,470 次查看
kunyichen
Contributor IV

@yeliWould you give me some comments for generation capsule1.bin? we want verify capsule update function for SR-IR?

0 项奖励

2,461 次查看
yeli
NXP Employee
NXP Employee

You can refer BSP release doc:  iMX Linux Users Guide. 

Chapter 4.8 Arm SystemReady-IR

0 项奖励

2,455 次查看
kunyichen
Contributor IV

@yeli  iMX Linux User Guide. don't have any generation capsule1.bin method

it just have testing method.

 

you can check

kunyichen_0-1632987875159.pngkunyichen_1-1632987895028.png

 

标记 (1)
0 项奖励

2,421 次查看
yeli
NXP Employee
NXP Employee

Using below command in u-boot to generate the capsule image

./tools/mkeficapsule --raw flash.bin --index 1 capsule1.bin

 

2,419 次查看
kunyichen
Contributor IV

@yeli,

         thank you for your reply, let's me to try!

0 项奖励

2,411 次查看
kunyichen
Contributor IV

verify capsule update for i.MX8MP passed

the below instructions for update bootloader on /dev/mmcblk2boot0

------------------------------------------------------------------------------------------------------------

u-boot=> env set dfu_alt_info "mmc 2=1 raw  0 0x2000 mmcpart 1"
u-boot=> efidebug boot add 0 Boot0000 mmc 2:1 capsule1.bin
u-boot=> efidebug boot next 0
u-boot=> setenv -e -nv -bs -rt -v OsIndications =0x04
u-boot=> efidebug capsule disk-update
u-boot=> reset
 

 

0 项奖励

3,085 次查看
Rebecca_Arm
Contributor II

Jason & Yeli,

Thank you, we really appreciate it!  Do you have a summary of changes that we can provide to our partners?  I noticed there were around 9 patches for the i.MX8MP, a few for the MQ and for the MN, and a few for what looks like general patches for i.MX8M.  Do you have any guidance on how to apply these patches to the existing Q2 release of the BSP?  Are the patches for the MQ and MN required for SystemReady certification, or different updates?

Thanks, Rebecca

0 项奖励

3,077 次查看
yeli
NXP Employee
NXP Employee

We have detail description in each patch commit.

LFU-188 is used to resolve a grub memory allocation problem on 8MP/8MN. The change is common for all iMX8M.

LFU-193 is changed to use kernel DTS for USB node, so that distro kernel usb can work

LF-3892 and LF-4182 are necessary DTS change for distro kernel and enable u-boot configs for SR-IR on 8MQ/MN/MP

LFU-198 fixed a capsulate update issue on 8MQ.

They only need to apply the patch from 1-15 one by one to Q2 release.  This series includes the support for 8MQ/MN system ready certification

3,038 次查看
Rebecca_Arm
Contributor II

Thank you Ye!  A few more questions:

- Is it "safe" to apply all the patches to the Q2 BSP irrespective of it's relevancy your device (eg. applying an MQ patch when using an MN)?

- Is the LFU-188 patch a recommended or critical patch for the i.MX8M family?  Would this patch or any other patches also apply to i.MX8MM devices?

-Rebecca

0 项奖励

3,031 次查看
yeli
NXP Employee
NXP Employee

It is safe to apply all patch to Q2 release irrespective of the devices.

If you want to install distro OS on 8MP/8MN, LFU-188 is mandatory. Otherwise it is optional. It will also apply to 8MM.  

3,157 次查看
JasonLiu
NXP Employee
NXP Employee

Dear Rebecca 

The request well received. The patches will be posted by this week. The patches will be integrated into NXP i.MX Linux BSP 2021 Q3 release. 

3,117 次查看
yeli
NXP Employee
NXP Employee

Attached the u-boot patches for iMX8MQ/MN/MP SR-IR test based on 5.10.35_2.0.0 release.

2,772 次查看
yeli
NXP Employee
NXP Employee

@Rebecca_Arm  We have more 3 patches added to facilitate the distro install. Please apply them with following previous patches.

LF-4276 is used to support USB host in kernel on 8MQ EVK.

LF-4200 is for ethernet support in kernel on 8MQ and 8MM EVK.

0 项奖励