Arm is working with several partners that are looking to achieve SystemReady certification on i.MX8M+ based platforms. The i.MX8M+ has a different uboot configuration that is not addressed in the June 2021 release of the BSP (Linux 5.10.35_2.0.0). We have a tight deadline to enable these partners and need to offer a workaround ahead of the Q3 release of the BSP. Would it be possible to provide an interim binary of the BSP to address this gap?
Thanks,
Rebecca_Arm
verify capsule update for i.MX8MP passed
the below instructions for update bootloader on /dev/mmcblk2boot0
------------------------------------------------------------------------------------------------------------
Jason & Yeli,
Thank you, we really appreciate it! Do you have a summary of changes that we can provide to our partners? I noticed there were around 9 patches for the i.MX8MP, a few for the MQ and for the MN, and a few for what looks like general patches for i.MX8M. Do you have any guidance on how to apply these patches to the existing Q2 release of the BSP? Are the patches for the MQ and MN required for SystemReady certification, or different updates?
Thanks, Rebecca
We have detail description in each patch commit.
LFU-188 is used to resolve a grub memory allocation problem on 8MP/8MN. The change is common for all iMX8M.
LFU-193 is changed to use kernel DTS for USB node, so that distro kernel usb can work
LF-3892 and LF-4182 are necessary DTS change for distro kernel and enable u-boot configs for SR-IR on 8MQ/MN/MP
LFU-198 fixed a capsulate update issue on 8MQ.
They only need to apply the patch from 1-15 one by one to Q2 release. This series includes the support for 8MQ/MN system ready certification
Thank you Ye! A few more questions:
- Is it "safe" to apply all the patches to the Q2 BSP irrespective of it's relevancy your device (eg. applying an MQ patch when using an MN)?
- Is the LFU-188 patch a recommended or critical patch for the i.MX8M family? Would this patch or any other patches also apply to i.MX8MM devices?
-Rebecca
@Rebecca_Arm We have more 3 patches added to facilitate the distro install. Please apply them with following previous patches.
LF-4276 is used to support USB host in kernel on 8MQ EVK.
LF-4200 is for ethernet support in kernel on 8MQ and 8MM EVK.