I checked internally and you are right -
there is no boot Nand flash via FlexSPI interface. Only NOR flash
Sorry.
Best regards
igor
We received the following Information from NXP via Email:
"I looked over available for me internal materials regarding the serial NAND and as I see - i.MX8Mn does not support serial NAND boot and there is no mentions about plans to provide it in the nearest future."
We already noticed that Serial NAND is mentioned in some parts of the IMX8Mn Reference Manual. It looks like the Table 6-11 "FlexSPI Configuration block" is copied from a device that supports NAND-Serial-Boot.
For example, the RT1050 supports Serial NAND boot and has the same definition of "FlexSPI Configuration block" (Table 9-14 in RT1050RM).
In addition, the RT1050RM defines detailed Information like:
- 9.6.2.2 FlexSPI NAND Flash Boot Flow and Boot Control Blocks (BCB)
- 9.6.2.3 Firmware Configuration Block
- 9.6.2.4 Discovered Bad Blocks Table (DBBT)
Why is this information missing in the IMX8Mn RM? Or does the IMX8Mn support only a special kind of Serial NAND devices?
Hi T
yes boot serial NAND Flash via FlexSPI is supported as described in
Table 6-11. FlexSPI Configuration block
i.MX 8M Nano Applications Processor Reference Manual
Bad blocks are not managed by the boot ROM, they should be managed by nand
in the same way as in emmc.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------