i.MX8M plus - MIPI CSI 2 supports packets with virtual channel ID

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8M plus - MIPI CSI 2 supports packets with virtual channel ID

ソリューションへジャンプ
1,287件の閲覧回数
shai_b
Senior Contributor II

Dear Team,

My customer is planning to use two MT9M114 (from On-Semi) CMOS sensors and combine the two MIPI-CSI2 ports into one port (using Lattice FPGA device).

My question is, does i.MX8M Plus MIPI-csi2 interface knows to handle virtual channel ID and separate back the MIPI signal into two channels?
Waiting for your kind response, Thanks in advance

BR,
Shai

ラベル(1)
0 件の賞賛
返信
1 解決策
1,282件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Shai

 

unfortunately i.MX8M Plus MIPI-CSI hardware does not support virtual channels, sorry.

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
812件の閲覧回数
M-tech
Contributor I

Dear Team,
Which of your processors does accept virtual channel for mipi-csi2 interface?
Thanks

0 件の賞賛
返信
1,283件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Shai

 

unfortunately i.MX8M Plus MIPI-CSI hardware does not support virtual channels, sorry.

 

Best regards
igor

0 件の賞賛
返信
1,274件の閲覧回数
shai_b
Senior Contributor II

@igorpadykov ,

Thank you for your feedback.

KR,

Shai

0 件の賞賛
返信