Hello,
We are working with two different hardware boards with the i.Mx8M Nano processor. We have successfully enabled secure boot on both boards using the following command:
$ fuse prog 1 3 0x02000000
Both boards successfully booted up with signed images.
Issue: While we were able to flash the new signed firmware onto Board 1 via USB using the UUU command, we were not able to do so on Board 2
Query: We used the same UUU tool to flash both boards. Could there be any hardware pin configurations (e.g., GPIO HIGH/LOW) that need to be adjusted to enable USB flashing via the UUU tool on Board 2?
Seems the boot mode is not in USB download mode. Please check the boot mode of the board 2.