i.MX8M Mini EVK: Changing PMIC Settings in SPL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8M Mini EVK: Changing PMIC Settings in SPL

1,252 Views
david_ochs1
Contributor III

Hi,

I need to change the settings of an NXP PMIC (PF8121) for a board that's based on the i.MX8M Mini EVK. I see a note on the EVK schematic that mentions a couple of voltage settings for the Rohm PMIC on the EVK are changed in SPL. Is anyone able to give me some guidance on how to do the same thing for the PF8121?

One path I've started down is to try and replicate what's being done on the EVK as close as possible. So far I have found that the power_bd71837_init function from pmic_bd71837.c is being called in SPL, but I can't see yet what else is being done to change the voltages. Does the device tree entry in the u-boot fsl-imx8mm-evk.dts make the changes occur in SPL? If so, how is that controlled - is there a menuconfig option that I haven't found yet?

I hope some of these questions make sense; clearly I don't have much experience with u-boot and SPL. Thanks in advance for your help.

Dave

Labels (1)
0 Kudos
3 Replies

994 Views
igorpadykov
NXP Employee
NXP Employee

Hi David

PF8121 is used on boundary devices Nitrogen8M Mini board

https://boundarydevices.com/official-release-of-the-nitrogen8m_mini-featuring-i-mx8m-mini/ 

all pmic settings can be done in spl.c, no need to adjust them in other places

u-boot-imx6/spl.c at boundary-v2018.07 · boundarydevices/u-boot-imx6 · GitHub 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

994 Views
david_ochs1
Contributor III

Thanks very much, igorpadykov, I see the SPL code now.

One more thing if you don't mind: How are the various regulators on the EVK controlled while the kernel is running? There must be drivers controlling their voltage setpoints, but the only one that I see show up in the fsl-imx8mm-evk.dts file is buck2:

&A53_0 {
   arm-supply = <&buck2_reg>;
};

For example, I can see that buck8 is being set to 1.1V while the kernel is running:

root@imx8mmevk:~# cat /sys/class/regulator/regulator.10/name
buck8

root@imx8mmevk:~# cat /sys/class/regulator/regulator.10/microvolts
1100000

But I can't see where it's being commanded to that value.

Thanks, as always!

Best,

Dave

0 Kudos

994 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dave

for regulators usage one can look at sect.2.5 Power Management

Linux Manual included in Linux L4.14.98_2.0.0 Documentation

Best regards
igor

0 Kudos