i.MX8M MINI on Chromium

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8M MINI on Chromium

331件の閲覧回数
rizwanm
Contributor II

Hi Team,

Unable to play .mp4 video offline in i.MX8M MINI Custom board in Linux 5.4.70 version 

(Chromium 83.0.4103.116 stable)

iMX8M Mini, using Zeus 5.4.47

Is it possible to play media formats AAC, MP3, and H.264 ? in i.MX8M MINI Processor & what are all the features covers in  Chromium 83.0.4103.116 stable version

Thanks 

 

ラベル(1)
0 件の賞賛
1 返信

323件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

chromium issue where it tries to use the native picker dialog. which is being discussed in the community.

https://bugs.chromium.org/p/chromium/issues/detail?id=963419
https://bugreports.qt.io/browse/QTBUG-92519

The current workaround is to add gtk to the yocto image will help. Also there is fix in the above thread, which you can point to customer to adopt.

 

 

0 件の賞賛