Hi,
I am working on i.MX8 M MINI platform. I need some explanation on i.MX M Soft reset process ? How to invoke csu_reset_b ?
Secondly, I want to use PMIC_ON_REQ to reset my PMIC. How to invoke it ?
Thanks and regards,
Sameer
已解决! 转到解答。
Hi
Yes, you can control pmic .Please see the screensot, linux supply api to control pmic regulator.
BR
Zhiming
Hi
1.The reset command will stop watchdog to trigger soc hardware reboot and pmic will not be closed.You can see 2.11 Watchdog (WDOG) in Reference Manual.
2. The PMIC PF regulator driver in Reference Manual is based on regulator core driver. It provides the following services for regulator control of the PMIC component:
• Switch ON/OFF all voltage regulators.
• Set the value for all voltage regulators.
• Get the current value for all voltage regulators.
BR
Zhiming
Hi Zhiming,
Thanks for your reply.
1. We have not used the PMIC Watchdog pin as used in EVK for processor reboot. Is there any other option to trigger processor reboot ?
2. Can we use PMIC_ON _REQ signal to turn ON and OFF the PMIC and help processor reboot ?
BR,
Sameer
Hello Zhiming,
I have one more question. As stated earlier, we have not used PMIC WDI for processor reboot in case of Kernel panic and such issues. Is there any solution to address such issue like use of internal watchdog for reboot ?
Thanks and BR,
Sameer