Hello,
Is it possible to use 2.5V for NVCC_ENET1?
I think there is a discrepancy between the datasheet (imx7dcec rev. 2) and the reference manual (imx7drm rev. 0.1).
The datasheet states only 1.8V and 3.3V as nominal supply voltages for NVCC_ENET1, while the reference manual states 1.8V, 2.5V and 3.3V (NVCC_ENET1 is outside of the state retention domain).
What is correct?
For my design it would make things much easier to use 2.5V.
Thanks and regards,
Reno
已解决! 转到解答。
Hi Reno
you are right 2.5V also can be used.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Reno
you are right 2.5V also can be used.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------