i.MX6ULL menuconfig fail

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6ULL menuconfig fail

5,778件の閲覧回数
stevenyu
Contributor III

Hi Support,

We try to run menuconfig as below, but it fail because of "No valid terminal found, unable to open devshell".

We have seen temp/log.do_menuconfig log file, and it looks like many kinds of terminals have been checked but still fail as below. Do you have any idea how to fix this problem ? 

Thanks a lot !

Regards,

Steven Yu

~/fsl-release-bsp-minimal/build-x11$ bitbake -c menuconfig linux-imx
WARNING: Host distribution "Ubuntu-16.04" has not been validated with this version of the build system; you may possibly experience unexpected failures. It is recommended that you use a tested distribution.
Loading cache: 100% |###########################################################################################################################################| ETA: 00:00:00
Loaded 2792 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION = "1.30.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "Ubuntu-16.04"
TARGET_SYS = "arm-poky-linux-gnueabi"
MACHINE = "imx6ull14x14evk"
DISTRO = "fsl-imx-x11"
DISTRO_VERSION = "4.1.15-2.0.1"
TUNE_FEATURES = "arm armv7ve vfp neon callconvention-hard cortexa7"
TARGET_FPU = "hard"
meta
meta-poky = "HEAD:f5da2a5913319ad6ac2141438ba1aa17576326ab"
meta-oe
meta-multimedia = "HEAD:247b1267bbe95719cd4877d2d3cfbaf2a2f4865a"
meta-fsl-arm = "HEAD:be78894e4682f111575470fb23e51e6ba523508d"
meta-fsl-arm-extra = "HEAD:3dfb82fc7e703eae9891b3ffda0e9393701f2396"
meta-fsl-demos = "HEAD:a165068f8a0d1cf29aabe4b4053f28be1c2aa492"
meta-bsp
meta-sdk = "HEAD:90399d99af8a2660ebe50b49752e95b210239fd9"
meta-browser = "HEAD:77736988073a5d90fcff9d0005c8477332ede387"
meta-gnome
meta-networking
meta-python
meta-filesystems = "HEAD:247b1267bbe95719cd4877d2d3cfbaf2a2f4865a"
meta-qt5 = "HEAD:ccae79be69c5268df3b47e4e14cea0591c39a531"

NOTE: Preparing RunQueue
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
ERROR: linux-imx-4.1.15-r0 do_menuconfig: No valid terminal found, unable to open devshell
ERROR: linux-imx-4.1.15-r0 do_menuconfig: Function failed: do_menuconfig
ERROR: Logfile of failure stored in: /home/stephen/fsl-release-bsp-minimal/build-x11/tmp/work/imx6ull14x14evk-poky-linux-gnueabi/linux-imx/4.1.15-r0/temp/log.do_menuconfig.23036
ERROR: Task 5 (/home/stephen/fsl-release-bsp-minimal/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-kernel/linux/linux-imx_4.1.15.bb, do_menuconfig) failed with exit code '1'
NOTE: Tasks Summary: Attempted 253 tasks of which 252 didn't need to be rerun and 1 failed.

Summary: 1 task failed:
/home/stephen/fsl-release-bsp-minimal/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-kernel/linux/linux-imx_4.1.15.bb, do_menuconfig
Summary: There was 1 WARNING message shown.
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.


~/fsl-release-bsp-minimal/build-x11$ cat /home/stephen/fsl-release-bsp-minimal/build-x11/tmp/work/imx6ull14x14evk-poky-linux-gnueabi/linux-imx/4.1.15-r0/temp/log.do_menuconfig.23036
DEBUG: Executing python function do_menuconfig
DEBUG: Attempting to spawn terminal "custom"
DEBUG: No custom terminal (OE_TERMINAL_CUSTOMCMD) set
DEBUG: Attempting to spawn terminal "tmux-running"
DEBUG: Attempting to spawn terminal "tmux-new-window"
DEBUG: Attempting to spawn terminal "gnome"
DEBUG: Gnome-Terminal 3.10 or later does not support --disable-factory
DEBUG: Attempting to spawn terminal "konsole"
DEBUG: Attempting to spawn terminal "mate"
DEBUG: Attempting to spawn terminal "xfce"
DEBUG: Attempting to spawn terminal "terminology"
DEBUG: Attempting to spawn terminal "rxvt"
DEBUG: Attempting to spawn terminal "xterm"
DEBUG: Attempting to spawn terminal "tmux"
DEBUG: Attempting to spawn terminal "screen"
ERROR: No valid terminal found, unable to open devshell
DEBUG: Python function do_menuconfig finished
ERROR: Function failed: do_menuconfig
~/fsl-release-bsp-minimal/build-x11$

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

3,107件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  the following - hope - helps.

https://community.nxp.com/thread/443991 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,107件の閲覧回数
stevenyu
Contributor III

Hi Yuri,

We have checked the information you provided, but it is a bad news.

1. we have checked if our system has ncurses library, and we found it has libncurses5-dev installed. 

2. the xterm option has also been verified, but error logs show as below. The error looks like { Unsupported terminal "xterm", defaulting to "auto" }

~/fsl-release-bsp-minimal/build-x11$ bitbake linux-imx -c menuconfig
WARNING: Host distribution "Ubuntu-16.04" has not been validated with this version of the build system; you may possibly experience unexpected failures. It is recommended that you use a tested distribution.
Loading cache: 100% |################################################################################################################################| ETA: 00:00:00
Loaded 2792 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION = "1.30.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "Ubuntu-16.04"
TARGET_SYS = "arm-poky-linux-gnueabi"
MACHINE = "imx6ull14x14evk"
DISTRO = "fsl-imx-x11"
DISTRO_VERSION = "4.1.15-2.0.1"
TUNE_FEATURES = "arm armv7ve vfp neon callconvention-hard cortexa7"
TARGET_FPU = "hard"
meta
meta-poky = "HEAD:f5da2a5913319ad6ac2141438ba1aa17576326ab"
meta-oe
meta-multimedia = "HEAD:247b1267bbe95719cd4877d2d3cfbaf2a2f4865a"
meta-fsl-arm = "HEAD:be78894e4682f111575470fb23e51e6ba523508d"
meta-fsl-arm-extra = "HEAD:3dfb82fc7e703eae9891b3ffda0e9393701f2396"
meta-fsl-demos = "HEAD:a165068f8a0d1cf29aabe4b4053f28be1c2aa492"
meta-bsp
meta-sdk = "HEAD:90399d99af8a2660ebe50b49752e95b210239fd9"
meta-browser = "HEAD:77736988073a5d90fcff9d0005c8477332ede387"
meta-gnome
meta-networking
meta-python
meta-filesystems = "HEAD:247b1267bbe95719cd4877d2d3cfbaf2a2f4865a"
meta-qt5 = "HEAD:ccae79be69c5268df3b47e4e14cea0591c39a531"

NOTE: Preparing RunQueue
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
WARNING: linux-imx-4.1.15-r0 do_menuconfig: Unsupported terminal "xterm", defaulting to "auto"
ERROR: linux-imx-4.1.15-r0 do_menuconfig: No valid terminal found, unable to open devshell
ERROR: linux-imx-4.1.15-r0 do_menuconfig: Function failed: do_menuconfig
ERROR: Logfile of failure stored in: /home/stephen/fsl-release-bsp-minimal/build-x11/tmp/work/imx6ull14x14evk-poky-linux-gnueabi/linux-imx/4.1.15-r0/temp/log.do_menuconfig.26804
ERROR: Task 5 (/home/stephen/fsl-release-bsp-minimal/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-kernel/linux/linux-imx_4.1.15.bb, do_menuconfig) failed with exit code '1'
NOTE: Tasks Summary: Attempted 253 tasks of which 252 didn't need to be rerun and 1 failed.

Summary: 1 task failed:
/home/stephen/fsl-release-bsp-minimal/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-kernel/linux/linux-imx_4.1.15.bb, do_menuconfig
Summary: There were 2 WARNING messages shown.
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.

~/fsl-release-bsp-minimal/build-x11$ cat /home/stephen/fsl-release-bsp-minimal/build-x11/tmp/work/imx6ull14x14evk-poky-linux-gnueabi/linux-imx/4.1.15-r0/temp/log.do_menuconfig.26804
DEBUG: Executing python function do_menuconfig
DEBUG: Attempting to spawn terminal "xterm"
WARNING: Unsupported terminal "xterm", defaulting to "auto"
DEBUG: Attempting to spawn terminal "custom"
DEBUG: No custom terminal (OE_TERMINAL_CUSTOMCMD) set
DEBUG: Attempting to spawn terminal "tmux-running"
DEBUG: Attempting to spawn terminal "tmux-new-window"
DEBUG: Attempting to spawn terminal "gnome"
DEBUG: Gnome-Terminal 3.10 or later does not support --disable-factory
DEBUG: Attempting to spawn terminal "konsole"
DEBUG: Attempting to spawn terminal "mate"
DEBUG: Attempting to spawn terminal "xfce"
DEBUG: Attempting to spawn terminal "terminology"
DEBUG: Attempting to spawn terminal "rxvt"
DEBUG: Attempting to spawn terminal "xterm"
DEBUG: Attempting to spawn terminal "tmux"
DEBUG: Attempting to spawn terminal "screen"
ERROR: No valid terminal found, unable to open devshell
DEBUG: Python function do_menuconfig finished
ERROR: Function failed: do_menuconfig

3. we also try to add dbus-launch before gnome-terminal, and the error messages are silimar.

~/fsl-release-bsp-minimal/build-x11$ cat /home/stephen/fsl-release-bsp-minimal/build-x11/tmp/work/imx6ull14x14evk-poky-linux-gnueabi/linux-imx/4.1.15-r0/temp/log.do_menuconfig.11434 
DEBUG: Executing python function do_menuconfig
DEBUG: Attempting to spawn terminal "gnome"
DEBUG: Gnome-Terminal 3.10 or later does not support --disable-factory
WARNING: Unsupported terminal "gnome", defaulting to "auto"
DEBUG: Attempting to spawn terminal "custom"
DEBUG: No custom terminal (OE_TERMINAL_CUSTOMCMD) set
DEBUG: Attempting to spawn terminal "tmux-running"
DEBUG: Attempting to spawn terminal "tmux-new-window"
DEBUG: Attempting to spawn terminal "gnome"
DEBUG: Gnome-Terminal 3.10 or later does not support --disable-factory
DEBUG: Attempting to spawn terminal "konsole"
DEBUG: Attempting to spawn terminal "mate"
DEBUG: Attempting to spawn terminal "xfce"
DEBUG: Attempting to spawn terminal "terminology"
DEBUG: Attempting to spawn terminal "rxvt"
DEBUG: Attempting to spawn terminal "xterm"
DEBUG: Attempting to spawn terminal "tmux"
DEBUG: Attempting to spawn terminal "screen"
ERROR: No valid terminal found, unable to open devshell
DEBUG: Python function do_menuconfig finished
ERROR: Function failed: do_menuconfig

0 件の賞賛
返信

937件の閲覧回数
javadR3
Contributor III

Maybe too late, but following steps solved my problem.

  1. install xterm if it is not installed
  2. export DISPLAY=":0"​; bitbake linux-imx -c menuconfig

 

 

0 件の賞賛
返信