i.MX6ULL Serial downloader

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6ULL Serial downloader

796 Views
ban45
Contributor III

Hi,

I want to change BOOTMODE to a serial downloader.

Do I need to change the logic of the BOOT MODE pin?

If BOOTMODE [1: 0] = 2b10 and the internal memory is empty, do you boot from USB or UART?

Pull up and pull down BOOT_CFG1[0]~BOOT_CFG4[7],

I have set it, but isn't it necessary for the serial downloader?

 

Does the USB download mode listed in the data sheet below include a UART?

i.MX 6ULL Applications Processor Reference Manual, Rev. 1, 11/2017 P331

8.12 SD/MMC manufacture mode 

Figure 8-27. SD/MMC manufacture boot flow

 

best regard

0 Kudos
Reply
1 Reply

787 Views
igorpadykov
NXP Employee
NXP Employee

Hi ban45

 

for boot resistors selection one can look at Table 6. Boot mode input recommendations

Hardware Development Guide for the i.MX 6ULL Applications Processor

 

>Does the USB download mode listed in the data sheet below include a UART?

 

yes as described in Figure 8-2. Serial Downloader boot flow

i.MX 6ULL Applications Processors for Consumer Products

 

Best regards
igor

0 Kudos
Reply