i.MX6ULL MII + TJA1101 reference design

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6ULL MII + TJA1101 reference design

Jump to solution
1,167 Views
m_c
Senior Contributor I

Does NXP has i.MX6ULL MII+TJA1101 reference design?

Labels (1)
0 Kudos
Reply
1 Solution
1,096 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello m.c,

There is not a reference design with this specific configuration. In part because the TJA1101 is Automotive Qualified and there are no i.MX6ULL automotive variants.

There is an Automotive Ethernet PHY RMII Daughter Card based on the TJA1101 which may be of help as reference (link below for more details, please note access to the schematics is moderated)

https://www.nxp.com/docs/en/user-guide/ADTJA1101-RMIIUG.pdf

My apologies for the inconvenience.

Regards,

View solution in original post

0 Kudos
Reply
2 Replies
1,097 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello m.c,

There is not a reference design with this specific configuration. In part because the TJA1101 is Automotive Qualified and there are no i.MX6ULL automotive variants.

There is an Automotive Ethernet PHY RMII Daughter Card based on the TJA1101 which may be of help as reference (link below for more details, please note access to the schematics is moderated)

https://www.nxp.com/docs/en/user-guide/ADTJA1101-RMIIUG.pdf

My apologies for the inconvenience.

Regards,

0 Kudos
Reply
852 Views
lionelrocher
Contributor I

I try to make the same things. do you have an example of dts with imx6ul

thanks

0 Kudos
Reply