i.MX6ULL MCLK options for SAI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6ULL MCLK options for SAI

Jump to solution
739 Views
makoto
Contributor I

Hi,

Please refer to the reference manual of i.MX6ULL(https://www.nxp.com/docs/en/reference-manual/IMX6ULLRM.pdf). In the page 3126, there's a description about MCLK Select as follows.

-----------------------------------------------

NOTE: Depending on the device, some Master Clock options might not be available. See the chip specific
information for the meaning of each option.
00 Master Clock (MCLK) 1 option selected.
01 Master Clock (MCLK) 1 option selected.
10 Master Clock (MCLK) 2 option selected.
11 Master Clock (MCLK) 3 option selected.

-----------------------------------------------

Would someone please explain the meaning of each option (1,2,3)?, or please let me know where the chip specific information is?

Thank you very much in advance.

Best regards,

makoto

Labels (2)
0 Kudos
1 Solution
604 Views
igorpadykov
NXP Employee
NXP Employee

Hi Makoto

options are the same as for i.MX6UL :

iMx6UL MSEL select  

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
605 Views
igorpadykov
NXP Employee
NXP Employee

Hi Makoto

options are the same as for i.MX6UL :

iMx6UL MSEL select  

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
604 Views
makoto
Contributor I

Hi Igor,

I got it. Thank you very much for your quick and clear answer!

Best regards,

makoto

0 Kudos