i.MX6ULL LCD Connections

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6ULL LCD Connections

837 Views
daneduplooy
Contributor III

Hi! I am brand new to application processors and am busy designing our first board. I have a few questions regarding the LCD interface please:

1. What is the mapping for the LCD_DATA00 - LCD_DATA23 signals to R0-R7 / G0-G7 / B0-B7?

2. Does "LCD_ENABLE" correlate to "DE" on the TFT?

3. Does "LCD_RESET" correlate to "DISP" on the TFT?

This would be for connecting a display like 4DLCD-43480272

https://4dsystems.com.au/catalog/product/view/id/955/s/4dlcd-43480272-ips/

https://4dsystems.com.au/mwdownloads/download/link/id/824/

Thanks!

Labels (2)
0 Kudos
Reply
1 Reply

778 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

For the RGB connection please see this:

6ULL LCD RGB.PNG

For the LCD_ENABLE and LCD_RESET please see our reference design.

The default supported LCD is the LCD8000-43T, it is the validated module, which has a 4.3 inch resistive touch screen and supports a resolution of up to 480x3(RGB)x272.

Hope this can do help for you

 

0 Kudos
Reply