i.MX6ULL ENET pause frame

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6ULL ENET pause frame

ソリューションへジャンプ
720件の閲覧回数
m_c
Senior Contributor I

In the chapter 22.6.1.1 of i.MX6ULL reference manual, it mentioned pause value. Is pause value in pause frame format? If not, where is the pause value comes from?

pastedImage_1.png

ラベル(1)
0 件の賞賛
返信
1 解決策
618件の閲覧回数
radhikasomaiya
Senior Contributor II

Hi m.c,

Yes, the pause value is in pause frame format. The pause value is decided by the value of a 16-bit pause quanta, which is defined in the frame payload bytes 2 (P1) and 3 (P2) as defined in the Table 22-6 Pause Frame Format (Values in Hex). Refer section 22.6.6 Full-duplex flow control operation from reference manual for detail.

Regards,

Radhika Somaiya.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
619件の閲覧回数
radhikasomaiya
Senior Contributor II

Hi m.c,

Yes, the pause value is in pause frame format. The pause value is decided by the value of a 16-bit pause quanta, which is defined in the frame payload bytes 2 (P1) and 3 (P2) as defined in the Table 22-6 Pause Frame Format (Values in Hex). Refer section 22.6.6 Full-duplex flow control operation from reference manual for detail.

Regards,

Radhika Somaiya.

0 件の賞賛
返信