i.MX6ULL ENET pause frame

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6ULL ENET pause frame

跳至解决方案
639 次查看
m_c
Senior Contributor I

In the chapter 22.6.1.1 of i.MX6ULL reference manual, it mentioned pause value. Is pause value in pause frame format? If not, where is the pause value comes from?

pastedImage_1.png

标签 (1)
0 项奖励
回复
1 解答
537 次查看
radhikasomaiya
Senior Contributor II

Hi m.c,

Yes, the pause value is in pause frame format. The pause value is decided by the value of a 16-bit pause quanta, which is defined in the frame payload bytes 2 (P1) and 3 (P2) as defined in the Table 22-6 Pause Frame Format (Values in Hex). Refer section 22.6.6 Full-duplex flow control operation from reference manual for detail.

Regards,

Radhika Somaiya.

在原帖中查看解决方案

0 项奖励
回复
1 回复
538 次查看
radhikasomaiya
Senior Contributor II

Hi m.c,

Yes, the pause value is in pause frame format. The pause value is decided by the value of a 16-bit pause quanta, which is defined in the frame payload bytes 2 (P1) and 3 (P2) as defined in the Table 22-6 Pause Frame Format (Values in Hex). Refer section 22.6.6 Full-duplex flow control operation from reference manual for detail.

Regards,

Radhika Somaiya.

0 项奖励
回复