i.MX6ULL EIM IO voltage level

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6ULL EIM IO voltage level

399 Views
aleksandervaiga
Contributor I

Hello, 

In our ongoing project we are inteding to interface I.MX6ULL with Lattice FPGA via EIM interface. The first question is can we use a 2.5V for EIM IO voltage reference instead of 3.3V like in evaluation boards that we have found (ex. i.MX6QP Saber AI, Kondor AX)? The second question is about powering EIM module. For its powering NVCC_NAND, NVCC_LCD, NVCC_CSI should be connected to the same power rail? Where can I find a detailed DC and AC characterctics for EIM in i.MX6ULL? Reference Manual does not contain DC values for EIM.  

Best regards,

Aleksandr Vaigachev  

Labels (1)
0 Kudos
1 Reply

315 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Aleksander Vaigachev,

The NVCC voltages and DC/AC characteristics are listed in the i.MX6ULL Datasheet (link below)

http://www.nxp.com/assets/documents/data/en/data-sheets/IMX6ULLCEC.pdf

I hope you find the desired information there!

Regards,

0 Kudos