i.MX6ULL CSI support for BT.656 Interlaced video

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6ULL CSI support for BT.656 Interlaced video

397件の閲覧回数
Kavita_r
Contributor I

We need i.MX6ULL CSI support for BT.656 Interlaced video. Linux version used is 4.1.15.
We have tried the patches supplied in this link : https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/How-to-enable-i-MX6UL-CSI-port-support-B...
But the video is not properly obtained. System hang is observed on using this.
Can you direct us to a working example or patch for this issue?

0 件の賞賛
返信
1 返信

390件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Kavita_r,

Unfortunately this patch is the only we have and is for 3.14 kernel your L4.1.15 must have this code included; Some suggestion that you may get are:

CSI CM TEST MODE is working as below:

1,only ungated mode.

2,data width should be configured to 8

3,data format should be configured to rgb888

 

It cannot be other format such as bt656. It uses CSI1_TST_CTRL register to configure {R,G,B} 24 bit value and taking it as RGB888/YUV444 format for further process.  The generated image size is due to the configured width & height in the registers.

 

Regards

 

0 件の賞賛
返信