i.MX6UL Ethernet and UART muxing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6UL Ethernet and UART muxing

645 Views
surendrajadhav
Contributor IV

Hello,

I am using Ethernet 2 in RMII mode. Here ball No. G14(ENET2_TX_ER), I am using as a RMII error signal.

I am also using UART3, where the same pin(G14) is used as UART3_CTS. Since I am using G14 as ENET2_TX_ER, can I use UART3 port without CTS.

The i.MX processor tool(eclipse) is not giving error to use G14 pin as a ENET2_TX_ER.

I understand that if I am using UART3 signals like Tx, Rx and RTS, then I can not allow CTS to use for other purpose than UART. Please clarify my this understanding.

Best regards,

Surendra.

Labels (1)
0 Kudos
Reply
5 Replies

542 Views
surendrajadhav
Contributor IV

Dear Igor,

Thanks a lot for your reply.

As you said I can use UART3 port without CTS, but let me know if I can use G14(ENET2_TX_ER) as Transimt error in Ethernet.

Regards,

Surendra

0 Kudos
Reply

542 Views
igorpadykov
NXP Employee
NXP Employee

Hi Surendra

 

yes, one can configure it as gpio and use as "Transimt error".

 

Best regards
igor

0 Kudos
Reply

542 Views
surendrajadhav
Contributor IV

Hello Igor,

Thanks again for your reply.

Here I want to clarify that I am not using the pin as a GPIO, but it belongs to Ethernet interface only.

Please see the attached file.

Regards,

SurendraEthernet-UART mux.png

0 Kudos
Reply

542 Views
igorpadykov
NXP Employee
NXP Employee

Hi Surendra

please use IOMUX Chapter and verify that this pin could be used as gpio (it is more accurate)

i.MX6UL Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6ULRM.pdf

Best regards
igor

0 Kudos
Reply

542 Views
igorpadykov
NXP Employee
NXP Employee

Hi Surendra

you are right one can use UART3 port without CTS, using it for other purpose.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply