i.MX6UL Battery Backup

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6UL Battery Backup

486 次查看
danielfield
Contributor I

I'm doing a design with the i.MX6UL processor with a coin cell backup for RTC and am needing to draw as little current as possible when there is no system power. 

Using the eval board for this processor, I'm seeing the current draw at 300 uA when powered from VDD_COIN_3V.  I'm assuming this large current draw is coming from various leakage currents on the design:

 - POR_B leakage current on the reset circuitry

 - PMIC_ON_REQ leakage current 

I'm assuming if I use MOSFET's to help isolate these lines during a coin cell only power I can get my coin cell current draw significantly lower?  Are there other areas of leakage current I should be concerned about?

标签 (1)
0 项奖励
1 回复

390 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Daniel

leakage may be caused by some pads which are powered by VSNVS,

this is  described in Table 10. Power and decoupling recommendations

Hardware Development Guide for the i.MX 6UltraLite Applications Processor
http://www.nxp.com/docs/en/user-guide/IMX6ULHDG.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励