i.MX6S h.264 encoding

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6S h.264 encoding

1,839 次查看
dmitryovsyannik
Contributor I

Dear i.MX experts!

Does i.MX6S supports h.264 1080p encoding? Freescale documentation so controversal...

标签 (4)
标记 (2)
0 项奖励
回复
2 回复数

599 次查看
ZeeFrench
NXP Employee
NXP Employee

Hello Dmitry,

Guess the confusion is coming from the fact VPU (video encoder and decoder bloc) is an option, according to http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6S&tab=Buy_Parametric_Tab&fromSea... not available on S1 and S4, please check automotive datasheet for complete list of option : http://www.freescale.com/files/32bit/doc/data_sheet/IMX6SDLAEC.pdf?fpsp=1&WT_TYPE=Data Sheets&WT_VENDOR=FREESCALE&WT_FILE_FORMAT=pdf&WT_ASSET=Documentation (or consumer and industrial but VPU is on all of those).

You could encode in software (make sure you use neon) but for that resolution at a very low frame rate, better use the VPU enabled part numbers.

Best regards, Philippe.

599 次查看
dmitryovsyannik
Contributor I

Thanks, Philippe!

Now everything is clear. Yes, I need hardware acceleration, so I will use part with VPU.

0 项奖励
回复