i.MX6QP-SABRE-SD with Dual Outputs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6QP-SABRE-SD with Dual Outputs

Jump to solution
949 Views
jacoblim
Contributor II

I'm trying to decide on the display hardware to purchase for the i.MX6QP-SABRE SD.

I have read that the board is compatible with the following: MCIMX-LVDS1, MCIMX28LCD and possibly MCIMXHDMICARD.

I am currently using the on-board HDMI as my primary output.

Has anyone tried HDMI + either LVDS, LCD, HDMICARD successfully on the i.MX6QP-SABRE-SD (I believe i.MX6Q-SABRE-SD should be similar)?

My ultimate goal would be to output 2 independent displays with the GPU.

EDIT: By the way, I am using Yocto.

Any help is appreciated.

Thanks  

0 Kudos
1 Solution
752 Views
jacoblim
Contributor II

Thanks Rita,

Have decided to purchase the LVDS panel for evaluation.

Jacob

View solution in original post

0 Kudos
5 Replies
752 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

The thread is created by my couleague https://community.nxp.com/docs/DOC-332671 on i.MX6Q, you can take it as an reference.

0 Kudos
752 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

Which version BSP are you using? Our android BSP on i.MX6QP-SABRE SD support dual display.
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
752 Views
jacoblim
Contributor II

Hi Rita,

I'm using Linux 4.1.15_2.0.1 Patch.

I understand from the Linux Release Notes that LVDS + HDMI is supported.

Just wondering what other configurations are possible and if anyone had tried them before purchasing the hardware.

Thanks

Jacob

0 Kudos
752 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Other display is OK, if it is not the default display support, you need to porting the screen diver to your board.

0 Kudos
753 Views
jacoblim
Contributor II

Thanks Rita,

Have decided to purchase the LVDS panel for evaluation.

Jacob

0 Kudos