Hi, All
We designed a customer board based on imx6q SabreAI board, and use SD3 as eMMC boot.
Now, it can download firmware with MFG Tool, however, it cannot boot up, because the board is always in download mode ( MFGTool always display " HID-compliance device".)
Maybe there are some mistakes when partitionion or MBR in the 1st 1kb of eMMC, but i'm not sure.
Could some one give some suggestion to help me to go forward.
below is the log of download using mfg tool.
=============================
U-Boot 2009.08-svn30 (May 24 2014 - 12:29:00)
CPU: Freescale i.MX6 family TO1.2 at 792 MHz
Thermal sensor with ratio = 183
Temperature: 31 C, calibration data 0x5874d47d
mx6q pll1: 792MHz
mx6q pll2: 528MHz
mx6q pll3: 480MHz
mx6q pll8: 50MHz
ipg clock : 66000000Hz
ipg per clock : 66000000Hz
uart clock : 80000000Hz
cspi clock : 60000000Hz
ahb clock : 132000000Hz
axi clock : 264000000Hz
emi_slow clock: 132000000Hz
ddr clock : 528000000Hz
usdhc1 clock : 198000000Hz
usdhc2 clock : 198000000Hz
usdhc3 clock : 198000000Hz
usdhc4 clock : 198000000Hz
nfc clock : 24000000Hz
Board: i.MX6Q-SABREAUTO: unknown-board Board: 0x63012 [POR]
Boot Device: MMC
I2C: ready
DRAM: 2 GB
MMC: mmc init ok - jason
FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2,FSL_USDHC: 3
Using default environment
In: serial
Out: serial
Err: serial
Found PFUZE100! deviceid=10,revid=11
Net: got MAC address from IIM: 00:00:00:00:00:00
FEC0 [PRIME]
Hit any key to stop autoboot: 0
## Booting kernel from Legacy Image at 10800000 ...
Image Name: Linux-3.0.35-svn27
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3183872 Bytes = 3 MB
Load Address: 10008000
Entry Point: 10008000
Verifying Checksum ... OK
## Loading init Ramdisk from Legacy Image at 10c00000 ...
Image Name: uboot initramfs rootfs
Image Type: ARM Linux RAMDisk Image (gzip compressed)
Data Size: 4545326 Bytes = 4.3 MB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Linux version 3.0.35-svn27 (xujianhua@semisky3) (gcc version 4.6.x-google 20120106 (prerelease) (GCC) ) #2 SMP PREEMPT Fri May 23 16:53:24 CST 2014
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: Freescale i.MX 6Quad/DualLite/Solo Sabre Auto Board, Semisky Inc.
Memory policy: ECC disabled, Data cache writealloc
CPU identified as i.MX6Q, silicon rev 1.2
PERCPU: Embedded 7 pages/cpu @82063000 s5184 r8192 d15296 u32768
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 520192
Kernel command line: console=ttymxc1,115200 rdinit=/linuxrc enable_wait_mode=off
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 262144 (order: 8, 1048576 bytes)
Inode-cache hash table entries: 131072 (order: 7, 524288 bytes)
Memory: 2048MB = 2048MB total
Memory: 2068248k/2068248k available, 28904k reserved, 360448K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
DMA : 0xfbe00000 - 0xffe00000 ( 64 MB)
vmalloc : 0xea800000 - 0xf2000000 ( 120 MB)
lowmem : 0x80000000 - 0xea000000 (1696 MB)
pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)
modules : 0x7f000000 - 0x7fe00000 ( 14 MB)
.init : 0x80008000 - 0x8003a000 ( 200 kB)
.text : 0x8003a000 - 0x805b66f0 (5618 kB)
.data : 0x805b8000 - 0x806064a0 ( 314 kB)
.bss : 0x806064c4 - 0x806318f0 ( 174 kB)
SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
Preemptible hierarchical RCU implementation.
NR_IRQS:624
MXC GPIO hardware
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms
arm_max_freq=1GHz
MXC_Early serial console at MMIO 0x21e8000 (options '115200')
bootconsole [ttymxc1] enabled
Console: colour dummy device 80x30
Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
CPU1: Booted secondary processor
CPU2: Booted secondary processor
CPU3: Booted secondary processor
Brought up 4 CPUs
SMP: Total of 4 processors activated (6324.22 BogoMIPS).
print_constraints: dummy:
NET: Registered protocol family 16
print_constraints: vddpu: 725 <--> 1300 mV at 700 mV fast normal
print_constraints: vddcore: 725 <--> 1300 mV at 1150 mV fast normal
print_constraints: vddsoc: 725 <--> 1300 mV at 1200 mV fast normal
print_constraints: vdd2p5: 2000 <--> 2775 mV at 2400 mV fast normal
print_constraints: vdd1p1: 800 <--> 1400 mV at 1100 mV fast normal
print_constraints: vdd3p0: 2625 <--> 3400 mV at 3000 mV fast normal
==<backlignt : 1 >n
hw-breakpoint: found 6 breakpoint and 1 watchpoint registers.
hw-breakpoint: 1 breakpoint(s) reserved for watchpoint single-step.
hw-breakpoint: maximum watchpoint size is 4 bytes.
L310 cache controller enabled
l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x32070000, Cache size: 1048576 B
bio: create slab <bio-0> at 0
mxs-dma mxs-dma-apbh: initialized
print_constraints: VA: 2800 mV
print_constraints: VD: 2800 mV
print_constraints: VLS: 2800 mV
print_constraints: VLC: 2800 mV
print_constraints: vmmc: 3300 mV
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
mc_pfuze 1-0008: ID: 0,Full lay: 1 ,Metal lay: 1
mc_pfuze 1-0008: FAB: 0 ,FIN: 0
print_constraints: SW1A: 300 <--> 1875 mV at 1375 mV
print_constraints: SW1B: 300 <--> 1875 mV at 300 mV
print_constraints: SW1C: 300 <--> 1875 mV at 1375 mV
print_constraints: SW2: 800 <--> 3950 mV at 3000 mV
print_constraints: SW3A: 400 <--> 1975 mV at 1500 mV
print_constraints: SW3B: 400 <--> 1975 mV at 1500 mV
print_constraints: SW4: 800 <--> 3950 mV at 3300 mV
print_constraints: SWBST: 5000 <--> 5150 mV at 5000 mV
print_constraints: VSNVS: 1200 <--> 3000 mV at 1800 mV
print_constraints: VREFDDR: at 750 mV
print_constraints: VGEN1: 800 <--> 1550 mV at 800 mV
print_constraints: VGEN2: 800 <--> 1550 mV at 1500 mV
print_constraints: VGEN3: 1800 <--> 3300 mV at 2800 mV
print_constraints: VGEN4: 1800 <--> 3300 mV at 1800 mV
print_constraints: VGEN5: 1800 <--> 3300 mV at 3000 mV
print_constraints: VGEN6: 1800 <--> 3300 mV at 2800 mV
imx-ipuv3 imx-ipuv3.0: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
imx-ipuv3 imx-ipuv3.1: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
Advanced Linux Sound Architecture Driver Version 1.0.24.
Bluetooth: Core ver 2.16
NET: Registered protocol family 31
Bluetooth: HCI device and connection manager initialized
Bluetooth: HCI socket layer initialized
Bluetooth: L2CAP socket layer initialized
Bluetooth: SCO socket layer initialized
i2c-core: driver [max17135] using legacy suspend method
i2c-core: driver [max17135] using legacy resume method
Switching to clocksource mxc_timer1
Clockevents: could not switch to one-shot mode:
Clockevents: could not switch to one-shot mode:
Clockevents: could not switch to one-shot mode: dummy_timer is not functional.
dummy_timer is not functional.
Could not switch to high resolution mode on CPU 2
Clockevents: could not switch to one-shot mode:
Could not switch to high resolution mode on CPU 1
dummy_timer is not functional.
Could not switch to high resolution mode on CPU 0
NET: Registered protocol family 2
IP route cache hash table entries: 65536 (order: 6, 262144 bytes)
TCP established hash table entries: 262144 (order: 9, 2097152 bytes)
TCP bind hash table entries: 65536 (order: 7, 786432 bytes)
TCP: Hash tables configured (established 262144 bind 65536)
TCP reno registered
UDP hash table entries: 1024 (order: 3, 32768 bytes)
UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Unpacking initramfs...
dummy_timer is not functional.
Could not switch to high resolution mode on CPU 3
Freeing initrd memory: 4436K
Static Power Management for Freescale i.MX6
wait mode is disabled for i.MX6
cpaddr = ea880000 suspend_iram_base=ea8e8000
PM driver module loaded
IMX usb wakeup probe
cpu regulator mode:ldo_enable
i.MXC CPU frequency driver
highmem bounce pool size: 64 pages
JFFS2 version 2.2. (NAND) 漏 2001-2006 Red Hat, Inc.
msgmni has been set to 3344
cryptodev: driver loaded.
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
mxc_sdc_fb mxc_sdc_fb.0: register mxc display driver ldb
_regulator_get: get() with no identifier
imx-ipuv3 imx-ipuv3.1: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)
Console: switching to colour frame buffer device 128x37
mxc_sdc_fb mxc_sdc_fb.1: register mxc display driver ldb
mxc_sdc_fb mxc_sdc_fb.2: register mxc display driver lcd
imx-sdma imx-sdma: loaded firmware 1.1
imx-sdma imx-sdma: initialized
Serial: IMX driver
imx-uart.1: ttymxc1 at MMIO 0x21e8000 (irq = 59) is a IMX
console [ttymxc1] enabled, bootconsole disabled
console [ttymxc1] enabled, bootconsole disabled
imx-uart.2: ttymxc2 at MMIO 0x21ec000 (irq = 60) is a IMX
imx-uart.3: ttymxc3 at MMIO 0x21f0000 (irq = 61) is a IMX
loop: module loaded
GPMI NAND driver registered. (IMX)
vcan: Virtual CAN interface driver
FEC Ethernet Driver
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
ARC USBOTG Device Controller driver (1 August 2005)
add wake up source irq 75
g_file_storage gadget: controller 'fsl-usb2-udc' not recognized
check_parameters:UTP settings are in place now, overriding defaults
g_file_storage gadget: No serial-number string provided!
g_file_storage gadget: File-backed Storage Gadget, version: 1 September 2010
g_file_storage gadget: Number of LUNs=1
fsl-usb2-udc: bind to driver g_file_storage
mousedev: PS/2 mouse device common for all mice
=======================goodix_ts_init======================
============================goodix_ts_probe==========================
input: Goodix_TouchScreen_GT80X as /devices/virtual/input/input0
================goodix_init_panel===================
================goodix_init_panel===================
Goodix-TS 1-0055: Guitar Version: GT801_1R08_2011121501_Goodix_Tech
============== Guitar Version: GT801_1R08_2011121501_Goodix_Tech ===============
g_file_storage gadget: high speed config #1
Goodix-TS 1-0055: Start Goodix_TouchScreen_GT80X in Interrupt mode
i2c-core: driver [Goodix-TS] using legacy suspend method
i2c-core: driver [Goodix-TS] using legacy resume method
using rtc device, snvs_rtc, for alarms
snvs_rtc snvs_rtc.0: rtc core: registered snvs_rtc as rtc0
i2c /dev entries driver
Linux video capture interface: v2.00
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video16
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video17
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video18
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video19
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video20
imx2-wdt imx2-wdt.0: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=1)
Bluetooth: Virtual HCI driver ver 1.3
Bluetooth: Generic Bluetooth USB driver ver 0.6
usbcore: registered new interface driver btusb
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
mmc0: SDHCI controller on platform [sdhci-esdhc-imx.2] using DMA
sdhci sdhci-esdhc-imx.3: no card-detect pin available!
mmc1: SDHCI controller on platform [sdhci-esdhc-imx.3] using DMA
sdhci sdhci-esdhc-imx.0: no write-protect pin available!
sdhci sdhci-esdhc-imx.0: no card-detect pin available!
mmc2: no vmmc regulator found
mmc2: SDHCI controller on platform [sdhci-esdhc-imx.0] using DMA
mxc_vdoa mxc_vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
VPU initialized
mxc_asrc registered
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
Cirrus Logic CS42888 ALSA SoC Codec Driver
Device with ID register fffffffb is not a CS42888
i2c-core: driver [cs42888] using legacy suspend method
i2c-core: driver [cs42888] using legacy resume method
imx_3stack asoc driver
ALSA device list:
No soundcards found.
TCP cubic registered
NET: Registered protocol family 17
can: controller area network core (rev 20090105 abi 8)
NET: Registered protocol family 29
can: raw protocol (rev 20090105)
can: broadcast manager protocol (rev 20090105 t)
Bluetooth: RFCOMM TTY layer initialized
Bluetooth: RFCOMM socket layer initialized
Bluetooth: RFCOMM ver 1.11
Bluetooth: BNEP (Ethernet Emulation) ver 1.3
Bluetooth: BNEP filters: protocol multicast
Bluetooth: HIDP (Human Interface Emulation) ver 1.2
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
Bus freq driver module loaded
Bus freq driver Enabled
mxc_dvfs_core_probe
DVFS driver module loaded
mmc0: new high speed DDR MMC card at address 0001
mmcblk0: mmc0:0001 008GE0 7.28 GiB
regulator_init_complete: VGEN6: incomplete constraints, leaving on
mmcblk0boot0: mmc0:0001 008GE0 partition 1 4.00 MiB
mmcblk0boot1: mmc0:0001 008GE0 partition 2 4.00 MiB
regulator_init_complete: VGEN5: incomplete constraints, leaving on
regulator_init_complete: VGEN4: incomplete constraints, leaving on
mmcblk0: p1 p2 p3 < p5 p6 p7 p8 > p4
regulator_init_complete: VGEN2: incomplete constraints, leaving on
regulator_init_complete: VLC: incomplete constraints, leaving on
regulator_init_complete: VLS: incomplete constraints, leaving on
regulator_init_complete: VD: incomplete constraints, leaving on
regulator_init_complete: VA: incomplete constraints, leaving on
snvs_rtc snvs_rtc.0: setting system clock to 1970-01-01 00:00:00 UTC (0)
mmcblk0: p4 size 13090816 extends beyond EOD, truncated
Freeing init memory: 200K
mmcblk0boot1: unknown partition table
Starting UTP
mmcblk0boot0: unknown partition table
ln: /etc/mtab: File exists
disable turn off display
Starting the hotplug events dispatcher udevd
udevd (2001): /proc/2001/oom_adj is deprecated, please use /proc/2001/oom_score_adj instead.
Synthesizing initial hotplug events
uuc 0.4 [built Aug 16 2013 01:24:08]
UTP: Waiting for device to appear
UTP: file/device node /dev/utp already exists
cpu_id is 0
UTP: received command '$ dd if=/dev/zero of=/dev/mmcblk0 bs=512 seek=1536 count=16'
UTP: executing "dd if=/dev/zero of=/dev/mmcblk0 bs=512 seek=1536 count=16"
16+0 records in
16+0 records out
8192 bytes (8.0KB) copied, 0.002714 seconds, 2.9MB/s
UTP: sending Success to kernel for command $ dd if=/dev/zero of=/dev/mmcblk0 bs=512 seek=1536 count=16.
utp_poll: pass returned.
UTP: received command '$ echo 0 > /sys/block/mmcblk0boot0/force_ro'
UTP: executing "echo 0 > /sys/block/mmcblk0boot0/force_ro"
UTP: sending Success to kernel for command $ echo 0 > /sys/block/mmcblk0boot0/force_ro.
utp_poll: pass returned.
UTP: received command 'send'
UTP: sending Success to kernel for command send.
UTP: received command '$ dd if=$FILE of=/dev/mmcblk0boot0 bs=512 seek=2 skip=2'
UTP: executing "dd if=$FILE of=/dev/mmcblk0boot0 bs=512 seek=2 skip=2"
910+1 records in
910+1 records out
466180 bytes (455.3KB) copied, 0.070847 seconds, 6.3MB/s
UTP: sending Success to kernel for command $ dd if=$FILE of=/dev/mmcblk0boot0 bs=512 seek=2 skip=2.
utp_poll: pass returned.
UTP: received command '$ echo 8 > /sys/devices/platform/sdhci-esdhc-imx.2/mmc_host/mmc0/mmc0:0001/boot_config'
UTP: executing "echo 8 > /sys/devices/platform/sdhci-esdhc-imx.2/mmc_host/mmc0/mmc0:0001/boot_config"
UTP: sending Success to kernel for command $ echo 8 > /sys/devices/platform/sdhci-esdhc-imx.2/mmc_host/mmc0/mmc0:0001/boot_config.
utp_poll: pass returned.
UTP: received command '$ echo 1 > /sys/block/mmcblk0boot0/force_ro'
UTP: executing "echo 1 > /sys/block/mmcblk0boot0/force_ro"
UTP: sending Success to kernel for command $ echo 1 > /sys/block/mmcblk0boot0/force_ro.
utp_poll: pass returned.
UTP: received command 'send'
UTP: sending Success to kernel for command send.
UTP: received command '$ tar xf $FILE '
UTP: executing "tar xf $FILE "
UTP: sending Success to kernel for command $ tar xf $FILE .
utp_poll: pass returned.
UTP: received command '$ sh -x mksdcard-android.sh /dev/mmcblk0'
UTP: executing "sh -x mksdcard-android.sh /dev/mmcblk0"
+ BOOTLOAD_RESERVE=8
+ BOOT_ROM_SIZE=8
+ SYSTEM_ROM_SIZE=512
+ CACHE_SIZE=512
+ RECOVERY_ROM_SIZE=8
+ VENDER_SIZE=8
+ MISC_SIZE=8
+ id -u
+ userid=0
+ [ 0 -ne 0 ]
+ moreoptions=1
+ node=na
+ cal_only=0
+ flash_images=0
+ not_partition=0
+ not_format_fs=0
+ [ 1 = 1 -a 1 -gt 0 ]
+ moreoptions=0
+ node=/dev/mmcblk0
+ [ 0 = 0 ]
+ [ 1 -gt 1 ]
+ [ 0 = 1 ]
+ [ 0 = 1 -a 1 - mmcblk0: unknown partition table
gt 0 ]
+ [ ! -e /dev/mmcblk0 ]
+ seprate=40
+ sfdisk -s /dev/mmcblk0
+ total_size=7634944
+ expr 7634944 / 1024
+ total_size=7456
+ expr 8 + 8
+ boot_rom_sizeb=16
+ expr 512 + 512 + 8 + 8 + 40
+ extend_size=1080
+ expr 7456 - 16 - 8 - 1080 + 40
+ data_size=6392
+ [ 0 -eq 1 ]
+ dd if=/dev/zero of=/dev/mmcblk0 bs=1024 count=1
1+0 records in
1+0 records out
1024 bytes (1.0KB) copied, 0.001788 seconds, 559.3KB/s
+ sfdisk --force -uM /dev/mmcblk0
Checking that no-one is using this disk right now ...
OK
Disk /dev/mmcblk0: 238592 cylinders, 4 heads, 16 sectors/track
sfdisk: ERROR: sector 0 does not have an msdos signature
/dev/mmcblk0: unrecognized partition table type
Old situation:
No partitions found
Warning: given size (6392) exceeds max allowable size (6352)
New situation:
Units = mebibytes of 1048576 bytes, blocks of 1024 bytes, counting from 0
Device Boot Start End MiB #blocks Id System
/dev/mmcblk0p1 0+ 15 16- 16383+ 83 Linux
/dev/mmcblk0p2 16 23 8 8192 83 Linux
/dev/mmcblk0p3 24 1103 1080 1105920 5 Extended
/dev/mmcblk0p4 1104 7495 6392 6545408 83 Linux
/dev/mmcblk0p5 24+ 535 512- 524287+ 83 Linux
/dev/mmcblk0p6 536+ 1047 512- 524287+ 83 Linux
/dev/mmcblk0p7 1048+ 1055 8- 8191+ 83 Linux
/dev/mmcblk0p8 1056+ 1063 8- 8191+ 83 Linux
Warning: partition 4 extends past end of disk
Successfully wrote the new partition table
Re-reading the partition table ...
mmcblk0: p1 p2 p3 < p5 p6 p7 p8 > p4
mmcblk0: p4 size 13090816 extends beyond EOD, truncated
If you created or changed a DOS partition, /dev/foo7, say, then use dd(1)
to zero the first 512 bytes: dd if=/dev/zero of=/dev/foo7 bs=512 count=1
(See fdisk(8).)
+ sfdisk --force -uM /dev/mmcblk0 -N1
Checking that no-one is using th mmcblk0: p1 p2 p3 < p5 p6 p7 p8 > p4
is disk right now ...
mmcblk0: p4 size 13090816 extends beyond EOD, truncated
OK
Disk /dev/mmcblk0: 238592 cylinders, 4 heads, 16 sectors/track
Old situation:
Units = mebibytes of 1048576 bytes, blocks of 1024 bytes, counting from 0
Device Boot Start End MiB #blocks Id System
/dev/mmcblk0p1 0+ 15 16- 16383+ 83 Linux
/dev/mmcblk0p2 16 23 8 8192 83 Linux
/dev/mmcblk0p3 24 1103 1080 1105920 5 Extended
/dev/mmcblk0p4 1104 7495 6392 6545408 83 Linux
/dev/mmcblk0p5 24+ 535 512- 524287+ 83 Linux
/dev/mmcblk0p6 536+ 1047 512- 524287+ 83 Linux
/dev/mmcblk0p7 1048+ 1055 8- 8191+ 83 Linux
/dev/mmcblk0p8 1056+ 1063 8- 8191+ 83 Linux
New situation:
Units = mebibytes of 1048576 bytes, blocks of 1024 bytes, counting from 0
Device Boot Start End MiB #blocks Id System
/dev/mmcblk0p1 8 15 8 8192 83 Linux
/dev/mmcblk0p2 16 23 8 8192 83 Linux
/dev/mmcblk0p3 24 1103 1080 1105920 5 Extended
/dev/mmcblk0p4 1104 7495 6392 6545408 83 Linux
/dev/mmcblk0p5 24+ 535 512- 524287+ 83 Linux
/dev/mmcblk0p6 536+ 1047 512- 524287+ 83 Linux
/dev/mmcblk0p7 1048+ 1055 8- 8191+ 83 Linux
/dev/mmcblk0p8 1056+ 1063 8- 8191+ 83 Linux
Warning: partition 4 extends past end of disk
Successfully wrote the new partition table
Re-reading the partition table ...
mmcblk0: p1 p2 p3 < p5 p6 p7 p8 > p4
mmcblk0: p4 size 13090816 extends beyond EOD, truncated
If you created or changed a DOS partition, /dev/foo7, say, then use dd(1)
to zero the first 512 bytes: dd if=/dev/zero of=/dev/foo7 bs=512 count=1
(See fdisk(8).)
UTP: sending Success to kernel for command $ sh -x mksdcard-android.sh /dev/mmcblk0.
utp_poll: pass returned.
UTP: received command '$ ls -l /dev/mmc* '
UTP: executing "ls -l /dev/mmc* "
brw-r----- 1 root disk 179, 0 Jan 1 00:00 /dev/mmcblk0
brw-r----- 1 root disk 179, 8 Jan 1 00:00 /dev/mmcblk0boot0
brw-r----- 1 root disk 179, 16 Jan 1 00:00 /dev/mmcblk0boot1
brw-r----- 1 root disk 179, 1 Jan 1 00:00 /dev/mmcblk0p1
brw-r----- 1 root disk 179, 2 Jan 1 00:00 /dev/mmcblk0p2
brw-r----- 1 root disk 179, 3 Jan 1 00:00 /dev/mmcblk0p3
brw-r----- 1 root disk 179, 4 Jan 1 00:00 /dev/mmcblk0p4
brw-r----- 1 root disk 179, 5 Jan 1 00:00 /dev/mmcblk0p5
brw-r----- 1 root disk 179, 6 Jan 1 00:00 /dev/mmcblk0p6
brw-r----- 1 root disk 179, 7 Jan 1 00:00 /dev/mmcblk0p7
brw-r----- 1 root disk 259, 0 Jan 1 00:00 /dev/mmcblk0p8
UTP: sending Success to kernel for command $ ls -l /dev/mmc* .
utp_poll: pass returned.
UTP: received command 'send'
UTP: sending Success to kernel for command send.
UTP: received command '$ dd if=$FILE of=/dev/mmcblk0p1'
UTP: executing "dd if=$FILE of=/dev/mmcblk0p1"
9644+0 records in
9644+0 records out
4937728 bytes (4.7MB) copied, 0.542027 seconds, 8.7MB/s
UTP: sending Success to kernel for command $ dd if=$FILE of=/dev/mmcblk0p1.
utp_poll: pass returned.
UTP: received command 'frf'
UTP: closing the file
UTP: sending Success to kernel for command frf.
utp_poll: pass returned.
UTP: received command '$ mkfs.ext4 -b 4096 -m 0 /dev/mmcblk0p4'
UTP: executing "mkfs.ext4 -b 4096 -m 0 /dev/mmcblk0p4"
mke2fs 1.41.4 (27-Jan-2009)
Filesystem label=
OS type: Linux
Block size=4096 (log=2)
Fragment size=4096 (log=2)
407200 inodes, 1626112 blocks
0 blocks (0.00%) reserved for the super user
First data block=0
Maximum filesystem blocks=1665138688
50 block groups
32768 blocks per group, 32768 fragments per group
8144 inodes per group
Superblock backups stored on blocks:
32768, 98304, 163840, 229376, 294912, 819200, 884736, 1605632
Writing inode tables: done
Creating journal (32768 blocks): done
Writing superblocks and filesystem accounting information: done
This filesystem will be automatically checked every 31 mounts or
180 days, whichever comes first. Use tune2fs -c or -i to override.
UTP: sending Success to kernel for command $ mkfs.ext4 -b 4096 -m 0 /dev/mmcblk0p4.
utp_poll: pass returned.
UTP: received command 'send'
UTP: sending Success to kernel for command send.
UTP: received command '$ tar xf $FILE '
UTP: executing "tar xf $FILE "
UTP: sending Success to kernel for command $ tar xf $FILE .
utp_poll: pass returned.
UTP: received command '$ sh -x mk-encryptable-data-android.sh /dev/mmcblk0 /dev/mmcblk0p4'
UTP: executing "sh -x mk-encryptable-data-android.sh /dev/mmcblk0 /dev/mmcblk0p4"
+ mkdir -p /tmp/data
+ mount /dev/mmcblk0p4 /tmp/data
EXT4-fs (mmcblk0p4): mounted filesystem with ordered data mode. Opts: (null)
+ df -k
+ grep /dev/mmcblk0p4
+ awk {print $2}
+ amount=6402176
+ [ -z 6402176 ]
+ stag=6402176
+ sleep 1
+ umount /dev/mmcblk0p4
+ rm -fr /tmp/data
+ stag=6402144
+ kilo=K
+ echo Get disk block size 6402176K
Get disk block size 6402176K
+ amountkilo=6402144K
+ echo Resize to 6402144K
Resize to 6402144K
+ e2fsck -f /dev/mmcblk0p4
e2fsck 1.41.4 (27-Jan-2009)
Pass 1: Checking inodes, blocks, and sizes
Pass 2: Checking directory structure
Pass 3: Checking directory connectivity
Pass 4: Checking reference counts
Pass 5: Checking group summary information
/dev/mmcblk0p4: 11/407200 files (0.0% non-contiguous), 61906/1626112 blocks
+ resize2fs /dev/mmcblk0p4 6402144K
resize2fs 1.41.4 (27-Jan-2009)
Resizing the filesystem on /dev/mmcblk0p4 to 1600536 (4k) blocks.
The filesystem on /dev/mmcblk0p4 is now 1600536 blocks long.
UTP: sending Success to kernel for command $ sh -x mk-encryptable-data-android.sh /dev/mmcblk0 /dev/mmcblk0p4.
utp_poll: pass returned.
UTP: received command '$ mkfs.ext4 /dev/mmcblk0p5'
UTP: executing "mkfs.ext4 /dev/mmcblk0p5"
mke2fs 1.41.4 (27-Jan-2009)
Filesystem label=
OS type: Linux
Block size=1024 (log=0)
Fragment size=1024 (log=0)
131072 inodes, 524284 blocks
26214 blocks (5.00%) reserved for the super user
First data block=1
Maximum filesystem blocks=67633152
64 block groups
8192 blocks per group, 8192 fragments per group
2048 inodes per group
Superblock backups stored on blocks:
8193, 24577, 40961, 57345, 73729, 204801, 221185, 401409
Writing inode tables: done
Creating journal (8192 blocks): done
Writing superblocks and filesystem accounting information: done
This filesystem will be automatically checked every 31 mounts or
180 days, whichever comes first. Use tune2fs -c or -i to override.
UTP: sending Success to kernel for command $ mkfs.ext4 /dev/mmcblk0p5.
utp_poll: pass returned.
UTP: received command '$ mkfs.ext4 /dev/mmcblk0p6'
UTP: executing "mkfs.ext4 /dev/mmcblk0p6"
mke2fs 1.41.4 (27-Jan-2009)
Filesystem label=
OS type: Linux
Block size=1024 (log=0)
Fragment size=1024 (log=0)
131072 inodes, 524284 blocks
26214 blocks (5.00%) reserved for the super user
First data block=1
Maximum filesystem blocks=67633152
64 block groups
8192 blocks per group, 8192 fragments per group
2048 inodes per group
Superblock backups stored on blocks:
8193, 24577, 40961, 57345, 73729, 204801, 221185, 401409
Writing inode tables: done
Creating journal (8192 blocks): done
Writing superblocks and filesystem accounting information: done
This filesystem will be automatically checked every 22 mounts or
180 days, whichever comes first. Use tune2fs -c or -i to override.
UTP: sending Success to kernel for command $ mkfs.ext4 /dev/mmcblk0p6.
utp_poll: pass returned.
UTP: received command 'frf'
UTP: closing the file
UTP: sending Success to kernel for command frf.
utp_poll: pass returned.
UTP: received command '$ mkfs.ext4 /dev/mmcblk0p7'
UTP: executing "mkfs.ext4 /dev/mmcblk0p7"
mke2fs 1.41.4 (27-Jan-2009)
Filesystem label=
OS type: Linux
Block size=1024 (log=0)
Fragment size=1024 (log=0)
2048 inodes, 8188 blocks
409 blocks (5.00%) reserved for the super user
First data block=1
Maximum filesystem blocks=8388608
1 block group
8192 blocks per group, 8192 fragments per group
2048 inodes per group
Writing inode tables: done
Creating journal (1024 blocks): done
Writing superblocks and filesystem accounting information: done
This filesystem will be automatically checked every 20 mounts or
180 days, whichever comes first. Use tune2fs -c or -i to override.
UTP: sending Success to kernel for command $ mkfs.ext4 /dev/mmcblk0p7.
utp_poll: pass returned.
UTP: received command 'pipe dd of=/dev/mmcblk0p5 bs=512'
pid is 3676, UTP: executing "dd of=/dev/mmcblk0p5 bs=512"
UTP: sending Success to kernel for command pipe dd of=/dev/mmcblk0p5 bs=512.
UTP: received command 'frf'
573440+0 records in
573440+0 records out
293601280 bytes (280.0MB) copied, 25.900929 seconds, 10.8MB/s
UTP: closing the file
UTP: sending Success to kernel for command frf.
utp_poll: pass returned.
UTP: received command 'pipe dd of=/dev/mmcblk0p2 bs=512'
pid is 3678, UTP: executing "dd of=/dev/mmcblk0p2 bs=512"
UTP: sending Success to kernel for command pipe dd of=/dev/mmcblk0p2 bs=512.
UTP: received command 'frf'
10720+0 records in
10720+0 records out
5488640 bytes (5.2MB) copied, 0.637624 seconds, 8.2MB/s
UTP: closing the file
UTP: sending Success to kernel for command frf.
utp_poll: pass returned.
UTP: received command '$ echo Update Complete!'
UTP: executing "echo Update Complete!"
Update Complete!
UTP: sending Success to kernel for command $ echo Update Complete!.
utp_poll: pass returned.
消息编辑者为:jianhua xu
解決済! 解決策の投稿を見る。
Thx Raymond and chipexpert, this issue is fixed now with changing initramfs.cpio.gz.uboot in MFGTool.
initramfs.cpio.gz.uboot is a binary file, i'm not sure what happen exactly, but i guess it should be releated with MBR in the 1st 1KB in eMMC.
(before i send the post, the boot config is already set correctly).
Thx a lot for both of your help. ^ ^
Thx Raymond and chipexpert, this issue is fixed now with changing initramfs.cpio.gz.uboot in MFGTool.
initramfs.cpio.gz.uboot is a binary file, i'm not sure what happen exactly, but i guess it should be releated with MBR in the 1st 1KB in eMMC.
(before i send the post, the boot config is already set correctly).
Thx a lot for both of your help. ^ ^
Dear jianhua Xu and all
I change mfgtool(try different version) and initramfs.cpio.gz.uboot, but always into download mode, have your any suggest? thanks
Hello,
the following Community thread may be useful :
https://community.nxp.com/thread/312758
Regards,
Yuri.
Hi,
We are also facing similar issue. can you please share the latest initramfs.cpio.gz.uboot file in MFG tool.
What are the changes that are done to the new initramfs.cpio.gz.uboot?
Thanks and Regards,
-Devaraj
Hi devarajgs
Actually, the root cause is not found. what i do is just to try to use two different version of tools, and found it can solve the problem. so i think it might be releated with that bin file.
Maybe you can also try this way. "Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER" and "Mfgtools-Rel-13.01.00_ER_MX6Q_UPDATER", they can be downloaded from website. if one is not ok, try another one, ..., use them interactively.
Anyway, i'm not sure it is help for you, but you can try ^^
Dear Jianhua
Can you send me the Mfgtools-Rel-13.01.00_ER_MX6Q_UPDATER soft, I can not downloard it now. My mail is: dreaminghell@163.com. Thanks!
Hi jianhua,
you should close MFG Tool, disconnect USB, power off board.
For booting from eMMC please set correct boot pins, then power-up board,
then provide log from terminal.
Best regards
chip
It seems mfg progress okay!
Did you ever check your EIM boot option config ? Even you flash eMMC device properly, wrong config may cause boot failed ,then enter download mode once again.