i.MX6Q: apb_slave and qv_value for MPCore-2 and 3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Q: apb_slave and qv_value for MPCore-2 and 3

593 Views
norishinozaki
Contributor V

Hello Champs,

In the RM, "Table 45-5. QoS and tidemark parameters"

I found entries for MPCore-0 and 1.

pastedImage_1.png

pastedImage_0.png

What is apb_slave and qv_value for MPCore-2 and 3?

Regards,

Nori Shinozaki

Labels (1)
0 Kudos
4 Replies

474 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nori

MPCore-0 does not mean arm core 0. Meaning is AXI (number 0) of

MPCore platform. That is internally 4xcores are connected to SCU,

SCU is connected to L2 cache, L2 has two AXI buses named as

"MPCore-0,1" connected to NIC GPV_0. Short RM description is below

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

474 Views
norishinozaki
Contributor V

Thanks Igor,

So when we change the priority of Cortex A9 cores, we change qv_value for both MPCore-0 and 1 at a time.

Correct?

Best regards,

Nori Shinozaki

0 Kudos

474 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nori,

this does not relate to A9 cores, it relates to L2 AXI buses (0 and 1),

for its usage one can refer to documetation of L2 cache controller

like ARM document DDI0246A PL310 and other L2 documentation.

Best regards

igor

0 Kudos

474 Views
norishinozaki
Contributor V

Igor,

Thanks, I found this diagram.

BR,

NS

pastedImage_0.png

0 Kudos