Hello ;
I ' m working on Wandboard Quad which has iMX6Q processor on it . I opened it 's UART2 features from it 's imx6q-wandboard.dts but I have some problem about it and my mind is confused if I did right or missed something while enabling the UART2 .
I can send data from the UART2_TX but even if I set up the both console and ttymxc1 (UART2) baudrates same , I recieve nonsense character 's .
And I enabled from im6q-wandboard.dts adding ;
&uart2 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_uart2_1>;
status = "okay" ;
};
Did I missing something or did I do something wrong about it ?
Thanks for your help ...