Hello,
I am developing a product that uses the i.MX6Q and I intend to make use of OpenCL to accelerate some computationally expensive algorithms.
When trying to run any OpenCL code (e.g. line 13 in opencl_test.c) galcore segfaults; see attached strace log and dmesg.txt.
Additional notes: 4.14.78 kernel
Any guidance is greatly appreciated.
-- Curtis
Hello curtis1,
Here you can see a overview of OpenCL in i.MX6
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/OpenCL-Hello-World/ta-p/1113358
Regards
Thank you for that information, but it does not address my specific issue.
My issue seems to be limited to the kernel galcore driver which segfaults on any call to libOpenCL.
Segmentation fault means problem with memory, is probable that you don´t include the galcore library correctly that the reason I send you that page.
The test program was compiled cleanly with : gcc opencl_test.c -lGAL -lOpenCL -o opencl_test
The segfault is occuring in the galcore kernel module as indicated in the dmesg log.
Are there any specific debug steps for diagnosing issues related to galcore?