Hi all,
I have a custom iMX6q derived from SABRE and I wanted to use a 7 inches 800x480 WVGA monitor attached to the LVDS channel 0.
The monitor works with an operating clock freq at 33.26 MHz, but it works well even with 38MHz (tested).
I'm using kernel 3.14.28_ga, I've modified the original SABRE DTS specifing:
mxcfb1: fb@0 {
compatible = "fsl,mxc_sdc_fb";
disp_dev = "ldb";
interface_pix_fmt = "RGB666";
mode_str ="LDB-WVGA";
default_bpp = <32>;
int_clk = <0>;
late_init = <0>;
status = "okay";
};
&ldb {
status = "okay";
primary;
lvds-channel@0 {
reg = <0>;
fsl,data-mapping = "spwg";
fsl,data-width = <18>;
status = "okay";
crtc = "ipu1-di0";
display-timings {
native-mode = <&timing1>;
timing1: 800x480 {
clock-frequency = <38000000>;
hactive = <800>;
vactive = <480>;
hback-porch = <56>;
hfront-porch = <50>;
vback-porch = <23>;
vfront-porch = <20>;
hsync-len = <150>;
vsync-len = <2>;
};
};
};
};
From dmesg output:
mxc_sdc_fb fb.18: registered mxc display driver ldb
Console: switching to colour frame buffer device 100x30
The LVDS manages to light up, but remains blank.
Testing with an oscilloscope it seems the clock output is giving 76MHz instead!
How can I set the right clock frequency?
Any ideas?
- ec
解決済! 解決策の投稿を見る。
Thanks everyone for answering,
Unfortunately, the solutions didn't work for me.
I've done some research and found a workaround (and, I think, the problem).
I found that the u-boot sets the various parent clocks before boot, but the kernel don't overwrite this setting (the specification in clk-imx6q.c doesn't apply).
Specifically, testing with devmem2 after boot :
CCM_CS2CDR (0x20C_402C) -> 0x007206C1 //MMDC_CH1 enabled on LDB_DI0_CLK_SEL)
After recompiling the uboot, setting manually the parent to PLL5_VIDEO, the issue disappear, and the kernel manages to control the PLL to the correct frequency.
I've added in the uboot platform file (board/freescale/mx6sabresd/mx6sabresd.c
/* Turn on LDB0,IPU DI0 clocks */
reg = __raw_readl(&mxc_ccm->CCGR3);
reg |= MXC_CCM_CCGR3_LDB_DI0_MASK;
writel(reg, &mxc_ccm->CCGR3);
/* set LDB0 clk select to 000 (pll5) */
reg = readl(&mxc_ccm->cs2cdr);
reg &= ~(MXC_CCM_CS2CDR_LDB_DI0_CLK_SEL_MASK);
reg |= (0 << MXC_CCM_CS2CDR_LDB_DI0_CLK_SEL_OFFSET);
writel(reg, &mxc_ccm->cs2cdr);
/* LDB clock div by 7 */
reg = readl(&mxc_ccm->cscmr2);
reg |= MXC_CCM_CSCMR2_LDB_DI0_IPU_DIV;
writel(reg, &mxc_ccm->cscmr2);
/* derive ipu1_di0_clk_root clock from ldb_di0_clk */
reg = readl(&mxc_ccm->chsccdr);
reg |= (CHSCCDR_CLK_SEL_LDB_DI0
<< MXC_CCM_CHSCCDR_IPU1_DI0_CLK_SEL_OFFSET);
writel(reg, &mxc_ccm->chsccdr);
After boot:
CCM_CS2CDR (0x20C_402C) -> 0x007200C1 //PLL5_CLK enabled on LDB_DI0_CLK_SEL
Maybe the kernel fails to write the registers in the initialization process?
Thanks again, - ec
Hi,
I believe, the parent clock is not mapped. You need to set the parent for LDB_DI0_SEL.
In IPU clock selection section, add the below changes in "~/linux-imx/arch/arm/mach-imx/clk-imx6q.c" file.
/* ipu clock initialization */ | |
imx_clk_set_parent(clk[IMX6QDL_CLK_LDB_DI0_SEL], clk[IMX6QDL_CLK_PLL5_VIDEO_DIV]); |
Regards,
Ansari
That worked for me, thanks!
Thanks everyone for answering,
Unfortunately, the solutions didn't work for me.
I've done some research and found a workaround (and, I think, the problem).
I found that the u-boot sets the various parent clocks before boot, but the kernel don't overwrite this setting (the specification in clk-imx6q.c doesn't apply).
Specifically, testing with devmem2 after boot :
CCM_CS2CDR (0x20C_402C) -> 0x007206C1 //MMDC_CH1 enabled on LDB_DI0_CLK_SEL)
After recompiling the uboot, setting manually the parent to PLL5_VIDEO, the issue disappear, and the kernel manages to control the PLL to the correct frequency.
I've added in the uboot platform file (board/freescale/mx6sabresd/mx6sabresd.c
/* Turn on LDB0,IPU DI0 clocks */
reg = __raw_readl(&mxc_ccm->CCGR3);
reg |= MXC_CCM_CCGR3_LDB_DI0_MASK;
writel(reg, &mxc_ccm->CCGR3);
/* set LDB0 clk select to 000 (pll5) */
reg = readl(&mxc_ccm->cs2cdr);
reg &= ~(MXC_CCM_CS2CDR_LDB_DI0_CLK_SEL_MASK);
reg |= (0 << MXC_CCM_CS2CDR_LDB_DI0_CLK_SEL_OFFSET);
writel(reg, &mxc_ccm->cs2cdr);
/* LDB clock div by 7 */
reg = readl(&mxc_ccm->cscmr2);
reg |= MXC_CCM_CSCMR2_LDB_DI0_IPU_DIV;
writel(reg, &mxc_ccm->cscmr2);
/* derive ipu1_di0_clk_root clock from ldb_di0_clk */
reg = readl(&mxc_ccm->chsccdr);
reg |= (CHSCCDR_CLK_SEL_LDB_DI0
<< MXC_CCM_CHSCCDR_IPU1_DI0_CLK_SEL_OFFSET);
writel(reg, &mxc_ccm->chsccdr);
After boot:
CCM_CS2CDR (0x20C_402C) -> 0x007200C1 //PLL5_CLK enabled on LDB_DI0_CLK_SEL
Maybe the kernel fails to write the registers in the initialization process?
Thanks again, - ec
Hello
When I apply the changes, the boot stops at "switch to ldo_bypass mode!":
U-Boot 2014.04 (Jul 22 2015 - 09:46:08)
CPU: Freescale i.MX6Q rev1.1 at 792 MHz
CPU: Temperature 10 C, calibration data: 0x5614cb7d
Reset cause: POR
Board: MX6-SabreSD
I2C: ready
DRAM: 1 GiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
*** Warning - bad CRC, using default environment
No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In: serial
Out: serial
Err: serial
Found PFUZE100 deviceid=10,revid=10
mmc0 is current device
Net: FEC [PRIME]
Normal Boot
Hit any key to stop autoboot: 0
mmc0 is current device
reading boot.scr
** Unable to read file boot.scr **
reading zImage
5930352 bytes read in 274 ms (20.6 MiB/s)
Booting from mmc ...
reading imx6q-sabresd.dtb
42259 bytes read in 19 ms (2.1 MiB/s)
Kernel image @ 0x12000000 [ 0x000000 - 0x5a7d70 ]
## Flattened Device Tree blob at 18000000
Booting using the fdt blob at 0x18000000
Using Device Tree in place at 18000000, end 1800d512
switch to ldo_bypass mode!
Any Idea?
Thanks.
Hi,
I think pll5 is not initialized in u-boot, this might be the reason of your freeze. There are two possible workarounds for this issue:
Regards
Hi,
Thank you for your input.
In U-boot level, we are not supporting any display(including LVDS) and we are supporting the displays (including LVDS) in kernel level only.
As per your referred community link, the LVDS clock parent settings has to be added during the "setup_display".
But in our case(in our custom board file) "setup_display" function is not there.
Please suggest us.
Regards,
Ansari
Hi, Ansari
I used this source file, and "setup_display" is present:
Isn't a valid version?
Btw, adding code in uboot actually is a workaround, I would like to set the right PLL in kernel boot process.
There is a bug in 3.14.28_ga?
Cheers, Ettore
Hi,
I have not tried that out. But you may try to change or select a different parent clock. And after looking at the code you could try to select the slipt-mode too.
You can try to add split-mode in the device node.
serial_clk = ldb->spl_mode ? chan.vm.pixelclock * 7 / 2 :
chan.vm.pixelclock * 7;
please let me know if that makes a difference.
Best Regards,
Alejandro