i.MX6Q IPU Error Interrupts.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6Q IPU Error Interrupts.

ソリューションへジャンプ
706件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6DQ reference manual (IMX6DQRM Rev.1).

Please see the explanation above Table 37-36.

It says what is happened when these errors in Table 37-36 occurred and what should user do to resolve the errors.

And in last sentence, it says "In that case the system may need to increase the clock to the IPU or simplify the use case.".

Could you let me know which clock in Table 37-8 is indicated as "clock to the IPU" in this sentence?

hsp_clk? or ipu_master_hclk?

Best Regards,

Satoshi Shimoda

ラベル(4)
タグ(2)
0 件の賞賛
1 解決策
546件の閲覧回数
Yuri
NXP Employee
NXP Employee

  In the case of IPU Error  Interrupts we have performance problem. Please try to

decrease screen resolution and / or frame rate. Also, other system resource

consuming processes, such as USB / SD / SATA transfer, may affect. As result

a general performance  issue may take place in the case. Perhaps it makes sense

to try system prioritization (such as provided by Linux nice command).

Note, the base clock for the IPU is IPUx_HSP_CLK_ROOT.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
1 返信
547件の閲覧回数
Yuri
NXP Employee
NXP Employee

  In the case of IPU Error  Interrupts we have performance problem. Please try to

decrease screen resolution and / or frame rate. Also, other system resource

consuming processes, such as USB / SD / SATA transfer, may affect. As result

a general performance  issue may take place in the case. Perhaps it makes sense

to try system prioritization (such as provided by Linux nice command).

Note, the base clock for the IPU is IPUx_HSP_CLK_ROOT.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛