i.MX6Q : IPU Capturing restrictions in size or proportions

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6Q : IPU Capturing restrictions in size or proportions

485 次查看
norishinozaki
Contributor V

Hello Champs,

I have little trouble of capturing in IPU at certain resolutions.

Let me check, is there any restrictions in resolution or proportions other than written in RM page 458.

"Frame size: up to 8192 x 4096 pixels (including blanking intervals)"

BR,

N.S.

标签 (2)
0 项奖励
回复
1 回复

430 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Nori

you are right :Frame size: up to 8192 x 4096 pixels

as described i.MX6DQ Reference Manual p.2723

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

There are no other restrictions in max. resolution

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复