i.MX6DL based Wandboard as a standalone AP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6DL based Wandboard as a standalone AP

620 Views
karthik_mohan
Contributor II

I am using a iMX6DL based Wandboard. I want to use it as a standalone AP. But the AP is not listing anywhere, so I would like to know why is that.

The kernel i am using is wandboard_imx_4.9.11_1.0.0_ga as my Kernel, and Ubuntu 16.04 as my rootfs.

I have cloned the latest version of hostapd source from git clone git://w1.fi/hostap.git.

Here is my configuration file for installing hostapd.

# Driver interface for Host AP driver
CONFIG_DRIVER_HOSTAP=y

# Driver interface for wired authenticator
#CONFIG_DRIVER_WIRED=y

# Driver interface for drivers using the nl80211 kernel interface
CONFIG_DRIVER_NL80211=y

# QCA vendor extensions to nl80211
#CONFIG_DRIVER_NL80211_QCA=y

# driver_nl80211.c requires libnl. If you are compiling it yourself
# you may need to point hostapd to your version of libnl.
#
#CFLAGS += -I$<path to libnl include files>
#LIBS += -L$<path to libnl library files>

# Use libnl v2.0 (or 3.0) libraries.
#CONFIG_LIBNL20=y

# Use libnl 3.2 libraries (if this is selected, CONFIG_LIBNL20 is ignored)
CONFIG_LIBNL32=y


# Driver interface for FreeBSD net80211 layer (e.g., Atheros driver)
#CONFIG_DRIVER_BSD=y
#CFLAGS += -I/usr/local/include
#LIBS += -L/usr/local/lib
#LIBS_p += -L/usr/local/lib
#LIBS_c += -L/usr/local/lib

# Driver interface for no driver (e.g., RADIUS server only)
#CONFIG_DRIVER_NONE=y

# WPA2/IEEE 802.11i RSN pre-authentication
CONFIG_RSN_PREAUTH=y

# Support Operating Channel Validation
#CONFIG_OCV=y

# Integrated EAP server
CONFIG_EAP=y

# EAP Re-authentication Protocol (ERP) in integrated EAP server
CONFIG_ERP=y

# EAP-MD5 for the integrated EAP server
/CONFIG_EAP_MD5=y

# EAP-TLS for the integrated EAP server
CONFIG_EAP_TLS=y

# EAP-MSCHAPv2 for the integrated EAP server
CONFIG_EAP_MSCHAPV2=y

# EAP-PEAP for the integrated EAP server
CONFIG_EAP_PEAP=y

# EAP-GTC for the integrated EAP server
CONFIG_EAP_GTC=y

# EAP-TTLS for the integrated EAP server
CONFIG_EAP_TTLS=y

# EAP-SIM for the integrated EAP server
#CONFIG_EAP_SIM=y

# EAP-AKA for the integrated EAP server
#CONFIG_EAP_AKA=y

# EAP-AKA' for the integrated EAP server
# This requires CONFIG_EAP_AKA to be enabled, too.
#CONFIG_EAP_AKA_PRIME=y

# EAP-PAX for the integrated EAP server
#CONFIG_EAP_PAX=y

# EAP-PSK for the integrated EAP server (this is _not_ needed for WPA-PSK)
#CONFIG_EAP_PSK=y

# EAP-pwd for the integrated EAP server (secure authentication with a password)
#CONFIG_EAP_PWD=y

# EAP-SAKE for the integrated EAP server
#CONFIG_EAP_SAKE=y

# EAP-GPSK for the integrated EAP server
#CONFIG_EAP_GPSK=y
# Include support for optional SHA256 cipher suite in EAP-GPSK
#CONFIG_EAP_GPSK_SHA256=y

# EAP-FAST for the integrated EAP server
#CONFIG_EAP_FAST=y

# EAP-TEAP for the integrated EAP server
# Note: The current EAP-TEAP implementation is experimental and should not be
# enabled for production use. The IETF RFC 7170 that defines EAP-TEAP has number
# of conflicting statements and missing details and the implementation has
# vendor specific workarounds for those and as such, may not interoperate with
# any other implementation. This should not be used for anything else than
# experimentation and interoperability testing until those issues has been
# resolved.
#CONFIG_EAP_TEAP=y

# Wi-Fi Protected Setup (WPS)
CONFIG_WPS=y
# Enable UPnP support for external WPS Registrars
#CONFIG_WPS_UPNP=y
# Enable WPS support with NFC config method
#CONFIG_WPS_NFC=y

# EAP-IKEv2
#CONFIG_EAP_IKEV2=y

# Trusted Network Connect (EAP-TNC)
#CONFIG_EAP_TNC=y

# EAP-EKE for the integrated EAP server
#CONFIG_EAP_EKE=y

# PKCS#12 (PFX) support (used to read private key and certificate file from
# a file that usually has extension .p12 or .pfx)
CONFIG_PKCS12=y

# RADIUS authentication server. This provides access to the integrated EAP
# server from external hosts using RADIUS.
CONFIG_RADIUS_SERVER=y

# Build IPv6 support for RADIUS operations
CONFIG_IPV6=y

# IEEE Std 802.11r-2008 (Fast BSS Transition)
CONFIG_IEEE80211R=y

# Use the hostapd's IEEE 802.11 authentication (ACL), but without
# the IEEE 802.11 Management capability (e.g., FreeBSD/net80211)
#CONFIG_DRIVER_RADIUS_ACL=y

# Wireless Network Management (IEEE Std 802.11v-2011)
# Note: This is experimental and not complete implementation.
#CONFIG_WNM=y

# IEEE 802.11ac (Very High Throughput) support
CONFIG_IEEE80211AC=y

# IEEE 802.11ax HE support
#CONFIG_IEEE80211AX=y

# IEEE 802.11be EHT support
# CONFIG_IEEE80211AX is mandatory for setting CONFIG_IEEE80211BE.
# Note: This is experimental and work in progress. The definitions are still
# subject to change and this should not be expected to interoperate with the
# final IEEE 802.11be version.
#CONFIG_IEEE80211BE=y

# Simultaneous Authentication of Equals (SAE), WPA3-Personal
#CONFIG_SAE=y

# SAE Public Key, WPA3-Personal
#CONFIG_SAE_PK=y

# Remove debugging code that is printing out debug messages to stdout.
# This can be used to reduce the size of the hostapd considerably if debugging
# code is not needed.
#CONFIG_NO_STDOUT_DEBUG=y

# Add support for writing debug log to a file: -f /tmp/hostapd.log
# Disabled by default.
CONFIG_DEBUG_FILE=y

# Send debug messages to syslog instead of stdout
#CONFIG_DEBUG_SYSLOG=y

# Add support for sending all debug messages (regardless of debug verbosity)
# to the Linux kernel tracing facility. This helps debug the entire stack by
# making it easy to record everything happening from the driver up into the
# same file, e.g., using trace-cmd.
#CONFIG_DEBUG_LINUX_TRACING=y

# Remove support for RADIUS accounting
#CONFIG_NO_ACCOUNTING=y

# Remove support for RADIUS
#CONFIG_NO_RADIUS=y

# Remove support for VLANs
#CONFIG_NO_VLAN=y

# Enable support for fully dynamic VLANs. This enables hostapd to
# automatically create bridge and VLAN interfaces if necessary.
#CONFIG_FULL_DYNAMIC_VLAN=y

# Use netlink-based kernel API for VLAN operations instead of ioctl()
# Note: This requires libnl 3.1 or newer.
#CONFIG_VLAN_NETLINK=y

# Remove support for dumping internal state through control interface commands
# This can be used to reduce binary size at the cost of disabling a debugging
# option.
#CONFIG_NO_DUMP_STATE=y

# Enable tracing code for developer debugging
# This tracks use of memory allocations and other registrations and reports
# incorrect use with a backtrace of call (or allocation) location.
#CONFIG_WPA_TRACE=y
# For BSD, comment out these.
#LIBS += -lexecinfo
#LIBS_p += -lexecinfo
#LIBS_c += -lexecinfo

# Use libbfd to get more details for developer debugging
# This enables use of libbfd to get more detailed symbols for the backtraces
# generated by CONFIG_WPA_TRACE=y.
#CONFIG_WPA_TRACE_BFD=y
# For BSD, comment out these.
#LIBS += -lbfd -liberty -lz
#LIBS_p += -lbfd -liberty -lz
#LIBS_c += -lbfd -liberty -lz

# hostapd depends on strong random number generation being available from the
# operating system. os_get_random() function is used to fetch random data when
# needed, e.g., for key generation. On Linux and BSD systems, this works by
# reading /dev/urandom. It should be noted that the OS entropy pool needs to be
# properly initialized before hostapd is started. This is important especially
# on embedded devices that do not have a hardware random number generator and
# may by default start up with minimal entropy available for random number
# generation.
#
# As a safety net, hostapd is by default trying to internally collect
# additional entropy for generating random data to mix in with the data
# fetched from the OS. This by itself is not considered to be very strong, but
# it may help in cases where the system pool is not initialized properly.
# However, it is very strongly recommended that the system pool is initialized
# with enough entropy either by using hardware assisted random number
# generator or by storing state over device reboots.
#
# hostapd can be configured to maintain its own entropy store over restarts to
# enhance random number generation. This is not perfect, but it is much more
# secure than using the same sequence of random numbers after every reboot.
# This can be enabled with -e<entropy file> command line option. The specified
# file needs to be readable and writable by hostapd.
#
# If the os_get_random() is known to provide strong random data (e.g., on
# Linux/BSD, the board in question is known to have reliable source of random
# data from /dev/urandom), the internal hostapd random pool can be disabled.
# This will save some in binary size and CPU use. However, this should only be
# considered for builds that are known to be used on devices that meet the
# requirements described above.
#CONFIG_NO_RANDOM_POOL=y

# Should we attempt to use the getrandom(2) call that provides more reliable
# yet secure randomness source than /dev/random on Linux 3.17 and newer.
# Requires glibc 2.25 to build, falls back to /dev/random if unavailable.
#CONFIG_GETRANDOM=y

# Should we use poll instead of select? Select is used by default.
#CONFIG_ELOOP_POLL=y

# Should we use epoll instead of select? Select is used by default.
#CONFIG_ELOOP_EPOLL=y

# Should we use kqueue instead of select? Select is used by default.
#CONFIG_ELOOP_KQUEUE=y

# Select TLS implementation
# openssl = OpenSSL (default)
# gnutls = GnuTLS
# internal = Internal TLSv1 implementation (experimental)
# linux = Linux kernel AF_ALG and internal TLSv1 implementation (experimental)
# none = Empty template
#CONFIG_TLS=openssl

# TLS-based EAP methods require at least TLS v1.0. Newer version of TLS (v1.1)
# can be enabled to get a stronger construction of messages when block ciphers
# are used.
#CONFIG_TLSV11=y

# TLS-based EAP methods require at least TLS v1.0. Newer version of TLS (v1.2)
# can be enabled to enable use of stronger crypto algorithms.
#CONFIG_TLSV12=y

# Select which ciphers to use by default with OpenSSL if the user does not
# specify them.
#CONFIG_TLS_DEFAULT_CIPHERS="DEFAULT:!EXP:!LOW"

# If CONFIG_TLS=internal is used, additional library and include paths are
# needed for LibTomMath. Alternatively, an integrated, minimal version of
# LibTomMath can be used. See beginning of libtommath.c for details on benefits
# and drawbacks of this option.
#CONFIG_INTERNAL_LIBTOMMATH=y
#ifndef CONFIG_INTERNAL_LIBTOMMATH
#LTM_PATH=/usr/src/libtommath-0.39
#CFLAGS += -I$(LTM_PATH)
#LIBS += -L$(LTM_PATH)
#LIBS_p += -L$(LTM_PATH)
#endif
# At the cost of about 4 kB of additional binary size, the internal LibTomMath
# can be configured to include faster routines for exptmod, sqr, and div to
# speed up DH and RSA calculation considerably
#CONFIG_INTERNAL_LIBTOMMATH_FAST=y

# Interworking (IEEE 802.11u)
# This can be used to enable functionality to improve interworking with
# external networks.
#CONFIG_INTERWORKING=y

# Hotspot 2.0
#CONFIG_HS20=y

# Enable SQLite database support in hlr_auc_gw, EAP-SIM DB, and eap_user_file
#CONFIG_SQLITE=y

# Enable Fast Session Transfer (FST)
#CONFIG_FST=y

# Enable CLI commands for FST testing
#CONFIG_FST_TEST=y

# Testing options
# This can be used to enable some testing options (see also the example
# configuration file) that are really useful only for testing clients that
# connect to this hostapd. These options allow, for example, to drop a
# certain percentage of probe requests or auth/(re)assoc frames.
#
#CONFIG_TESTING_OPTIONS=y

# Automatic Channel Selection
# This will allow hostapd to pick the channel automatically when channel is set
# to "acs_survey" or "0". Eventually, other ACS algorithms can be added in
# similar way.
#
# Automatic selection is currently only done through initialization, later on
# we hope to do background checks to keep us moving to more ideal channels as
# time goes by. ACS is currently only supported through the nl80211 driver and
# your driver must have survey dump capability that is filled by the driver
# during scanning.
#
# You can customize the ACS survey algorithm with the hostapd.conf variable
# acs_num_scans.
#
# Supported ACS drivers:
# * ath9k
# * ath5k
# * ath10k
#
# For more details refer to:
# https://wireless.wiki.kernel.org/en/...umentation/acs
#
CONFIG_ACS=y

# Multiband Operation support
# These extensions facilitate efficient use of multiple frequency bands
# available to the AP and the devices that may associate with it.
#CONFIG_MBO=y

# Client Taxonomy
# Has the AP retain the Probe Request and (Re)Association Request frames from
# a client, from which a signature can be produced which can identify the model
# of client device like "Nexus 6P" or "iPhone 5s".
#CONFIG_TAXONOMY=y

# Fast Initial Link Setup (FILS) (IEEE 802.11ai)
#CONFIG_FILS=y
# FILS shared key authentication with PFS
#CONFIG_FILS_SK_PFS=y

# Include internal line edit mode in hostapd_cli. This can be used to provide
# limited command line editing and history support.
#CONFIG_WPA_CLI_EDIT=y

# Opportunistic Wireless Encryption (OWE)
# Experimental implementation of draft-harkins-owe-07.txt
#CONFIG_OWE=y

# Airtime policy support
#CONFIG_AIRTIME_POLICY=y

# Override default value for the wpa_disable_eapol_key_retries configuration
# parameter. See that parameter in hostapd.conf for more details.
#CFLAGS += -DDEFAULT_WPA_DISABLE_EAPOL_KEY_RETRIES=1

# Wired equivalent privacy (WEP)
# WEP is an obsolete cryptographic data confidentiality algorithm that is not
# considered secure. It should not be used for anything anymore. The
# functionality needed to use WEP is available in the current hostapd
# release under this optional build parameter. This functionality is subject to
# be completely removed in a future release.
#CONFIG_WEP=y

# Remove all TKIP functionality
# TKIP is an old cryptographic data confidentiality algorithm that is not
# considered secure. It should not be used anymore. For now, the default hostapd
# build includes this to allow mixed mode WPA+WPA2 networks to be enabled, but
# that functionality is subject to be removed in the future.
#CONFIG_NO_TKIP=y

# Pre-Association Security Negotiation (PASN)
# Experimental implementation based on IEEE P802.11z/D2.6 and the protocol
# design is still subject to change. As such, this should not yet be enabled in
# production use.
# This requires CONFIG_IEEE80211W=y to be enabled, too.
#CONFIG_PASN=y

# Device Provisioning Protocol (DPP) (also known as Wi-Fi Easy Connect)
CONFIG_DPP=y
# DPP version 2 support
CONFIG_DPP2=y
# DPP version 3 support (experimental and still changing; do not enable for
# production use)
#CONFIG_DPP3=y

 

Here is my hostapd configuration file.

ctrl_interface=/var/run/hostapd
ctrl_interface_group=0
interface=wlp3s0
driver=nl80211
ssid=test
channel=0
beacon_int=100
hw_mode=g
wmm_enabled=1
ieee80211n=1
macaddr_acl=0
ht_capab=[SHORT-GI-20][SHORT-GI-40]
auth_algs=1
ignore_broadcast_ssid=0
wpa=3
wpa_passphrase=deathnote
wpa_key_mgmt=WPA-PSK
wpa_pairwise=TKIP
rsn_pairwise=CCMP

 

Here is the log messages when start hostapd

random: Trying to read entropy from /dev/randomstapd ../../hostapd-minima
Configuration file: ../../hostapd-minimal.conf
ctrl_interface_group=0
nl80211: Using driver-based roaming
nl80211: TDLS supported
nl80211: Supported cipher 00-0f-ac:1
nl80211: Supported cipher 00-0f-ac:5
nl80211: Supported cipher 00-0f-ac:2
nl80211: Supported cipher 00-0f-ac:4
nl80211: Supported cipher 00-0f-ac:6
nl80211: Using driver-based off-channel TX
nl80211: Supported vendor command: vendor_id=0x1018 subcmd=1
nl80211: Supported vendor event: vendor_id=0x1018 subcmd=0
nl80211: Supported vendor event: vendor_id=0x1018 subcmd=1
nl80211: Use separate P2P group interface (driver advertised support)
nl80211: Enable multi-channel concurrent (driver advertised support)
nl80211: use P2P_DEVICE support
nl80211: key_mgmt=0xd0f enc=0x10f auth=0x7 flags=0x380cfac0 rrm_flags=0x00
nl80211: interface wlan0 in phy phy0
nl80211: Set mode ifindex 3 iftype 3 (AP)
nl80211: Setup AP(wlan0) - device_ap_sme=1 use_monitor=0
nl80211: Subscribe to mgmt frames with AP handle 0x7d57c0 (device SME)
nl80211: Register frame type=0xd0 (WLAN_FC_STYPE_ACTION) nl_handle=0x7d570
nl80211: Register frame command failed (type=208): ret=-114 (Operation al)
nl80211: Register frame match - hexdump(len=1): 04
nl80211: Register frame type=0xd0 (WLAN_FC_STYPE_ACTION) nl_handle=0x7d570
nl80211: Register frame type=0xd0 (WLAN_FC_STYPE_ACTION) nl_handle=0x7d570
nl80211: Register frame type=0xd0 (WLAN_FC_STYPE_ACTION) nl_handle=0x7d570
nl80211: Register frame type=0xd0 (WLAN_FC_STYPE_ACTION) nl_handle=0x7d570
nl80211: Register frame command failed (type=208): ret=-114 (Operation al)
nl80211: Register frame match - hexdump(len=1): 06
nl80211: Register frame type=0xd0 (WLAN_FC_STYPE_ACTION) nl_handle=0x7d570
nl80211: Register frame command failed (type=208): ret=-114 (Operation al)
nl80211: Register frame match - hexdump(len=1): 08
nl80211: Register frame type=0xd0 (WLAN_FC_STYPE_ACTION) nl_handle=0x7d570
nl80211: Register frame command failed (type=208): ret=-114 (Operation al)
nl80211: Register frame match - hexdump(len=1): 09
nl80211: Register frame type=0xd0 (WLAN_FC_STYPE_ACTION) nl_handle=0x7d570
nl80211: Register frame command failed (type=208): ret=-114 (Operation al)
nl80211: Register frame match - hexdump(len=1): 0a
nl80211: Register frame type=0xd0 (WLAN_FC_STYPE_ACTION) nl_handle=0x7d570
nl80211: Register frame command failed (type=208): ret=-114 (Operation al)
nl80211: Register frame match - hexdump(len=1): 11
nl80211: Register frame type=0xd0 (WLAN_FC_STYPE_ACTION) nl_handle=0x7d570
nl80211: Register frame command failed (type=208): ret=-114 (Operation al)
nl80211: Register frame match - hexdump(len=1): 7f
nl80211: Failed to subscribe for mgmt frames from SME driver - trying to t
nl80211: Enable Probe Request reporting nl_preq=0x7d57c0
nl80211: Register frame type=0x40 (WLAN_FC_STYPE_PROBE_REQ) nl_handle=0x70
rfkill: initial event: idx=1 type=1 op=0 soft=0 hard=0
nl80211: Add own interface ifindex 3 (ifidx_reason -1)
nl80211: if_indices[16]: 3(-1)
phy: phy0
BSS count 1, BSSID mask 00:00:00:00:00:00 (0 bits)
nl80211: Regulatory information - country=00
nl80211: 2402-2472 @ 40 MHz 20 mBm
nl80211: 2457-2482 @ 20 MHz 20 mBm (no IR)
nl80211: 2474-2494 @ 20 MHz 20 mBm (no OFDM) (no IR)
nl80211: 5170-5250 @ 80 MHz 20 mBm (no IR)
nl80211: 5250-5330 @ 80 MHz 20 mBm (DFS) (no IR)
nl80211: 5490-5730 @ 160 MHz 20 mBm (DFS) (no IR)
nl80211: 5735-5835 @ 80 MHz 20 mBm (no IR)
nl80211: 57240-63720 @ 2160 MHz 0 mBm
nl80211: Added 802.11b mode based on 802.11g information
nl80211: Mode IEEE 802.11g: 2412 2417 2422 2427 2432 2437 2442 2447 2452 2
nl80211: Mode IEEE 802.11a: 5180 5200 5220 5240 5260 5280 5300 5320 5500 5
nl80211: Mode IEEE 802.11b: 2412 2417 2422 2427 2432 2437 2442 2447 2452 2
Allowed channel: mode=1 chan=1 freq=2412 MHz max_tx_power=20 dBm
Allowed channel: mode=1 chan=2 freq=2417 MHz max_tx_power=20 dBm
Allowed channel: mode=1 chan=3 freq=2422 MHz max_tx_power=20 dBm
Allowed channel: mode=1 chan=4 freq=2427 MHz max_tx_power=20 dBm
Allowed channel: mode=1 chan=5 freq=2432 MHz max_tx_power=20 dBm
Allowed channel: mode=1 chan=6 freq=2437 MHz max_tx_power=20 dBm
Allowed channel: mode=1 chan=7 freq=2442 MHz max_tx_power=20 dBm
Allowed channel: mode=1 chan=8 freq=2447 MHz max_tx_power=20 dBm
Allowed channel: mode=1 chan=9 freq=2452 MHz max_tx_power=20 dBm
Allowed channel: mode=1 chan=10 freq=2457 MHz max_tx_power=20 dBm
Allowed channel: mode=1 chan=11 freq=2462 MHz max_tx_power=20 dBm
Allowed channel: mode=2 chan=36 freq=5180 MHz max_tx_power=20 dBm
Allowed channel: mode=2 chan=40 freq=5200 MHz max_tx_power=20 dBm
Allowed channel: mode=2 chan=44 freq=5220 MHz max_tx_power=20 dBm
Allowed channel: mode=2 chan=48 freq=5240 MHz max_tx_power=20 dBm
Allowed channel: mode=2 chan=52 freq=5260 MHz max_tx_power=20 dBm
Allowed channel: mode=2 chan=56 freq=5280 MHz max_tx_power=20 dBm
Allowed channel: mode=2 chan=60 freq=5300 MHz max_tx_power=20 dBm
Allowed channel: mode=2 chan=64 freq=5320 MHz max_tx_power=20 dBm
Allowed channel: mode=2 chan=100 freq=5500 MHz max_tx_power=20 dBm
Allowed channel: mode=2 chan=104 freq=5520 MHz max_tx_power=20 dBm
Allowed channel: mode=2 chan=108 freq=5540 MHz max_tx_power=20 dBm
Allowed channel: mode=2 chan=112 freq=5560 MHz max_tx_power=20 dBm
Allowed channel: mode=2 chan=116 freq=5580 MHz max_tx_power=20 dBm
Allowed channel: mode=2 chan=132 freq=5660 MHz max_tx_power=20 dBm
Allowed channel: mode=2 chan=136 freq=5680 MHz max_tx_power=20 dBm
Allowed channel: mode=2 chan=140 freq=5700 MHz max_tx_power=20 dBm
Allowed channel: mode=2 chan=144 freq=5720 MHz max_tx_power=20 dBm
Allowed channel: mode=2 chan=149 freq=5745 MHz max_tx_power=20 dBm
Allowed channel: mode=2 chan=153 freq=5765 MHz max_tx_power=20 dBm
Allowed channel: mode=2 chan=157 freq=5785 MHz max_tx_power=20 dBm
Allowed channel: mode=2 chan=161 freq=5805 MHz max_tx_power=20 dBm
Allowed channel: mode=2 chan=165 freq=5825 MHz max_tx_power=20 dBm
Allowed channel: mode=0 chan=1 freq=2412 MHz max_tx_power=20 dBm
Allowed channel: mode=0 chan=2 freq=2417 MHz max_tx_power=20 dBm
Allowed channel: mode=0 chan=3 freq=2422 MHz max_tx_power=20 dBm
Allowed channel: mode=0 chan=4 freq=2427 MHz max_tx_power=20 dBm
Allowed channel: mode=0 chan=5 freq=2432 MHz max_tx_power=20 dBm
Allowed channel: mode=0 chan=6 freq=2437 MHz max_tx_power=20 dBm
Allowed channel: mode=0 chan=7 freq=2442 MHz max_tx_power=20 dBm
Allowed channel: mode=0 chan=8 freq=2447 MHz max_tx_power=20 dBm
Allowed channel: mode=0 chan=9 freq=2452 MHz max_tx_power=20 dBm
Allowed channel: mode=0 chan=10 freq=2457 MHz max_tx_power=20 dBm
Allowed channel: mode=0 chan=11 freq=2462 MHz max_tx_power=20 dBm
Completing interface initialization
Mode: IEEE 802.11g Channel: 6 Frequency: 2437 MHz
DFS 0 channels required radar detection
nl80211: Set freq 2437 (ht_enabled=1, vht_enabled=0, he_enabled=0, eht_en)
* freq=2437
* eht_enabled=0
* he_enabled=0
* vht_enabled=0
* ht_enabled=1
* radar_background=0
* sec_channel_offset=0
* channel_type=1
RATE[0] rate=10 flags=0x1
RATE[1] rate=20 flags=0x1
RATE[2] rate=55 flags=0x1
RATE[3] rate=110 flags=0x1
RATE[4] rate=60 flags=0x0
RATE[5] rate=90 flags=0x0
RATE[6] rate=120 flags=0x0
RATE[7] rate=180 flags=0x0
RATE[8] rate=240 flags=0x0
RATE[9] rate=360 flags=0x0
RATE[10] rate=480 flags=0x0
RATE[11] rate=540 flags=0x0
hostapd_setup_bss(hapd=0x7d31d0 (wlan0), first=1)
nl80211: flush -> DEL_STATION wlan0 (all)
Using interface wlan0 with hwaddr 28:ed:e0:14:c6:4c and ssid "test"
Deriving WPA PSK based on passphrase
SSID - hexdump_ascii(len=4):
74 65 73 74 test
PSK (ASCII passphrase) - hexdump_ascii(len=9): [REMOVED]
PSK (from passphrase) - hexdump(len=32): [REMOVED]
random: Got 20/20 random bytes
Get randomness: len=32 entropy=0
GMK - hexdump(len=32): [REMOVED]
Get randomness: len=32 entropy=0
Key Counter - hexdump(len=32): [REMOVED]
WPA: Delay group state machine start until Beacon frames have been configd
nl80211: Set beacon (beacon_set=0)
nl80211: Beacon head - hexdump(len=55): 80 00 00 00 ff ff ff ff ff ff 28 6
nl80211: Beacon tail - hexdump(len=133): 2a 01 04 32 04 30 48 60 6c 30 140
nl80211: ifindex=3
nl80211: beacon_int=100
nl80211: beacon_rate=0
nl80211: rate_type=0
nl80211: dtim_period=2
nl80211: ssid=test
* beacon_int=100
* dtim_period=2
nl80211: hidden SSID not in use
nl80211: privacy=3
nl80211: auth_algs=0x1
nl80211: wpa_version=0x3
nl80211: key_mgmt_suites=0x2
nl80211: pairwise_ciphers=0x18
nl80211: group_cipher=0x8
wlan0: Deauthenticate all stations at BSS start
nl80211: sta_remove -> DEL_STATION wlan0 ff:ff:ff:ff:ff:ff --> 0 (Success)
WPA: Start group state machine to set initial keys
WPA: group state machine entering state GTK_INIT (VLAN-ID 0)
Get randomness: len=32 entropy=0
GTK - hexdump(len=32): [REMOVED]
WPA: group state machine entering state SETKEYSDONE (VLAN-ID 0)
wpa_driver_nl80211_set_key: ifindex=3 (wlan0) alg=2 addr=0xb5aec key_idx=1
nl80211: NEW_KEY
nl80211: KEY_DATA - hexdump(len=32): [REMOVED]
broadcast key
nl80211: NL80211_CMD_SET_KEY - default key
nl80211: Set wlan0 operstate 0->1 (UP)
netlink: Operstate: ifindex=3 linkmode=-1 (no change), operstate=6 (IF_OP)
nl80211: TX queue param set: queue=0 aifs=1 cw_min=3 cw_max=7 burst_time=5
Failed to set TX queue parameters for queue 0.
nl80211: TX queue param set: queue=1 aifs=1 cw_min=7 cw_max=15 burst_time5
Failed to set TX queue parameters for queue 1.
nl80211: TX queue param set: queue=2 aifs=3 cw_min=15 cw_max=63 burst_tim5
Failed to set TX queue parameters for queue 2.
nl80211: TX queue param set: queue=3 aifs=7 cw_min=15 cw_max=1023 burst_t5
Failed to set TX queue parameters for queue 3.
wlan0: interface state UNINITIALIZED->ENABLED
wlan0: AP-ENABLED
wlan0: Setup of interface done.
ctrl_iface not configured!
RTM_NEWLINK: ifi_index=3 ifname=wlan0 wext ifi_family=0 ifi_flags=0x11043)
RTM_NEWLINK: ifi_index=3 ifname=wlan0 operstate=5 linkmode=0 ifi_family=0)
nl80211: Set IF_OPER_UP again based on ifi_flags and expected operstate
netlink: Operstate: ifindex=3 linkmode=-1 (no change), operstate=6 (IF_OP)
RTM_NEWLINK: ifi_index=3 ifname=wlan0 operstate=6 linkmode=0 ifi_family=0)
nl80211: Event message available
nl80211: Drv Event 48 (NL80211_CMD_DISCONNECT) received for wlan0
nl80211: Disconnect event
wlan0: Event DEAUTH (11) received
hostapd_notif_disassoc: Skip event with no address
nl80211: Event message available
nl80211: Drv Event 36 (NL80211_CMD_REG_CHANGE) received for wlan0
nl80211: Regulatory domain change
* initiator=0
* type=1
wlan0: Event CHANNEL_LIST_CHANGED (27) received
nl80211: Event message available
nl80211: Drv Event 33 (NL80211_CMD_TRIGGER_SCAN) received for wlan0
wlan0: nl80211: Scan trigger
wlan0: Event SCAN_STARTED (47) received
Unknown event 47
nl80211: Event message available
nl80211: Drv Event 35 (NL80211_CMD_SCAN_ABORTED) received for wlan0
wlan0: nl80211: Scan aborted
nl80211: Scan probed for SSID 'YourNemesis '
nl80211: Scan probed for SSID ''
nl80211: Scan included frequencies: 2412 2417 2422 2427 2432 2437 2442 245
wlan0: Event SCAN_RESULTS (3) received
nl80211: Event message available
nl80211: Drv Event 33 (NL80211_CMD_TRIGGER_SCAN) received for wlan0
wlan0: nl80211: Scan trigger
wlan0: Event SCAN_STARTED (47) received
Unknown event 47
nl80211: Event message available
nl80211: Drv Event 34 (NL80211_CMD_NEW_SCAN_RESULTS) received for wlan0
wlan0: nl80211: New scan results available
nl80211: Scan probed for SSID 'YourNemesis '
nl80211: Scan probed for SSID ''
nl80211: Scan included frequencies: 2412 2417 2422 2427 2432 2437 2442 245
wlan0: Event SCAN_RESULTS (3) received
RTM_NEWLINK: ifi_index=3 ifname=wlan0 wext ifi_family=0 ifi_flags=0x11043)
RTM_NEWLINK: ifi_index=3 ifname=wlan0 operstate=5 linkmode=0 ifi_family=0)
nl80211: Set IF_OPER_UP again based on ifi_flags and expected operstate
netlink: Operstate: ifindex=3 linkmode=-1 (no change), operstate=6 (IF_OP)
RTM_NEWLINK: ifi_index=3 ifname=wlan0 operstate=6 linkmode=0 ifi_family=0)
nl80211: Event message available
nl80211: Drv Event 16 (NL80211_CMD_STOP_AP) received for wlan0
wlan0: Event INTERFACE_UNAVAILABLE (28) received
Interface wlan0 is unavailable -- stopped
wlan0: Event EAPOL_RX (23) received
IEEE 802.1X: 99 bytes from 52:3f:ce:69:ac:4a (encrypted=-1)
IEEE 802.1X data frame from not associated/Pre-authenticating STA
RTM_NEWLINK: ifi_index=3 ifname=wlan0 wext ifi_family=0 ifi_flags=0x11043)
RTM_NEWLINK: ifi_index=3 ifname=wlan0 wext ifi_family=0 ifi_flags=0x11043)
RTM_NEWLINK: ifi_index=3 ifname=wlan0 wext ifi_family=0 ifi_flags=0x11043)
nl80211: Event message available
nl80211: Drv Event 46 (NL80211_CMD_CONNECT) received for wlan0
nl80211: Connect event (status=0 ignore_next_local_disconnect=0)
nl80211: Associated on 5745 MHz
nl80211: Associated with 52:3f:ce:69:ac:4a
nl80211: Operating frequency for the associated BSS from scan results: 57z
nl80211: Associated on 5745 MHz
nl80211: Associated with 52:3f:ce:69:ac:4a
nl80211: Set drv->ssid based on scan res info to 'YourNemesis '
wlan0: Event ASSOC (0) received
hostapd_notif_assoc: Skip event with no address
RTM_NEWLINK: ifi_index=3 ifname=wlan0 operstate=5 linkmode=0 ifi_family=0)
nl80211: Set IF_OPER_UP again based on ifi_flags and expected operstate
netlink: Operstate: ifindex=3 linkmode=-1 (no change), operstate=6 (IF_OP)
RTM_NEWLINK: ifi_index=3 ifname=wlan0 operstate=6 linkmode=0 ifi_family=0)
wlan0: Event EAPOL_RX (23) received
IEEE 802.1X: 155 bytes from 52:3f:ce:69:ac:4a (encrypted=-1)
IEEE 802.1X data frame from not associated/Pre-authenticating STA
....

 

I have tried a search on Google, but I really don't know what I need to search for. Can anyone help me to solve this? Please bear in mind that I am new to this and so would appreciate being told in plain English what I need to do or where I need to start

Thank you

 

0 Kudos
2 Replies

606 Views
karthik_mohan
Contributor II

I understand. But Technexion doesn't have an open forum as per my understanding, so where shall I ask ?

0 Kudos

613 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Please contact wandboard for this issue, since i.Mx6 from NXP does not have a solution for you.

Regards

 

0 Kudos