i.MX6D: AR8033 Ethernet PHY register setting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6D: AR8033 Ethernet PHY register setting

3,282 Views
ganesank
Contributor III

Hi,

 

Our Electrical team wants to change a register setting in AR8033 ethernet PHY in order to pass EMI/EMC Regulatory tests. The change is in PHY control register (section 5.3.7 in page 97 of AR8033 datasheet. Attached) to reduce to voltage from 1.8 v to 1.5v.

  

The Power-ON default value is 1.5 v but it was changed (highlighted) in the BSP in file arch/arm/mach-imx/mach-imx6q.c (Linux 4.9)

 

static int ar8031_phy_fixup(struct phy_device *dev)

{

       u16 val;

 

       /* Set RGMII IO voltage to 1.8V */

       phy_write(dev, 0x1d, 0x1f);

       phy_write(dev, 0x1e, 0x8);

 

       /* disable phy AR8031 SmartEEE function. */

       phy_write(dev, 0xd, 0x3);

       phy_write(dev, 0xe, 0x805d);

       phy_write(dev, 0xd, 0x4003);

       val = phy_read(dev, 0xe);

       val &= ~(0x1 << 8);

       phy_write(dev, 0xe, val);

 

       /* To enable AR8031 output a 125MHz clk from CLK_25M */

       phy_write(dev, 0xd, 0x7);

       phy_write(dev, 0xe, 0x8016);

       phy_write(dev, 0xd, 0x4007);

 

       val = phy_read(dev, 0xe);

       val &= 0xffe3;

       val |= 0x18;

       phy_write(dev, 0xe, val);

 

       /* introduce tx clock delay */

       phy_write(dev, 0x1d, 0x5);

       val = phy_read(dev, 0x1e);

       val |= 0x0100;

       phy_write(dev, 0x1e, val);

 

       return 0;

}

 

#define PHY_ID_AR8031  0x004dd074

 

Question to the team:

I have removed those source code lines to pass the tests but I am interested in knowing why Freescale/NXP set it to 1.8V. Are there any other side effects in leaving it to default value of 1.5v. My electrical team says that Ethernet Eye pattern may have an impact by reducing this voltage. Does anyone have background about this. Any information regarding this would be appreciated. Regulatory tests are passing with good margin by keeping this voltage to 1.5 v but I wanted to ensure that we are not compromising on any other factors.

Tags (1)
0 Kudos
Reply
2 Replies

2,051 Views
jimmychan
NXP TechSupport
NXP TechSupport

I think you can use it at 1.5V. It should not have any side effect.

0 Kudos
Reply

1,553 Views
asim_zaidi
NXP Employee
NXP Employee

A confidential and proprietary document was incorrectly attached to this thread and has hence been removed by the Community Admins.

For secure communication or sharing confidential information please submit a ticket at https://support.nxp.com/.

0 Kudos
Reply