1) We use Use L3.0.35_4.1.0_130816_images_MX6.tar.gz on i.MX6Q-SDP with below commands to do dual record but fail.
2) Have to submit SR, but he suggest post here.
3) Also try the apply unoffical patch from <OV5640 and OV5642 cameras on iMX6 | Freescale Community>, and it can do dual record. But will encounter performance issue while playing movie.
------------------------------------------------------------------
1)
modprobe ov5640_camera_mipi
modprobe ov5642_camera
modprobe mxc_v4l2_capture
gst-launch -e mfw_v4lsrc device=/dev/video0 ! mfw_ipucsc ! vpuenc codec=6 ! matroskamux ! filesink location=video0.mkv &
gst-launch -e mfw_v4lsrc device=/dev/video1 ! mfw_ipucsc ! vpuenc codec=6 ! matroskamux ! filesink location=video1.mkv &
ERROR message
root@freescale ~$ gst-launch -e mfw_v4lsrc device=/dev/video1 ! mfw_ipucsc ! vpu
enc codec=6 ! matroskamux ! filesink location=video1.mkv &
root@freescale ~$ MFW_GST_V4LSRC_PLUGIN 3.0.7 build on Aug 16 2013 20:15:40.
IPU_CSC_CORE_LIBRARY_VERSION_INFOR_01.00.
MFW_GST_IPU_CSC_PLUGIN 3.0.7 build on Aug 16 2013 20:16:04.
Setting pipeline to PAUSED ...
[INFO] Product Info: i.MX6Q/D/S
vpuenc versions :smileyhappy:
plugin: 3.0.7
wrapper: 1.0.35(VPUWRAPPER_ARM_LINUX Build on Aug 16 2013 20:14:38)
vpulib: 5.4.16
firmware: 2.3.10.40778
imx-ipuv3 imx-ipuv3.0: handler already installed on irq 0
Error registering rot irq
ERROR: Pipeline doesn't want to pause.
Setting pipeline to NULL ...
Freeing pipeline ...
------------------------------------------------------------------
2) SR 1-1226100721
The latest mxc V4L2 capture driver supports 2 cameras simultaneously.
The below v4l2 capture unit test command lines may verify this feature on MX6 SabreSD platform:
root@freescale /unit_tests$ ./mxc_v4l2_capture.out -iw 1024 -ih 768 -ow 1024 -oh 768 -m 8 -fr 15 -d /dev/video0 -i 1 -c 100 /test1.yuv & root@freescale /unit_tests$ ./mxc_v4l2_capture.out -iw 1024 -ih 768 -ow 1024 -oh 768 -m 8 -fr 15 -d /dev/video1 -i 0 -c 100 /test2.yuv in_width = 1024, in_height = 768 out_width = 1024, out_height = 768 top = 0, left = 0 in_width = 1024, in_height = 768 out_width = 1024, out_height = 768 top = 0, left = 0
If this will not help, please post issue on Community, our multimedia experts will try to help You there.
------------------------------------------------------------------
3)
gst-launch -e mfw_v4lsrc device=/dev/video0 ! mfw_ipucsc ! vpuenc codec=6 ! mpegtsmux ! filesink location=video0.ts&
gst-launch -e mfw_v4lsrc device=/dev/video1 ! mfw_ipucsc ! vpuenc codec=6 ! mpegtsmux ! filesink location=video1.ts&
gst-launch playbin2 uri=file:///Wife.mp4&
ERROR message
WARNING: from element /GstPlayBin2:playbin20/GstPlaySink:playsink0/GstBin:vbin/GstAutoVideoSink:videosink/MFW_GST_V4LSINK_INFO_T:videosink-actual-sink-mfw_v4l: A lot of buffers are being dropped.
Additional debug info:
gstbasesink.c(2866): gst_base_sink_is_too_late (): /GstPlayBin2:playbin20/GstPlaySink:playsink0/GstBin:vbin/GstAutoVideoSink:videosink/MFW_GST_V4LSINK_INFO_T:videosink-actual-sink-mfw_v4l:
There may be a timestamping problem, or this computer is too slow.
------------------------------------------------------------------
解決済! 解決策の投稿を見る。
Hi m.c,
Rogerio and Daiane have replied to you in Re: i.MX6 gstreamer dual record fail
Could you please try the latest kernel from git repository?
Branch: imx_3.0.35
It has the following patch that adds support for 2 cameras instances:
Would you please have a try?
Best Regards
Dan
m.C. do you have further questions? If yes plese keep working with our enginer, otherwise we will close the DI in 3 days.
Thanks,
Yixing
Hi m.c,
Rogerio and Daiane have replied to you in Re: i.MX6 gstreamer dual record fail
Could you please try the latest kernel from git repository?
Branch: imx_3.0.35
It has the following patch that adds support for 2 cameras instances:
Would you please have a try?
Best Regards
Dan
hi, Wang
your link about "patch that adds support for 2 cameras instances" can't access!
can you supply it as attachement?
We need the function that dual camera record simultaneously too.
Thanks.