We have a custom board which includes :
i.MX6 solo lite
LPDDR2
4 GB eMMC 5.0 connectd to USDHC2 configured for 8 bit DDR or SDR
We can flash the eMMC with u-boot using MFG tool
We can run u-boot from MFG tool
We are trying to run u-boot form User partition.
We read almost all the discussions regarding i,MX6 and eMMC , we tried all the solutions but the device always falls into HID mode, we cannot pass the boot ROM and we cannot see any data coming back from the eMMC, only commands runnig from the i.MX.
We saw in previous post the iMX6 can work with eMMC 5.0 but we also saw the booting from it is not possible.
So, we have some questions:
1. can the i.MX6 (in general and solo lite specific) boot from eMMC 5.0 and above? read and write operation are working fine emulating it as eMMC 4.4, but boot is not happening?
2. if you succeeded booting from eMMC 5.0, how did you do it? what is the iMX6 fuses configuration? what is the eMMC configuration? are there any other needed tasks to be done?
3. if booting is not possible, any suggestion? should we add a NOR flash for u-boot? should we go down to eMMC4.4? will eMMC 4.4 going to be discontinued soon? we were told they are not manufactured any more.
4. is there a difference in the reset pin od the USDHC2 and USDHC 3/4? if yest what is the implication on the system in general and on the boot process specific?
5. what about i.MX7, its performance is good enough for our product, can i.MX7 boot from eMMC 5.0?
Thanks for any help you can provide.
Please try to update mmc.c file as menitoned in this document:
https://community.nxp.com/docs/DOC-332187
Have a great day,
Victor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------